CLI BDM Programmer for ColdFire V2 on Linux or Windows

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CLI BDM Programmer for ColdFire V2 on Linux or Windows

5,240 Views
lucaskt
Contributor I

Hello,

 

I was wondering if there are any CLI (Command Line Interface) USB BDM Flash Programmers for ColdFire V2 for either Linux (preferably) or Windows.

 

I've been trying to perform this recording on Linux via BDM tools (http://sourceforge.net/projects/bdm/) , and so far have been unsucessful.

 

I was also wondering if the default Code Warrior recorder can be used outside the IDE, or is it built-in?

 

Thanks for any replies.

Lucas

Tags (2)
0 Kudos
Reply
2 Replies

1,483 Views
greg_b
Contributor I
0 Kudos
Reply

1,483 Views
diep
Contributor I

Hi

If I use "CLI BDM Programmer for ColdFire V2 on Linux or Windows", what hardware tool do I have to use to programming for MCF5271?

thank

0 Kudos
Reply