CLI BDM Programmer for ColdFire V2 on Linux or Windows

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CLI BDM Programmer for ColdFire V2 on Linux or Windows

5,260件の閲覧回数
lucaskt
Contributor I

Hello,

 

I was wondering if there are any CLI (Command Line Interface) USB BDM Flash Programmers for ColdFire V2 for either Linux (preferably) or Windows.

 

I've been trying to perform this recording on Linux via BDM tools (http://sourceforge.net/projects/bdm/) , and so far have been unsucessful.

 

I was also wondering if the default Code Warrior recorder can be used outside the IDE, or is it built-in?

 

Thanks for any replies.

Lucas

ラベル(2)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,503件の閲覧回数
greg_b
Contributor I
0 件の賞賛
返信

1,503件の閲覧回数
diep
Contributor I

Hi

If I use "CLI BDM Programmer for ColdFire V2 on Linux or Windows", what hardware tool do I have to use to programming for MCF5271?

thank

0 件の賞賛
返信