BDM doubt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,602件の閲覧回数
isaacmartinezsa
Contributor II

if a program BDM HCS08 series.

can program the "MC9S08SE8CRL"?,

or is there except for a microcontroller?,

I'm new to microcontrollers

ラベル(1)
0 件の賞賛
返信
1 解決策
2,386件の閲覧回数
carloscuev
Contributor V

If I undestand your question correctly, you want to know if a HCS08 programmer will program a MC9S08SE8CRL. The answer is yes, there's nothing apecial about SE8, has S08 core.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,387件の閲覧回数
carloscuev
Contributor V

If I undestand your question correctly, you want to know if a HCS08 programmer will program a MC9S08SE8CRL. The answer is yes, there's nothing apecial about SE8, has S08 core.

0 件の賞賛
返信
2,386件の閲覧回数
isaacmartinezsa
Contributor II

Same thing that S08 HCS08,

if yes why they put HC?

0 件の賞賛
返信
2,386件の閲覧回数
carloscuev
Contributor V

Yes HCS08 and S08 is the same, what's not the same is HC08 and HCS08. HC08 is the old motorola core, which was updated and now it's called HCS08, or S08 for short.

0 件の賞賛
返信