BDM doubt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BDM doubt

Jump to solution
2,656 Views
isaacmartinezsa
Contributor II

if a program BDM HCS08 series.

can program the "MC9S08SE8CRL"?,

or is there except for a microcontroller?,

I'm new to microcontrollers

Labels (1)
0 Kudos
Reply
1 Solution
2,440 Views
carloscuev
Contributor V

If I undestand your question correctly, you want to know if a HCS08 programmer will program a MC9S08SE8CRL. The answer is yes, there's nothing apecial about SE8, has S08 core.

View solution in original post

0 Kudos
Reply
3 Replies
2,441 Views
carloscuev
Contributor V

If I undestand your question correctly, you want to know if a HCS08 programmer will program a MC9S08SE8CRL. The answer is yes, there's nothing apecial about SE8, has S08 core.

0 Kudos
Reply
2,440 Views
isaacmartinezsa
Contributor II

Same thing that S08 HCS08,

if yes why they put HC?

0 Kudos
Reply
2,440 Views
carloscuev
Contributor V

Yes HCS08 and S08 is the same, what's not the same is HC08 and HCS08. HC08 is the old motorola core, which was updated and now it's called HCS08, or S08 for short.

0 Kudos
Reply