NXP Model-Based Design Tools Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP Model-Based Design Tools Knowledge Base

Discussions

Sort by:
Developing embedded applications for NXP microcontrollers—especially platforms like the S32K series—often involves using tools such as MATLAB/Simulink (MBDT – Model-Based Design Toolbox), S32 Design Studio (S32DS), and AUTOSAR tools like EB tresos. This article walks through the key steps involved in creating a new model and configuring it properly for NXP hardware, focusing on a practical workflow used in automotive and embedded systems projects.
View full article
Plot embedded data in a Chart or Gauge in a Web Browser
View full article
  Battery Management System Software and Hardware Environment 0 Table of Contents •Introduction •Software •Hardware •References •Conclusion 1 Introduction This article presents a comprehensive overview of the hardware and software components required to design and implement a high-voltage Battery Management System (BMS). It focuses on solutions based on NXP hardware platforms, combined with the integrated development ecosystems provided by NXP and MathWorks. The objective is to highlight how these technologies work together to streamline system development, deployment, and validation. 2 Software The software environment provides the modeling, simulation, communication, code generation, and deployment capabilities required by the Battery Management System. 2.1 Deep Learning Toolbox SorinIBancila_0-1786527787490.png   Deep Learning Toolbox brings artificial intelligence into the model-based workflow. It provides MATLAB functions, apps, and Simulink blocks for designing, training, simulating, and analyzing deep neural networks. This makes AI-based behavior easier to develop, understand, and validate before deployment. In the Battery Management System, deep learning can support battery state estimation, fault detection, and operating-condition classification. The toolbox can create and evaluate neural networks, import pretrained models from PyTorch, TensorFlow, and ONNX, and integrate trained networks into Simulink for system-level simulation. Artificial intelligence is not treated as a separate development activity. Neural network behavior can be simulated and verified together with the battery control model. Networks can also be optimized through quantization, projection, or pruning, and prepared for embedded deployment through automatic code generation. This reduces integration risk and makes AI-based BMS functions easier to validate within the complete system. For more information, see the Deep Learning Toolbox documentation in the References chapter. 2.2 Vehicle Network Toolbox SorinIBancila_1-1786527804953.png   Vehicle Network Toolbox brings CAN communication into the model-based workflow. It provides MATLAB functions and Simulink blocks for sending, receiving, encoding, and decoding CAN messages, making network behavior visible and testable before deployment. In the Battery Management System, commands, feedback, and status information are exchanged over CAN, linking the ECU with the surrounding vehicle architecture. The toolbox helps define signal interfaces, pack and unpack CAN messages, simulate bus traffic, and validate communication before target execution. Communication is not treated as a late integration step. CAN interaction can be simulated and verified together with the control model. This reduces integration risk and makes ECU behavior easier to validate end to end. For more information, see the Vehicle Network Toolbox documentation in the References chapter. 2.3 NXP Model-Based Design Toolbox for BMS SorinIBancila_2-1786527835753.png   The NXP Model-Based Design Toolbox for BMS extends the NXP Model-Based Design Toolbox for S32K3 with BMS support. It enables configuration and integration of the MC33775A, MC33774A, MC33772C, MC33665A, and MC33664. The S32K3 toolbox includes peripheral blocks that provide access to key microcontroller resources such as ADC, PWM, CAN, SPI, UART, timers, and interrupts. These interfaces facilitate communication between the S32K3 microcontroller and the supported BMS integrated circuits. Together, the toolboxes support the development and deployment of BMS applications on the S32K3 platform, leveraging the underlying S32K3 and BMS software stack. The workflow also integrates with NXP configuration tools and supports real-time monitoring and visualization through FreeMASTER, simplifying application development, validation, and debugging. 3 Hardware The central hardware platform is the 800 V Battery Management System Reference Design using ETPL. The kit contains: RD-K358BMU - Battery Management Unit RD33774CNTEVB - Cell Monitoring Unit RD772BJBTPL8EVB - Battery Junction Box BATT-18EMULATOR - 18-cell battery pack emulator SorinIBancila_3-1786527864628.png   3.1 RD-K358BMU The RD-K358BMU is an NXP reference Battery Management Unit (BMU) designed for evaluation, development, and rapid prototyping of 800 V high-voltage Battery Management System (HVBMS) hardware and software. It provides a representative automotive-grade BMU platform built around the S32K358 microcontroller, enabling developers to evaluate battery-management architectures, safety concepts, communication interfaces, diagnostics, and control strategies in a realistic system environment. The board integrates several NXP components, including the S32K358, FS26, MC33665A, HB2000, TJA1145A, PCA2131, NBP8 and MC12XS6. Together, these components provide the processing, power management, communication, sensing, actuation, diagnostics, and safety capabilities required in a high-voltage BMS application. SorinIBancila_4-1786527890248.png   3.2 Cell Monitoring Unit: MC33774A The RD33774CNT3EVB is a centralized Cell Monitoring Unit (CMU) reference design intended for the development and evaluation of 800 V high-voltage Battery Management System (HVBMS) applications. It uses Electrical Transport Protocol Link (ETPL) communication to connect with the broader BMS architecture and support reliable data exchange within the battery system. The board includes three MC33774 Analog Front End (AFE) devices arranged in a daisy-chain configuration. These AFEs are responsible for measuring and monitoring battery cell parameters, helping developers evaluate cell supervision, diagnostics, and communication strategies in a centralized BMS topology.   SorinIBancila_5-1786527906947.png   3.3 Battery Junction Box: MC33772C The RD772BJBTPL8EVB is a Battery Junction Box (BJB) reference design developed for 800 V high-voltage Battery Management System (HVBMS) applications. It leverages Electrical Transport Protocol Link (ETPL) communication to ensure robust and isolated data exchange within the battery system. The board features two MC33772C battery sensor ICs configured to deliver redundant measurements of voltage and current, improving diagnostic coverage and supporting functional safety requirements. It also performs isolation measurements, which are essential for monitoring insulation integrity and detecting potential fault conditions in high-voltage environments. SorinIBancila_6-1786527924913.png   3.4 18-Cell Battery Pack Emulator The BATT-18EMULATOR board is designed to emulate a multi-cell battery pack and is easily interfaced with MC33774 battery cell controller evaluation boards. It enables quick evaluation of NXP Battery Cell Controller (BCC) ICs and supports software development by providing a controlled and flexible test environment. The board allows users to intuitively adjust the voltage of each of the 18 emulated cells, as well as the voltage levels on selected analog inputs typically used for temperature sensing. This capability makes it particularly useful for validating measurement accuracy, system behavior, and control algorithms without requiring a physical battery pack. Additionally, the BATT-18EMULATOR provides three independent outputs, allowing up to three BCC ICs to be connected simultaneously to a single emulator board. 4 References Deep Learning Toolbox Documentation Vehicle Network Toolbox Documentation NXP Model-Based Design Toolbox 800 V Battery Management System Reference Designs Using ETPL 5 Conclusion This article described the software and hardware environment required for the Battery Management System. The software combines MathWorks model-based design capabilities with NXP BMS and S32K3 platform support. The hardware integrates the S32K3 with NXP battery-cell controllers, communication interfaces, and associated BMS devices. Together, these elements provide the foundation for battery monitoring, communication, algorithm development, code generation, deployment, and validation. Next article: BMS architecture and model description, including the main software components, communication interfaces, data flow, and overall application structure.
View full article
    1 Table of Contents • Introduction • Simulink Model Overview • Inputs • Algorithm • LED Output • Diagnostics • References • Conclusion     2 Introduction This article describes how the Front Lights System (FLS) and the Rear Lights System (RLS) applications work internally, by walking through the Simulink models and describing how signals travel from the CAN bus all the way to the LED strip on the evaluation board. The goal is to give a practical understanding of what each model does, from the moment a command is received up to the moment the corresponding lamp is turned on. Both nodes are described together because they share the same overall architecture, the same execution pattern, and almost the same set of subsystems. The differences between them are limited to the lighting functions that only make sense on one side of the vehicle (Daytime Running Lights on the front, Stop Lights on the rear) and to a few CAN identifiers. Presenting them side by side keeps the article shorter and highlights how the same design pattern is reused across projects. Earlier articles in this series introduced the boards, the toolchain, and the general project layout. This article focuses on the application logic.     3 Simulink Model Overview Each application is implemented as an individual Simulink model, one for the Front Node and one for the Rear Node, structured into communication, control, and output subsystems. From a model perspective, the application can be divided into four logical areas: CAN reception and unpacking Per-function logic control LED aggregation Diagnostics Roxana_Grigore01_0-1785008050809.png   Figure 1 - Front Lights main Simulink application Roxana_Grigore01_1-1785008086857.png   Figure 2 - Rear Lights main Simulink application The reception area receives CAN frames from the Central Controller and makes the extracted signals available to the rest of the model through shared Data Store Memory blocks. The control area contains one Stateflow chart per lighting function and decides which lamps should be on or off. The output area builds the color pattern from the lamp requests. This separation keeps the model modular and makes it easier to add new lighting functions without changing the reception or the actuation logic.     4 Inputs Each node receives information from three main categories of inputs. CAN Network Inputs CAN communication is the main source of information for both applications. All messages come from the Central Controller and are defined in the DBC file that ships with each project. On the Front Lights node the application consumes: Gear Mode - 4 bits Activate Headlights - 0 = OFF, 1 = LOW BEAM, 2 = HIGH BEAM Activate Fog Lights - 1-bit on/off command Turn Commands - packs the signals: Activate Hazard Lights Turn Left Turn Right On the Rear Lights node the set is almost the same, with Gear Mode replaced by Press Brake - an 8-bit signal that carries the brake pedal position. The other three messages are shared with the front node. Local Fault Input On top of the CAN traffic, each node reads a digital fault input through a DIO block. The value of this pin is stored in a shared Data Store ( FLS_Fault or RLS_Fault ) and is consumed by every logic-control chart. When the fault is asserted, the charts switch to a dedicated fault branch and the LEDs display a blink pattern to signal the condition visually. Configuration Inputs Before normal operation begins, each model runs an Initialize Function that sets up the peripherals used by the application. Roxana_Grigore01_2-1785008112285.png   Figure 3 - Initialize Function This subsystem enables the CAN controller interrupts and moves the controller into the started mode.     5 Algorithm Internally, each node performs four main processing activities. Message Reception The first step consists of collecting the incoming CAN traffic. Reception is interrupt-driven: a Can_RxIndication handler is registered at the top level of the model and fires a function-call trigger every time a new frame arrives. The trigger runs the CAN Unpack subsystem exactly once and captures the frame identifier, the payload, and the length. Model Representation of Message Reception Inside the CAN Unpack subsystem there is one CAN Unpack block per DBC message. Each block decodes the incoming frame and extracts the signals declared in the DBC file. Roxana_Grigore01_3-1785008150116.png   Figure 4 - Front Lights CAN reception subsystem Roxana_Grigore01_4-1785008170382.png   Figure 5 - Rear Lights CAN reception subsystem Overall, the reception subsystem receives the CAN frames, decodes the payload into named signals, and places them into the shared Data Stores. Per-Function Logic Control Every lighting function is implemented as a dedicated Stateflow chart. All charts follow the same skeleton: an Idle state where the lamp is OFF, one or more active states covering the operating modes, and a small fault branch ( Fault_Detected and Fault_Detected_Off ) that toggles a per-function fault flag whenever the shared fault input is asserted. Head Lights Logic Control The head lights chart reads CCS_ActivateHeadLights and moves from Idle to Head_Lights_LowBeam when the command equals 1, and to Head_Lights_HighBeam when it equals 2. Direct crossovers between the two beams are allowed without going through Idle. When the fault input is asserted, the chart enters the fault branch and toggles Low_Beam and High_Beam to create a blink pattern. Roxana_Grigore01_5-1785008190854.png   Figure 6 - Head Lights logic control chart Fog Lights Logic Control The fog lights chart moves from Idle to Fog_Lights_Active when CCS_ActivateFogLights is 1 and returns to Idle when the command drops back to 0. The fault branch is identical to the one used by the head lights chart. Roxana_Grigore01_6-1785008208315.png   Figure 7 - Fog Lights logic control chart DRL Logic Control (Front only) The DRL chart only exists on the front node. It keeps the daytime running lights on whenever the vehicle is in a drive gear: Idle moves to DRL_Active when CCS_GearMode is between 1 and 4, and drops back to Idle when the gear returns to 0. Fault handling is identical to the other charts. Roxana_Grigore01_7-1785008230958.png   Figure 8 - DRL logic control chart (Front Lights only) Stop Lights Logic Control (Rear only) The stop lights chart keeps the stop lights on as long as the brake pedal is pressed: Idle transitions to Brake_Active when CCS_PressBrake is different from 0, and returns to Idle when the pedal is released. The fault branch is identical to the other charts. Roxana_Grigore01_8-1785008253941.png   Figure 9 - Stop Lights logic control chart (Rear Lights only) Turn Lights (Turn Signals and Hazards) The turn lights chart handles both the direction indicators and the hazard lights, and also generates the blinking pattern. It uses parallel states: an outer super-state selects between Idle, Turn_Left_Active, Turn_Right_Active and Hazard_Active, while inside each active super-state a pair of On and Off states swaps every 500 ms using after(0.5, sec) transitions. From Idle, the chart enters Turn_Left_Active when CCS_TurnLeft is asserted, Turn_Right_Active when CCS_TurnRight is asserted, and Hazard_Active when CCS_ActivateHazardLights is asserted. Direct crossovers between left and right are allowed. When the fault input is asserted, the chart moves into the fault branch. Roxana_Grigore01_9-1785008272825.png   Figure 10 - Turn Lights logic control chart     6 LED Output The per-function charts do not drive the LED strip directly. They only produce simple lamp requests, and a central Stateflow chart is in charge of turning those requests into a color pattern that the LED strip can display. Each lighting mode has its own state inside this chart, and every state sets the colors that represent that mode on the strip. For example, the head lights use white, the fog lights light up a few dedicated pixels, and the turn signals move step by step across one side of the strip. The hazard mode reuses the same effect on both sides at the same time. On the front node the chart also includes a state for the daytime running lights, and on the rear node it includes a state for the stop lights. Once the color pattern is ready, it is passed to a Function-Call Subsystem that sends it to the physical LED strip. This subsystem takes care of the low-level details, so the rest of the model only deals with lighting behavior. Roxana_Grigore01_10-1785008298820.png   Figure 11 - LED output chart     7 Diagnostics Alongside the normal lighting behavior, each node also reports its own health to the rest of the system. A local fault input is read at runtime and made available to every logic chart, so the lamps can switch to a fault indication whenever a problem is detected on the board. The same fault information is also sent back to the Central Controller over CAN, using a short dedicated message. This way, the rest of the vehicle can react to a lighting-node fault without having to check anything manually. In addition, the model exposes its internal signals to FreeMASTER, which allows the developer to observe the CAN commands, the lamp requests, and the fault flags live during development and troubleshooting.     8 References Front and Rear Lights - Overview Front and Rear Lights - SW & HW Environment Model-Based Design Toolbox (MBDT) Community Model-Based Design Toolbox (MBDT) - S32K3 - How To MATLAB® and Simulink® Documentation     9 Conclusion This article described the internal behavior of the Front Lights and Rear Lights nodes by looking at how information flows through the models. It explained how CAN commands are received, interpreted by dedicated Stateflow charts, and finally turned into the corresponding lighting behavior on the LED strip, while the local fault status is reported back to the Central Controller. Because both applications share the same architecture, they were presented together. The only real differences are the set of lighting functions specific to each side of the vehicle (DRL on the front, Stop Lights on the rear) and the identifiers used for the fault message. The next articles in the series will take a closer look at specific parts of these applications, such as the CAN communication, the LED driving, and the tools used to validate and troubleshoot the lighting behavior.
View full article
  1 Table of Contents • Introduction • Component Configuration  • Conclusion • References 2 Introduction Before configuring the DIO component, make sure that the pins you intend to use have already been configured in both the Pins Tool and the Port component. If not, refer to the previous articles on pins and port configuration. 3 Component Configuration In order to configure the Dio peripheral, press on the Dio component on the left side of the screen for the Dio Configuration tab to be opened. There, press on the Dio Config tab. portpin.png Understanding how the DioPort and DioChannel are organized might prove useful later. The number present under the DioPort label represents the corresponding value of the Dio port that you want to access. Below you can find a table with the correspondence between the values and the registers. Register half DioPort value AL 0 AH 1 BL 2 BH 3 CL 4 CH 5 DL 6 DH 7 EL 8 EH 9 Each of those is half of a register and together every line forms a 32-bit register. For example, AL and AH contain all the pin values that are assigned to PTA. AL contains the first 16 pins and AH contains the next 16 pins. For example, the RGBLED0_RED pin is assigned to PTA29. From that we can conclude that, since 29 is higher than 15 (the 16th value of AL, since the first value is 0), the PTA29 pin must be assigned to the AH register. To reiterate, the PTA0–PTA15 pins belong to the AL register while the PTA16–PTA31 (the value must be offset by -16 when computing the Id) pins belong to the AH register, and this is true for the rest of the registers too: PTB, PTC, PTD, PTE. Note: When computing the channel Id for pins in the upper half of a port (e.g. PTA16–PTA31), subtract 16 from the pin number. To create a new channel, select the appropriate DioPort and click the + button next to DioChannel. A new channel entry will be created. Fill in the required channel information according to the pin that was previously configured in the Pins Tool and Port component. ADDNEWCHANNEL.png   Repeat this process for each newly configured pin, ensuring that the channel is added under the correct DioPort. 4 Conclusion After configuring the required DioChannels, save the configuration and regenerate the code. The configured DIO channels can then be used by the application to access the corresponding digital inputs and outputs. 5 References NXP Model-Based Design Toolbox – Community Interacting with Digital Inputs/Outputs on MR-CANHUBK344
View full article
  1 Table of Contents • Introduction • Pins Configuration • Configure Port Component • Conclusion • References 2 Introduction Before a microcontroller can interact with external hardware, its pins must be configured correctly. Whether you want to read a button state, drive an LED, communicate with a sensor, or use a peripheral, the first step is to configure the corresponding pins. 3 Pins Configuration First, identify the pin you want to use. In this example, we will use the following pin: RGBLED0_RED PTA29 GPIO29 Note: When working in S32 Configuration Tools, the pin MSCR value (third line) is not required. However, it will be needed later if you also configure the same pins in EB tresos. Configure the pins according to their intended use: input, output, or input/output. To begin, open the Pins Tool by clicking the Pins button in the upper-right corner. configToolView.png In the Pins Tool, the pins are organized into Functional Groups. In the default projects provided with the Model-Based Design Toolbox, these groups are arranged based on the peripheral to which the pins are routed. functionalGroups.png For this step, focus on the Pins tab in the upper-left area of the window. Search for the pin you want to configure; in this example, PTA29. pinPinsView.png If the desired functionality is already routed to a different pin, first disable that routing by clearing the corresponding selection before assigning it to PTA29. Next, update the identifier and label as needed, then enable the routing by selecting the checkbox on the left. This opens the routing selection dialog. selecttypeofsignal.png Select SIUL2:gpio,29 , as it matches the intended functionality. A second dialog then prompts you to select the pin direction. directionofpin.png  In this example, the LED is configured as Input/Output, matching the configuration used by the example project. Depending on the intended use of the pin, a different direction may be required — for example, a push button is typically configured as an input. Additional examples can be found in the default projects provided with the Model-Based Design Toolbox. 4 Configure Port Component The Port component must reflect the same pin configuration defined in the Pins Tool. After returning to the Peripherals Tool, the Port component may be highlighted in red because the pin configuration was modified in the Pins Tool and has not yet been updated in the Port component. PortComponent.png  In the default Model-Based Design Toolbox projects, PortPins are grouped into PortContainers according to their associated peripheral, such as Dio_Pins or Can_Pins . Locate the Dio_Pins PortContainer and update the PortPin entries so that they match the values configured in the Pins Tool. rgbled.png The pin will already contain the MSCR value inherited from the Pins configuration. Update the pin name as desired so it can be easily identified in the model, then repeat the process for each additional pin. The PortPin Id uniquely identifies each PortPin entry. The identifier must remain unique across all PortContainers. Note: If a duplicate PortPin Id value is used, the configuration will report an error. Assign a unique PortPin Id value to each configured pin. For example, a configuration containing 40 pins can use identifiers within the range described by the tool configuration. 5 Conclusion Once the pin configuration is complete and the Port component has been updated accordingly, you can continue with the configuration of the software components that will use those pins. 6 References NXP Model-Based Design Toolbox – Community Interacting with Digital Inputs/Outputs on MR-CANHUBK344
View full article
  1 Table of Contents • Introduction • Required Software • Required Hardware • Communication and Board-Specific Setup • References • Conclusion   2 Introduction The Main Node is the central application target used throughout this project. It sits between the simulation environment running on the host PC and the physical hardware that represents the various vehicle domains. While the previous article introduced the purpose of the Main Node and its role within the overall system, this article focuses on the environment that makes that functionality possible. Developing and validating the Main Node requires more than a target board. The application is modeled, tested, configured, deployed, and monitored using a collection of software tools that work together with the hardware platform. Understanding this environment is important for anyone interested in reproducing the setup or following the remaining articles in the series. This article describes the software components used during development, the hardware platform used to run the application, and the communication infrastructure that connects the Main Node to the rest of the system. CristinaB_0-1784806267828.png   Figure 1. Position of the Main Node within the system architecture.   3 Required Software The Main Node software environment combines MathWorks modeling tools with NXP target support and development utilities. Together, these tools provide the workflow used to model the application, generate code, configure the hardware platform, deploy the software, and observe its behavior during validation and runtime analysis. 3.1 Modeling and Application Development The Main Node application is developed as a Simulink model. MATLAB and Simulink are used to describe the behavior of the application before any software is deployed to hardware. Communication interfaces, application states, signal handling, and system-level functionality are assembled and validated within the modeling environment, allowing development to begin long before the target board is involved. The software environment used for this project includes: MATLAB R2024a or newer Simulink Simulink Coder Embedded Coder MATLAB Coder Stateflow These tools provide the code-generation workflow that transforms the model into embedded software capable of running on the target hardware. 3.2 Network Definition and Validation Communication is one of the primary responsibilities of the Main Node. It exchanges information with the simulation environment, the zonal gateways, and the remaining vehicle-domain nodes through a shared CAN network. Vehicle Network Toolbox is used to bring those communication interfaces directly into MATLAB and Simulink. By using the same DBC definitions during development and validation, communication behavior can be verified before deployment and remain consistent across the complete system. The shared DBC maintained with CANdb++ acts as a common communication contract between all participating nodes. Required tools: Vehicle Network Toolbox CANdb++ 3.1 or newer 3.3 Target Support and Code Generation The bridge between the Simulink model and the target hardware platform is provided by the required NXP Model-Based Design Toolbox package. The toolbox provides: Main target platform support Peripheral integration blocks Build integration Deployment support FreeMASTER integration Using these components, the generated software can be executed directly on the target hardware without requiring manual integration of low-level peripheral code. 3.4 Build and Configuration Environment After code generation, the application is built and deployed using the NXP software toolchain integrated inside Model-Based Design Toolbox package. These tools are used to compile, link, and deploy the generated software to the target board. In parallel, EB tresos is used to maintain the low-level configuration required by the Main Node environment. CAN communication, UART telemetry, I2C initialization, interrupt configuration, and board-level peripheral settings are all managed through this configuration flow. Together, these tools ensure that the generated software and the target configuration remain aligned throughout development. 3.5 Runtime Monitoring and Validation Once deployed, the Main Node can be observed through two complementary mechanisms. FreeMASTER Lite provides runtime visibility into application variables and internal states, while CAN analysis tools are used to inspect the communication exchanged across the network. These tools are used throughout development and validation activities to verify both application behavior and network communication. CristinaB_1-1784806393422.png   Figure 2. Development workflow used by the Main Node application.   4 Required Hardware Unlike the peripheral nodes, the Main Node is responsible for connecting the simulation environment with the physical hardware network. As a result, the hardware environment includes both the target board and the supporting infrastructure used during development, validation, and system-level execution. 4.1 S32N55 Board The Main Node application executes on an S32N55 board selected for the central application role. Within this setup, the board serves as the central application platform and hosts the software responsible for coordinating communication between the simulation environment and the zonal gateways. The board provides: CAN FD communication interfaces UART communication interfaces Debug and deployment connectivity I2C peripherals Processing resources required by the Main Node application The Main Node target board is the primary hardware platform referenced throughout this article series. 4.2 Host PC The host PC provides the environment used to interact with the full setup. Depending on the activity being performed, it may host: MATLAB and Simulink RoadRunner simulation environments FreeMASTER Lite CAN analysis software The host PC communicates with the Main Node both through the CAN network and through the dedicated telemetry interface used by FreeMASTER. 4.3 CAN Analyzer A CAN analyzer is used during development and validation to monitor network traffic exchanged between the Main Node and the zonal gateways. Beyond debugging, the analyzer also provides a convenient method of validating DBC definitions, message timing, and network integration behavior before the full setup is assembled.   5 Communication and Board-Specific Setup Several aspects of the Main Node environment are specific to the selected target board and are worth understanding before reproducing the setup. 5.1 Communication Topology The Main Node does not communicate directly with every vehicle-domain node. Instead, it exchanges information with the two zonal gateways, which distribute the relevant signals toward the corresponding vehicle-domain nodes. This arrangement keeps the system organized around a zonal architecture while allowing each subsystem to be developed and validated independently. 5.2 CAN Transceiver Initialization One hardware-specific detail of the target board concerns the external CAN transceiver. Note: Before CAN communication becomes available, the transceiver must first be switched from standby mode into normal operation. This transition is not controlled directly through a dedicated GPIO. Instead, it is performed through an I2C-connected port expander located on the board. As a result, the startup sequence requires an I2C initialization step before the FlexCAN controller can begin communication. CristinaB_2-1784806522309.png   Figure 3. CAN transceiver enable sequence on the target board. 5.3 FreeMASTER Telemetry Interface In addition to the CAN network, the Main Node exposes runtime telemetry through a dedicated UART connection used by FreeMASTER Lite. This interface is used throughout validation and runtime analysis to visualize application variables and monitor system behavior in real time.   6 References Model-Based Design Toolbox (MBDT) Community NXP S32N Vehicle Super-Integration Processors MathWorks Vehicle Network Toolbox NXP FreeMASTER Run-Time Debugging Tool   7 Conclusion This article introduced the environment used to develop, deploy, and validate the Main Node application. It described the software workflow, the hardware platform, and the communication infrastructure that connect the Main Node to both the simulation environment and the physical hardware network. Particular attention was given to the Main Node's position within the system topology, the UART-based telemetry interface used by FreeMASTER, and the I2C-controlled CAN transceiver initialization required by the target board. The next article moves beyond the enablement layer and focuses on the Main Node application itself, describing the information it receives, the processing it performs, and the outputs it publishes back into the system network.
View full article
      1 Table of Contents • Introduction • Software Environment • Hardware Environment • References • Conclusion     2 Introduction Turning a vehicle concept into an interactive Virtual Vehicle requires more than a standalone simulation model. It requires a connected software and hardware environment that can define the vehicle architecture, simulate the powertrain and vehicle dynamics, place the vehicle in realistic driving scenarios, visualize the behavior in 3D, and allow user interaction through driver-in-the-loop inputs. This article continues the Virtual Vehicle system series by moving from the system-level overview to the enablement layer behind the application. It highlights the MathWorks tools and host-side hardware resources that make the virtual vehicle demonstrator possible. At the core of the workflow is Model-Based Design. MathWorks tools are used to configure the vehicle architecture with Virtual Vehicle Composer, model the powertrain and vehicle dynamics, define and execute driving scenarios, create 3D road environments, exchange CAN-based signals, and analyze simulation results. The same environment also supports interactive execution, where driver inputs from a steering wheel and pedals can influence the virtual vehicle behavior during scenario playback.     3 Software Environment The software environment provides the modeling, simulation, scenario definition, visualization, communication, and analysis capabilities required by the Virtual Vehicle system. Each MathWorks tool contributes a specific part of the workflow, from vehicle architecture definition and plant modeling to 3D scenario execution and CAN-based interaction with external systems. 3.1 MATLAB and Simulink R2025b MATLAB and Simulink form the central engineering environment for the Virtual Vehicle. MATLAB.pngFigure 1. MATLAB MATLAB provides the scripting, data management, parameterization, and analysis capabilities required to configure simulations, process logged signals, and evaluate test results. Simulink.pngFigure 2. Simulink Simulink provides the model-based design environment in which the virtual vehicle, control logic, communication interfaces, and test harnesses are assembled. The system-level model can connect plant models, vehicle dynamics, driver inputs, scenario interfaces, and network communication blocks into a single executable simulation. 3.2 Virtual Vehicle Composer Virtual Vehicle Composer.pngFigure 3. Virtual Vehicle Composer Virtual Vehicle Composer is the configuration and assembly environment used to create the Virtual Vehicle model. It allows the user to define the vehicle class, select the powertrain architecture, choose the vehicle dynamics fidelity, configure components, specify test scenarios, select logged signals, build the vehicle model, run the configured tests, and analyze the results. In this Virtual Vehicle system, Virtual Vehicle Composer acts as the entry point for building a consistent vehicle model. It assembles the selected architecture from predefined and customizable components and prepares the model for closed-loop simulation in Simulink. The app also supports repeatable test execution. The same virtual vehicle can be operated across selected scenarios, while relevant signals are logged for review. This makes it suitable for early design studies, component comparison, control validation, and system-level behavior analysis before moving to hardware integration. 3.3 Powertrain Blockset Powertrain Blockset.pngFigure 4. Powertrain Blockset Powertrain Blockset provides the vehicle powertrain modeling foundation for the Virtual Vehicle model. It includes reference applications and component libraries for conventional, hybrid, and battery-electric propulsion systems. In this system, Powertrain Blockset supports the definition of the propulsion architecture, energy storage, electric motors, drivetrain elements, tires, driver models, and supervisory control behavior. It also provides workflows that help configure, resize, calibrate, and analyze the selected powertrain components. The generated vehicle model can be used for performance analysis, energy management studies, range evaluation, component sizing, control parameter optimization, and hardware-in-the-loop preparation. Because the models are open, project-specific subsystems can be integrated into the generated architecture when needed. 3.4 Vehicle Dynamics Blockset Vehicle Dynamics Blockset.pngFigure 5. Vehicle Dynamics Blockset Vehicle Dynamics Blockset provides the vehicle motion and handling foundation for the Virtual Vehicle. It includes reference applications and component libraries for propulsion, steering, suspension, vehicle body, brakes, tires, driver models, and supervisory controllers. For the Virtual Vehicle system, the blockset enables different levels of vehicle dynamics fidelity depending on the simulation objective. Longitudinal dynamics can be used for drive-cycle and energy studies, while combined longitudinal, lateral, and vertical dynamics can be used for handling, chassis behavior, and more complex driving scenarios. The blockset also supports 3D visualization workflows, allowing the virtual vehicle behavior to be observed in a realistic environment. This helps connect numerical simulation results with intuitive visual feedback during ride, handling, ADAS, and driver-in-the-loop demonstrations. 3.5 Automated Driving Toolbox Automated Driving Toolbox.pngFigure 6. Automated Driving Toolbox Automated Driving Toolbox supports the definition, simulation, and analysis of driving scenarios used to exercise the Virtual Vehicle. It provides capabilities for creating road layouts, actors, trajectories, sensor-related contexts, and repeatable test cases. In this setup, the toolbox is used to create controlled and repeatable traffic situations around the ego vehicle. These scenarios can be used to evaluate how the virtual vehicle behaves in predefined maneuvers, traffic interactions, lane-following conditions, or other driving situations relevant to the demonstration. By combining scenario definition with the vehicle model, the Virtual Vehicle can be validated in a structured way. Instead of testing only isolated model behavior, the complete system can be exercised against realistic road and traffic conditions. 3.6 Vehicle Network Toolbox Vehicle Network Toolbox.pngFigure 7. Vehicle Network Toolbox Library Vehicle Network Toolbox brings vehicle network communication into the model-based workflow. It provides MATLAB functions and Simulink blocks for sending, receiving, encoding, and decoding messages over in-vehicle network protocols such as CAN, CAN FD, J1939, and XCP. In the Virtual Vehicle, the toolbox is used to exchange selected vehicle signals with external systems or hardware components. CAN messages can be packed and unpacked using database-driven definitions, allowing the model to follow the same signal structure expected by the vehicle-level architecture. This makes communication behavior visible and testable during simulation. Commands, feedback, status information, and selected virtual vehicle signals can be validated before deployment or integration with physical controllers, reducing late-stage integration risk. 3.7 RoadRunner RoadRunner.pngFigure 8. RoadRunner RoadRunner provides the 3D scene creation environment used by the Virtual Vehicle system. It enables the design of detailed road networks, intersections, lane markings, traffic signs, buildings, terrain, and other environmental assets required for realistic driving simulation. In this workflow, RoadRunner supplies the visual and spatial context in which the virtual vehicle operates. The generated scenes can represent controlled proving-ground layouts, urban intersections, highway segments, or demonstration environments used for scenario execution. When combined with Simulink and the vehicle model, RoadRunner helps transform the simulation from a signal-level model into an interactive visual experience. This is especially useful for driver-in-the-loop demonstrations, ADAS workflows, and stakeholder-facing presentations. 3.8 Simulink 3D Animation Simulink 3D Animation.pngFigure 9. Simulink 3D Animation Library Simulink 3D Animation connects Simulink models and MATLAB algorithms to a 3D simulation environment, enabling dynamic systems to be visualized in photorealistic scenes. In the Virtual Vehicle system, it provides the visualization and interaction layer used to observe vehicle behavior in a 3D environment during simulation. The toolbox can use prebuilt scenes or imported scenes created in RoadRunner, and it allows vehicles, objects, lighting, weather effects, and sensor-related elements to be controlled during simulation. This makes it suitable for connecting the Virtual Vehicle model to visually rich driving environments. For driver-in-the-loop operation, Simulink 3D Animation also supports interactive navigation and manual control through hardware devices. This allows steering wheel and pedal inputs to influence the simulated vehicle while the resulting motion is visualized in the 3D scene. 3.9 Stateflow Stateflow.pngFigure 10. Stateflow Library Stateflow provides the graphical environment for modeling state machines, decision logic, and event-driven behavior inside the Virtual Vehicle system. It is used when vehicle behavior must depend on operating modes, transitions, conditions, timers, or fault states. Within the Virtual Vehicle model, Stateflow can support supervisory control, mode management, scenario state handling, driver input interpretation, startup and shutdown sequencing, or fallback behavior. This helps separate discrete decision logic from continuous plant and controller behavior. Using Stateflow keeps the system behavior easier to understand, review, and validate. Complex conditions can be represented explicitly as states and transitions, which improves traceability during simulation and debugging.     4 Hardware Environment The hardware environment provides the execution platform, user input interface, and visualization resources required to operate the Virtual Vehicle system interactively. The main components are the GPU-accelerated PC and the Xbox-compatible steering wheel and pedal controller. 4.1 PC with GPU Acceleration The PC is the main host platform for the Virtual Vehicle system. It runs MATLAB, Simulink, Virtual Vehicle Composer, RoadRunner-related workflows, and the supporting toolboxes used to model, simulate, visualize, and analyze the vehicle behavior. GPU acceleration is important because the system includes visually rich 3D scenes and interactive simulation workflows. The graphics hardware helps render the driving environment smoothly, maintain responsive visualization, and support a more realistic driver-in-the-loop experience. In this setup, the PC also acts as the integration point between the simulation model, the 3D environment, the input devices, and any external communication interfaces. This makes it the central execution and orchestration node of the Virtual Vehicle demonstration. 4.2 Xbox-Compatible Wheel Controller Xbox-Compatible Wheel Controller The Xbox-compatible wheel controller provides the physical driver input interface for the Virtual Vehicle system. It allows the user to control steering, acceleration, and braking through a steering wheel and pedal set instead of using keyboard-based commands. This input device makes the simulation suitable for driver-in-the-loop demonstrations. User actions can be mapped into the Simulink model and used to influence the virtual vehicle response during scenario execution. The wheel controller improves the realism and accessibility of the demonstration. It allows engineers and stakeholders to experience the virtual vehicle behavior interactively, making it easier to evaluate the relationship between driver input, vehicle response, and 3D scene feedback.     5 References The following resources provide useful background for the technologies referenced in this article: MathWorks MATLAB and Simulink documentation MathWorks Virtual Vehicle Composer documentation MathWorks Powertrain Blockset documentation MathWorks Vehicle Dynamics Blockset documentation MathWorks Automated Driving Toolbox documentation MathWorks Vehicle Network Toolbox documentation MathWorks RoadRunner documentation MathWorks Simulink 3D Animation documentation MathWorks Stateflow documentation     6 Conclusion This section described the software and hardware enablement required for the Virtual Vehicle system. The software environment combines MATLAB and Simulink with Virtual Vehicle Composer, Powertrain Blockset, Vehicle Dynamics Blockset, Automated Driving Toolbox, Vehicle Network Toolbox, RoadRunner, Simulink 3D Animation, and Stateflow to support vehicle configuration, system-level modeling, scenario execution, 3D visualization, communication, and analysis. The hardware environment combines a GPU-accelerated PC with a steering wheel and pedal controller to support interactive driver-in-the-loop execution. Together, these elements provide the foundation for building, operating, visualizing, and validating the virtual vehicle before integration with physical controllers or target hardware.
View full article
  1 Table of Contents • Introduction • Required Software • Required Hardware • References • Conclusion   2 Introduction This article focuses on the software and hardware environment required to build, deploy, and monitor the parking sensor node. On the software side, it presents the MATLAB/Simulink workflow, NXP's Model-Based Design Toolbox (MBDT) for S32K1xx devices, FreeMASTER, and the supporting build environment. On the hardware side, it describes the S32K144-Q100 evaluation board, the MaxBotix MB1020 ultrasonic sensors, the wiring approach, and the communication/debug interfaces used in the setup. The goal is to provide a clear setup foundation before moving into the next article, where the internal model architecture, control flow, and application behavior will be described in more detail.   3 Required Software The parking sensor application is developed using a model-based workflow built around MATLAB, Simulink, Stateflow, and NXP's MBDT for S32K1xx devices. The Simulink model remains the main development artifact, while the supporting toolchain is used to generate code, build the application, download it to the target board, and monitor the running system. 3.1 MATLAB, Simulink and Stateflow MATLAB and Simulink provide the main environment for developing the parking sensor application model. Simulink and Stateflow are used to organize the application structure, configure the processing blocks, and prepare the model for deployment on the S32K144 target. georgevictor_3-1784704792783.png   Figure 1. PSS top-level model in Simulink 3.2 NXP Model-Based Design Toolbox for S32K1xx NXP's Model-Based Design Toolbox (MBDT) for S32K1xx acts as the bridge between the Simulink model and the S32K144 hardware. It provides dedicated blocks for configuring and using the microcontroller peripherals required by the parking sensor node. In this project, MBDT is used for Analog-to-Digital Converter (ADC) acquisition, General-Purpose Input/Output (GPIO) control, Local Interconnect Network (LIN) communication, and FreeMASTER for real-time data visualisation. This allows the model to interact directly with the target hardware without requiring the developer to manually implement low-level peripheral code. The key point for this article is that MBDT keeps the hardware configuration close to the model. The detailed usage of each block and how the blocks are arranged inside the application will be explained in the model architecture article. 3.3 Code Generation and Deployment Flow The application is prepared for embedded deployment through the code generation flow supported by Simulink, Embedded Coder, ARM Cortex-M support, and NXP MBDT. From the developer's perspective, the main workflow remains inside Simulink: the model is configured, generated, built, and deployed to the S32K144 board. NXP's toolchain environment integrated in MBDT provides the compiler and target support used by the build process. In this setup, it does not need to be treated as a separate development step. The generated application can be downloaded to the S32K144-Q100 evaluation board through the MBDT build/deploy workflow using the on-board JTAG debug interface. This keeps the setup straightforward: once MBDT is installed, the application can be built and programmed from the Simulink workflow. 3.4 FreeMASTER FreeMASTER is used as the runtime monitoring tool during development. It provides visibility into the embedded application while it is running on the S32K144 board. In the Parking Sensors System (PSS) setup, FreeMASTER is used to monitor live ADC samples from the ultrasonic sensors, processed distance values, and selected application variables. This helps during bring-up and validation because the developer can check the behavior of the generated application without adding custom debug code. Note: The FreeMASTER channel is separate from the LIN communication used by the parking node to exchange data with the zonal controller. 3.5 Toolchain Versions The following software components are used for this demo setup: Component Version / Variant MATLAB / Simulink / Stateflow R2024a or newer Embedded Coder Matching MATLAB release ARM Cortex-M support Matching MATLAB release NXP MBDT for S32K1xx 4.3.0 FreeMASTER 3.2 or newer These versions define the reference environment used to build and deploy the parking sensor application.   4 Required Hardware The hardware setup is centered on the S32K144-Q100 evaluation board, which acts as the local parking sensor node. Four MaxBotix MB1020 ultrasonic sensors are connected to the board through analog inputs and control lines. The board also connects to the zonal controller over LIN and to the development PC through the FreeMASTER interface. georgevictor_0-1784704554486.png   Figure 2. Parking Sensor Node Hardware Setup 4.1 NXP S32K144-Q100 Evaluation Board The S32K144-Q100 evaluation board is the target hardware used for the parking sensor node. It provides the microcontroller platform required to run the generated application and includes the peripherals needed by the demo: ADC channels for the ultrasonic sensor outputs, GPIO pins for sensor control, LIN support for communication with the zonal controller, and a debug interface for programming and monitoring. In this setup, the board performs the hardware-side interaction with the sensors and communication interfaces. georgevictor_1-1784704591517.png   Figure 3. S32K144-Q100 Evaluation Board Used for the Parking Sensor Node The board configuration used by the project is summarized below. Setting Value Device S32K144 Package 100-LQFP SRAM size 64 KB External crystal 8 MHz System clock 80 MHz Memory model FLASH Debug interface JTAG The exact configuration is provided by the MBDT configuration block in the Simulink model. 4.2 MaxBotix MB1020 Ultrasonic Sensors The demo uses four MaxBotix MB1020 sensors, also known as LV-MaxSonar-EZ ultrasonic sensors. Each sensor provides an analog voltage output that varies with the measured distance, which makes the device easy to connect to the S32K144 ADC inputs. The sensor also includes an RX pin that can be used as an enable or control input. 4.3 Sensor Wiring and Pin Mapping Each MB1020 sensor is connected to the S32K144-Q100 board using two main signal types. The analog output pin is connected to one ADC input channel, while the RX pin is connected to a GPIO output and can be used by the application to control the sensor. Power and ground are distributed from the evaluation board through the breadboard. The following pin mapping comes from the PSS model connection annotation. Sensor Analog pin to S32K144 RX enable pin to S32K144 SONAR1 — Left AN → PTB2, ADC0_SE6, J2.11 RX → PTA11, J1.2 SONAR2 — Center Left AN → PTB3, ADC0_SE7, J2.9 RX → PTA17, J1.4 SONAR3 — Right AN → PTA0, ADC0_SE9, J5.7 RX → PTD10, J1.6 SONAR4 — Center Right AN → PTA1, ADC0_SE15, J5.5 RX → PTD11, J1.8 Power and ground connections are defined as follows. Signal Connection GND Breadboard black rail → J13.4 on S32K144-Q100 VCC 5 V Breadboard red rail → J3.9 on S32K144-Q100 georgevictor_2-1784704626909.png   Figure 4. Sensor Wiring Between the S32K144-Q100 Board and MB1020 Sensors 4.4 ADC Configuration The MB1020 sensors provide analog voltage outputs, so the S32K144 ADC is used to convert these signals into digital values. In the project setup, ADC0 is configured for software-triggered acquisition and uses the channels assigned to the four ultrasonic sensors. Setting Value ADC instance ADC0 Resolution 12-bit Trigger source Software trigger Voltage reference 5 V / 0 V Used channels ADC0_SE6, ADC0_SE7, ADC0_SE9, ADC0_SE15 Averaging Enabled, 4 samples This section describes only the peripheral setup. The timing of the acquisitions and the conversion from ADC values to distance measurements will be covered in the next article. 4.5 LIN Interface to the Zonal Controller The parking node communicates with the zonal controller using LIN. In this setup, the parking node is configured as a LIN slave, while the zonal controller acts as the LIN master. Setting Value Peripheral LPUART2 in LIN mode Node function Slave Baud rate 19200 bit/s Checksum Enhanced LIN 2.x LIN TX pin PTD7 LIN RX pin PTD6 The physical connection between the parking node and the zonal controller uses LIN and ground lines. Signal Zonal board pin Parking S32K144-Q100 pin LIN J31.8 J11.1 GND J31.2 J11.4 4.6 FreeMASTER Debug Channel FreeMASTER uses a dedicated serial channel that allows the developer to monitor the application on the PC while the parking node continues to communicate with the zonal controller. Setting Value Interface LPUART1 Baud rate 115200 bit/s RX pin PTC6 TX pin PTC7 Usage Runtime monitoring and variable visualization   5 References Developing a Parking Sensor System with Model-Based Design Toolbox Model-Based Design Toolbox for S32K Community Model-Based Design Toolbox for S32K How To NXP Support Package for S32K1xx NXP Model-Based Design Toolbox for S32K1 Toolbox Download NXP S32K144 Reference Manual and S32K144-Q100 evaluation board user guide MaxBotix MB1020 / LV-MaxSonar-EZ1 datasheet MathWorks documentation: MATLAB, Simulink, Stateflow, Embedded Coder, ARM Cortex-M support FreeMASTER Run-Time Debugging Tool   6 Conclusion This article described the software and hardware environment required to build and run the Parking Sensor System. The software side is based on MATLAB, Simulink, Stateflow, NXP MBDT, code generation support, and FreeMASTER. The hardware side uses the S32K144-Q100 evaluation board, four MaxBotix MB1020 ultrasonic sensors, ADC input channels, GPIO control lines, LIN communication, and a dedicated FreeMASTER serial channel. With this environment in place, the PSS model can be built, downloaded to the S32K144 board, monitored in real time, and connected to the zonal demo setup. The next article will move inside the model and explain the application architecture, including the sensor acquisition flow, model structure, distance conversion, and LIN communication behavior.
View full article
    1 Table of Contents • Introduction • Required Software • Required Hardware • References • Conclusion     2 Introduction This article belongs to the Front and Rear Lights series and describes the software and hardware environment used throughout the project. Before looking into signal routing, control logic, or integration aspects, it is important to first understand the tools and platforms that support the development and execution of the front and rear lights application. This article introduces the software components used to develop, configure, and deploy the application, together with the hardware platforms used to demonstrate the lighting functionality. This information provides the foundation needed for the remaining articles in the series. Model-Based Design sits at the center of the workflow. MathWorks tools handle the modeling of the front and rear lighting control logic, the definition of the CAN communication interfaces, and validation across simulation stages. NXP tools then deploy those models to the S32K3 target platform, wiring the generated application to real-time peripherals, LED driver hardware, and lighting feedback signals.     3 Required Software 3.1. Vehicle Network Toolbox Within this workflow, Vehicle Network Toolbox plays a central role in defining, simulating, and validating the CAN interfaces of the front and rear lights module. It brings DBC-driven message definitions directly into Simulink, allowing communication behavior to be tested alongside the control logic long before integration. Every command received from the central controller and every status message sent back to the network is modeled using the exact structure defined in the DBC files, keeping the application perfectly aligned with the vehicle-level specification. Vehicle Network Toolbox is available as an add-on in MATLAB/Simulink, adding support for CAN communication and DBC-based message definitions.   Roxana_Grigore01_0-1784635448020.png   Figure 1 - Vehicle Network Toolbox 3.2. Stateflow Stateflow is used to model the control logic of both lighting modules, translating the CAN commands received from the central controller into concrete lighting actions. Each function is represented as a state machine, where transitions are triggered by incoming signals and internal conditions. This approach keeps the logic structured and readable: activation, deactivation, mode switching, and fault handling are all captured in the same diagram. Stateflow is available as an add-on that can be installed directly from within MATLAB/Simulink, extending the environment with state machine modeling capabilities. Roxana_Grigore01_1-1784635471606.png   Figure 2 - Stateflow 3.3. NXP Model-Based Design Toolbox for S32K3 NXP Model-Based Design Toolbox for S32K3 is the link between the Simulink model and the S32K3 microcontroller. It takes care of generating the code, building it, and running it on the target, turning the lighting model into a real embedded application. Through its peripheral blocks, the model can directly use the resources needed by the front and rear lights modules, such as DIO, CAN, and UART without leaving the Simulink environment. It also connects to the NXP configuration tools and supports FreeMASTER for real-time monitoring, which makes it easy to check how the lighting logic actually behaves on the hardware. Roxana_Grigore01_2-1784635492503.png   Figure 3 - Development flow diagram     4 Required Hardware 4.1. FRDM Automotive S32K312 Development Board (FRDM-A-S32K312) The front and rear lights application runs on the FRDM Automotive S32K312 Development Board, a development platform based on the NXP S32K312 microcontroller. The board provides access to the communication interfaces and processing capabilities of the target device while offering an integrated platform for software development, debugging, and validation activities. Within the scope of this project, the board is used to execute the lighting application and exchange messages with the central controller through the CAN network. Its communication interfaces, debugging connectivity, and expansion capabilities make it suitable for evaluating body electronics use cases and lighting control scenarios. Roxana_Grigore01_3-1784635516304.png   Figure 4 - FRDM Automotive S32K312 Development Board 4.2. CAN analyzer Emulates the central controller when the node is not yet integrated with the full system. It injects the CAN commands defined in the DBC files (turn signals, headlight modes, hazard, brake indication, etc.) and captures the status messages sent back by the module, enabling the CAN interface and control logic to be validated in a controlled and repeatable way. 4.3. Addressable LED Strip The physical lighting output is represented by an addressable LED strip, in which each LED can be controlled individually. This makes it possible to reproduce all the relevant lighting functions on a single strip - turn signals, hazard lights, headlight modes, and brake indication - by assigning different LEDs or groups of LEDs to each function. The result is a clear visual representation of the module's behavior, making it easy to demonstrate how the control logic reacts to incoming CAN commands.     5 References Model-Based Design Toolbox (MBDT) MATLAB® and Simulink® Documentation S32K3 Microcontrollers FRDM Automotive S32K312 Development Board (FRDM-A-S32K312)     6 Conclusion This article described the software and hardware enablement required for the front and rear lights modules. The software environment combines MathWorks modeling and vehicle network capabilities with NXP target support, while the hardware environment brings together the FRDM Automotive S32K312 Development Board, a CAN analyzer, and an addressable LED strip. Together, these elements provide the foundation for modeling, simulation, communication, code generation, deployment, and validation of the lighting application. The next article will focus on the architecture and model description of the front and rear lights modules, including the control logic, CAN interfaces, and overall application structure.
View full article
      1 Table of Contents • Introduction • Overview • Context • References • Conclusion     2 Introduction Virtual vehicles are becoming a common part of modern automotive development, helping teams validate vehicle behavior, driver interaction, and system integration in realistic digital environments before moving to broader physical testing. Virtual vehicle plant model.pngFigure 1. Virtual vehicle plant model The goal of this first article is to present the virtual vehicle system used in the Hello World demo at a high level and establish the context for the articles that follow. The focus here is on what the subsystem is, why it is relevant in the demo, and how Model-Based Design supports its development within the MathWorks and NXP ecosystem.     3 Overview The importance of this subsystem lies not only in its functional role of simulating the vehicle and linking it to a physical zonal architecture, but also in how it demonstrates an efficient model-based workflow. Rather than building separate assets for vehicle behavior, driver interaction, visualization, and hardware communication, the workflow starts from a configurable virtual vehicle model that can be tested, extended, and connected to other parts of the system. The Virtual Vehicle Composer is a MathWorks tool that enables you to create a Simulink vehicle model for system-level testing, software integration testing, and driver-in-the-loop workflows. The generated model can simulate key vehicle functions such as powertrain, steering, braking, and overall vehicle dynamics. Powertrain Blockset and Vehicle Dynamics Blockset provide reference applications and component models that help define and simulate vehicle behavior in more detail. Simulink 3D Animation supports visualization and interaction with 3D environments, helping connect the vehicle model to a more realistic driving experience. This accelerates development in several ways: The vehicle can be configured and built from a structured workflow rather than assembled manually from scratch. The same model can support simulation, software integration, and connection to external hardware. The built-in 3D interface with Unreal Engine helps connect the vehicle behavior to a realistic visual environment. RoadRunner scenes and scenarios can be incorporated into the simulation workflow to create interactive driving scenarios. CAN communication and feedback from the physical setup can be integrated into the Simulink-based system model. The same workflow can be extended to support additional sensing paths, such as radar data generation and off-board processing on NXP radar hardware. This series is intended for: Engineers learning Model-Based Design with MATLAB and Simulink Developers working with NXP automotive processors and microcontrollers Teams building virtual validation and hardware-connected automotive demonstrations Engineers interested in Driver-in-the-Loop workflows Students and researchers studying vehicle architectures, simulation, and embedded integration Anyone interested in a reproducible example of simulation-to-hardware integration using MathWorks tools and NXP platforms Readers will gain a clearer, step-by-step understanding of how a virtual vehicle can be created, integrated into a 3D driving scene, connected to a physical zonal platform, and used as part of a broader model-based development workflow.     4 Context Created with the Virtual Vehicle Composer, the Simulink hybrid electric vehicle (HEV) model is used not only for standalone simulation, but is reused as the common integration point for driver inputs, RoadRunner-based scene interaction, including actor scenarios implemented in RoadRunner, Unreal Engine visualization, CAN communication, and closed-loop feedback from the physical setup. Virtual vehicle system model.pngFigure 2. Virtual vehicle system model In the implemented setup, a driver controls the virtual vehicle through an Xbox-compatible steering wheel and pedals. These inputs are processed by the Simulink model, which updates the vehicle behavior inside a RoadRunner scene rendered through Unreal Engine. At the same time, the virtual vehicle sends key signals such as speed, steering, braking, turn indicators, hazard lights, and beam light commands over CAN to a physical setup that represents an electric vehicle built from multiple NXP reference boards organized in a zonal architecture. The physical platform includes a main node, zonal nodes, and multiple end nodes. These elements receive the simulation-driven commands and reproduce the state of the virtual vehicle in hardware. Communication is bidirectional, so feedback generated by the physical setup can also influence the simulated vehicle. For example, if front or rear parking sensors detect an obstacle, that information can be returned to the virtual vehicle model and used to trigger braking behavior. All major functional aspects of this interaction, including driver input handling, vehicle behavior, signal exchange, and feedback response, are defined in the Simulink model. This supports rapid refinement and validation before deeper integration into the full system. An additional part of the setup extends the virtual vehicle interaction toward sensing and perception workflows. Actor poses from the virtual scene are used to generate a radar cube, which is sent to an NXP S32R45 board that runs a radar processing chain. This expands the role of the virtual vehicle beyond motion and body-domain interaction. It shows how the simulated environment can also stimulate external sensing functions and hardware processing paths as part of the same demo workflow. Virtual Vehicle Highlight.pngFigure 3. Virtual Vehicle highlighted within the demo The virtual vehicle component is highlighted in the architecture diagram from Figure 3 to show its position in the overall project setup and its connection to the driver interface, the 3D environment, the physical zonal platform, and the radar processing path. The next articles in the series will build on this system overview and examine the virtual vehicle in more detail, including the software and hardware environment, the model architecture, the vehicle creation workflow, the driver input options, RoadRunner and Unreal integration, CAN communication, and the final results and challenges observed during development.     5 References The following resources provide useful background for the technologies referenced in this article: MathWorks documentation for Virtual Vehicle Composer MathWorks virtual vehicle documentation and examples MathWorks RoadRunner documentation MathWorks documentation for Unreal Engine simulation with Simulink NXP Model-Based Design Toolbox overview     6 Conclusion The virtual vehicle subsystem provides the foundation for the Hello World demo by supplying a reusable vehicle model that supports simulation, validation, and integration within a model-based workflow. This article established its purpose and position in the overall architecture. In the next articles, we will move from this high-level overview to the practical details of how the subsystem is created, connected, and exercised in the complete demo.
View full article