NXP FTF 2016 - Training Presentations

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP FTF 2016 - Training Presentations

Discussions

Sort by:
Learn how to easily drive powerful three-phase brushless DC (BLDC) motors which require large field effect transistors (FET). This training will cover how to quickly use a three-phase pre-driver IC in order to control a BLDC motor with protection and diagnosis as well as relevant current and voltage measurements for secure, safe, and accurate control. This course will be based on KDS, Processor Expert MCU agnostic analog software component, and complete Freedom development platform including MCU FRDM-KV10Z, 3-phase FET pre-driver expansion board FRDM-GD3000EVB and a power stage accessory board FRDM-PWRSTG1EVB. All participants will receive a free hardware development kit for BLDC motor control applications support.
View full article
Today’s designers are facing ever increasing challenges to protect their intellectual property and products from counterfeiting or unauthorized access. To help customers better understand the solutions offered by NXP, Future’s System Design Center has designed a Secure Access Demo board to showcase the capabilities of the LPC43S57, a microcontroller with integrated security, and the A700X, a tamper resistant secure MCU solution. This class will present an overview of the architecture of a secured system and provide an introduction to the secured elements from NXP. Watch Video Presentation
View full article
About a decade ago, NXP introduced its first generation Near Field Magnetic Induction (NFMI) radio, to help connecting hearing impaired persons with the digital world. Today, besides medical applications, NFMI is also being used in consumer devices to reduce power consumption and not be affected by body tissue absorption. NXP NFMI allows for hearable and wearable devices that can fit inside an ear canal or be worn on the body. Power levels are low enough to run for a week on a single ZnAir battery. Applications include truly wireless earbuds, implantable electronics, body area networks, under water communication devices, and many other low power.
View full article
Trusted Platform Modules (TPMs) are standards based hardware roots of trust with protected key storage. This session covers how QorIQ Trust Architecture primitives can be used as Soft TPM, thereby reducing BOM cost by eliminating a discrete TPM chip.
View full article
With 5G solutions still being in the design phase, NXP delivers RF solutions based to meet the growing data demand. These solutions are called 4.5G and are based on smart combinations of existing 4G and Wi-Fi technology and will enable a high throughput internet connections everywhere on this planet. This lecture will show you the existing 4G and Wi-Fi RF solutions and how they can be utilized for 4.5 G networks and which steps need to be taken to bring these solutions towards the 5G network. Watch Video Presentation
View full article
V2X technology has the potential to drastically reduce road accidents and improve the traffic flow by fusing in-car sensor data with data obtained from other road users and from the surrounding infrastructure - visibly or unvisbily and far beyond the driver's line of sight. Vehicle to cloud data communication provides a pathway for anonymous data collection and dissemination. When the true potential for V2X is realized and it becomes a true part of the vehicle safety system it is vital that the authenticity and security of data are guaranteed. In addition, the vehicle control units that coordinate active stability systems must be protected against external influences that might subvert the mechanisms design. This presentation will explore the various security countermeasures needed to make V2X a safe and secure technology for the future. Watch Video Presentation
View full article
Building on top of 11 years of usage within data centers, Xen Hypervisor is uniquely placed to support a new range of use cases for embedded solutions. In particular, its isolation and security features, flexible virtualization modes and architecture, driver disaggregation, and strong ARM support make it a perfect fit for embedded applications. Artem Mygaiev, GlobalLogic’s Embedded Practice Head, will explore the virtualization nuances and challenges of using Xen Hypervisor for embedded applications through the demonstration of his own company’s journey in developing a platform that leverages Xen for virtual network equipment, IoT, automotive, and other embedded use cases.
View full article
Unified Extensible Firmware Interface (UEFI) provides a standard, modern environment for booting an operating system and running pre-boot applications. UEFI is already extensively used across the server, mobile and embedded market and supports multiple architectures (x86, ARM®) and has support for booting multiple OS (like Windows®, Linux, Mac). This session describes the UEFI bootloader on QorIQ LS series processors (LS1043A board) and how we can migrate from U-Boot bootloader to the UEFI bootloader on the LS processors. This session also showcases how it can be used to boot an CentOS Distribution using GRUB2 bootloader. For loading the CentOS kernel and RFS images we demonstrate PXE boot (Boot over Network) method. So essentially this session showcases a standard chained bootloading architecture which is extensively used to support embedded distributions like CentOS, Ubuntu, ONIE etc. Watch Video Presentation
View full article
NXP’s latest generation of passive UHF RFID, called UCODE® DNA, can be used in Automatic Vehicle Identification (AVI) systems that make it easier to identify – and collect from – drivers of vehicles that aren’t properly registered. In an AVI system for vehicle registration, readers can be installed above, below, or to the side of the road. They can also be embedded in a handheld device, for use by government personnel. The tag, attached to the vehicle, uses the energy produced by the reader’s RF field, so there’s no need for a battery and the tag has a very long lifespan. Cryptography-based security minimizes errors and practically eliminates fraud. Vehicle owners (and fee collectors) can be confident that the right person is being billed, since readings are both highly accurate and highly secure.
View full article
Transport ticketing requirements have evolved significantly over the last years - from transaction security to multi-application needs and the possibility to integrate mobile ticketing to an existing environment. NXP's MIFARE® products have consistently been able to meet these requirements and strongly establish an excellent reputation as the leading contactless solution delivering convenience, flexibility and scalability. Over 1,000 business partners including application developers, service and solution providers, system integrators and card manufacturers make up the open MIFARE community and ecosystem. MIFARE DESFire EV2 is the next-generation of MIFARE ICs with highest security level (EAL5+ Common Criteria certification) for hardware and software. Its enhanced key management makes it the ideal multi-application platform for unlimited applications.
View full article
The I2C bus has expanded from its humble beginnings in 1980s home electronics to both small and large scale systems in the modern world. Applications range from Smartphones to Server farms, and while they're true to the original simple signaling protocol other I2C bus components are needed to expand, adapt or buffer those signals. We take an in depth technical look at the simple Bus Buffer. Often needed, and seldom understood. Watch Video Presentation
View full article
Solid state RF energy provides cooking appliance OEMs the opportunity to create differentiated cooking appliances. When combined with emerging food services, these appliances can enable greater levels of consumer convenience while delivering consistent cooking results. This session will cover the underlying basics of how solid state RF cooking is performed, its benefits, and how it can be combined in an IoT appliance to deliver even further differentiation. Watch Video Presentation
View full article
This session provides an overview of the new opportunities and challenges opened by applying Automotive Ethernet in in-vehicle Networks. We will describe how the NXP portfolio of PHYs and Switches addresses these challenges and outline the new opportunities arising from the combined portfolios after the merger. The presentation will also address ways of using the Automotive Ethernet portfolio in the industrial and automation markets. Watch Video Presentation
View full article
As the Smart Home starts to gather momentum, a number of competing Wireless Communication standards are fighting for dominance. With ZigBee® now becoming dominant in the low-power networking market, there is no surprise that two new low power technology Thread and Bluetooth® Low Energy with the new Mesh capability are both trying to enter this market to get a piece of the cake. Moreover competing IoT platforms from the Thread Group (Google/Nest), Allseen Alliance (Qualcomm), Apple's Homekit, the Open Interconnect Consortium (Intel) and many others are creating even more confusion. So in this confusing array of Wireless Communication standards and Iot platforms, what are the main features of each and what does it means for NXP? This session will provide an overview of these Wireless connectivity standards and IoT platforms, their capabilities, and their implication for NXP IoT. Watch Video Presentation
View full article
This presentation will describe the updates to Crypto Services Engine (CSE) made by NXP, where are they used and how to protect your application. NXP was the first semiconductor vendor to offer a Secure Hardware Extension (SHE) compliant security module on its automotive microcontrollers, the CSE. Since the introduction of the CSE, there have been many enhancements, and extensions of its capability, we will cover additional use cases and device configurations. Watch Video Presentation
View full article
Whether your requirements are size and power, or range and bandwidth, there is a right-sized Wi-Fi solution available now for your i.MX-based processor design! Through partnerships with industry leaders in Wi-Fi technology and module design, NXP can now offer proven Wi-Fi solutions across a range of size, power and performance levels suitable for consumer, automotive, industrial and battery-powered mobile or remote i.MX-based applications. In this session we will cover the latest Wi-Fi protocols, certifications, and interoperability issues for Wi-Fi, as well as the range of wireless LAN solutions now available for use with i.MX applications processors and evaluation boards. Watch Video Presentation
View full article
This hands-on workshop will help you get started with our latest MAC57D5xx processor for instrument cluster and human machine interfaces together with the recent release of MQX. Practical use cases will be demonstrated and exercised during this hands-on workshop session.
View full article
This session will cover a number of topics relevant to all IoT systems and presented because of instructor’s involvement with the IPSO Alliance. The overriding goal of this session is to help prepare you to design your IoT system starting with the device, up to the Cloud and all the other required components. This session describes the IP protocols dedicated to IoT because it helps shape the system capabilities. This demo will use MQTT in conjunction with the Amazon AWS IoT service. IoT systems are made of multiple components. The most visible ones are the Cloud/web tools. In the demo, the activities are structured around the IT services that differentiate products. The Cloud services that will be covered in the session included in addition to data storage rules and actions, web visualization, and analytics. The demo code and Cloud accounts will be available to participants.
View full article
This session will cover the different vision processing capabilities of the S32V234 automotive vision processor with a focus on the Image Sensor Processor (ISP). The presentation will demonstrate how the cost of a vision system can be cut down by using the ISP to accept raw camera input data and to process it using algorithms like debayering, white balancing, format conversion, HDR and de-noising. The aim of the session is to give an introduction to camera processing, to present the architecture of the ISP and to demonstrate how it can be programmed using a visual tool developed by NXP.
View full article
Networking devices use high-speed differential signaling that can exceed 10 Gbps. Circuit design for the transmitter (TX) and receiver (RX) elements in the high speed channel have capabilities of offset signal losses in the PCB and system. This session will review the high-speed signal channel and its characteristics and illustrate how the TX and RX circuits in general are used to offset signal losses. It will also show key characteristics of the channels that are needed to allow these TX and RX circuits to work effectively. This session will also address maximum length of the PCB channel, PCB-specific structures that need to be optimized and the usage of the IBIS-AMI models for 5-10 Gbps operation. Examples of channels from PCB designs at NXP will also be included. Watch Video Presentation
View full article