mcu-s32k144(s32design studio version2.2) data lost from generated flash image file of srec-format

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mcu-s32k144(s32design studio version2.2) data lost from generated flash image file of srec-format

2,443件の閲覧回数
zhou_2020
Contributor I

Dear madam or sir: 

I have created a new software project in s32design studio  version 2.2, using s32k144-mcu without sdk.  output flash image  is configured as motorola's  srec format. 

  I encountered a question about the .ld file and  it generated data。

 The default flash memory is composed of  m_interrupts,m_flash_config and text.

but the m_interrupts and m_flash_config  zone were  lost  in  project's output srec file (pictures shows as below).

 

But when i build the older version  software project which downloaded  from NXP.com,this problem disappeared。 

 

0 件の賞賛
返信
1 返信

2,437件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

Can you attach the project?

When I create a new project in S32DS 2.2 and select Create flash image, the generated srec file is correct.

danielmartynek_0-1603975741956.png

danielmartynek_2-1603975764671.png

danielmartynek_3-1603975772930.png

 

Regards,

Daniel

 

 

0 件の賞賛
返信