S912XEG128J2VAA - which IDE?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S912XEG128J2VAA - which IDE?

4,143 Views
shanep
Contributor I

Hi Team

Which  NXP IDE  do I use for the S912XEG128J2VAA.

I downloaded CodeWarrior for HCS12(X) Microcontrollers v5.2 but cannot find this part (S912XEG128J2VAA) in the list.

On the S912XEG128J2VAA webpage it does point to this V5.2 IDE but no such device is listed,

Any recommendations?

Regards

Shane

0 Kudos
Reply
7 Replies

4,132 Views
shanep
Contributor I

Hi Kef2

 

i do not see that in my list

 

shanep_0-1662449823226.png

 

0 Kudos
Reply

4,126 Views
kef2
Senior Contributor V

Your screenshot is unreadable.

 

Yes, it seems S12XEG128 is missing in CW5.2. 

Add missing derivatives to CW5.2 

0 Kudos
Reply

4,117 Views
shanep
Contributor I

Thank you for this - it is much appreciated!

 

Regards

Shane

0 Kudos
Reply

4,139 Views
kef2
Senior Contributor V

kef2_0-1662387462186.png

 

0 Kudos
Reply

4,074 Views
shanep
Contributor I

Out of interest what version of CW are you using?

0 Kudos
Reply

4,066 Views
kef2
Senior Contributor V

On older machine I have old 5.1 setup, on another one 5.2 with added missing derivatives according to above mentioned instructions, both are OK with missing 5.2 derivatives.

I hope you didn't install to program files. Program files on Windows 10 is too tricky to be compatible with this old IDE.

0 Kudos
Reply

4,047 Views
shanep
Contributor I

Thank you for the info!

0 Kudos
Reply