S912XEG128J2VAA - which IDE?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S912XEG128J2VAA - which IDE?

4,172 Views
shanep
Contributor I

Hi Team

Which  NXP IDE  do I use for the S912XEG128J2VAA.

I downloaded CodeWarrior for HCS12(X) Microcontrollers v5.2 but cannot find this part (S912XEG128J2VAA) in the list.

On the S912XEG128J2VAA webpage it does point to this V5.2 IDE but no such device is listed,

Any recommendations?

Regards

Shane

0 Kudos
Reply
7 Replies

4,161 Views
shanep
Contributor I

Hi Kef2

 

i do not see that in my list

 

shanep_0-1662449823226.png

 

0 Kudos
Reply

4,155 Views
kef2
Senior Contributor V

Your screenshot is unreadable.

 

Yes, it seems S12XEG128 is missing in CW5.2. 

Add missing derivatives to CW5.2 

0 Kudos
Reply

4,146 Views
shanep
Contributor I

Thank you for this - it is much appreciated!

 

Regards

Shane

0 Kudos
Reply

4,168 Views
kef2
Senior Contributor V

kef2_0-1662387462186.png

 

0 Kudos
Reply

4,103 Views
shanep
Contributor I

Out of interest what version of CW are you using?

0 Kudos
Reply

4,095 Views
kef2
Senior Contributor V

On older machine I have old 5.1 setup, on another one 5.2 with added missing derivatives according to above mentioned instructions, both are OK with missing 5.2 derivatives.

I hope you didn't install to program files. Program files on Windows 10 is too tricky to be compatible with this old IDE.

0 Kudos
Reply

4,076 Views
shanep
Contributor I

Thank you for the info!

0 Kudos
Reply