I upload the boot loader to QSPI at address 0 and fip.bin to QSPI at address 0x100000, the probe message is as follow:
NOTICE: Reset status: Power-On Reset NOTICE: BL2: v2.5(release):bsp37.0-2.5 NOTICE: BL2: Built : 16:13:38, Nov 2 2023 Warning: Instruction at BL33_ENTRYPOINT (0xffaa0000) is 0x0, which is not a B or BL! NOTICE: BL2: Booting BL31
Why should upload fip.bin to qspi? and the fip.bin seems can't be booted