Setting higher stack size in MCUxpresso

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Setting higher stack size in MCUxpresso

2,179 Views
db_1017
Contributor I

1. Using  PN7462 kit. and software version PN7462AUPspPackageFull-v05_22_01.

2. From where to set stack size , if need to change it to higher value

Also from where to view stack size usage during debug?

 

MCUXpresso IDE v11.3.0 [Build 5222] [2021-01-11] is used.

Labels (1)
0 Kudos
Reply
1 Reply

2,161 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hello @db_1017 ,

 

Please kindly refer to "17.12.2 LPCXpresso style Heap and Stack" for details. You may find it in the folder of "C:\nxp\MCUXpressoIDE_11.3.0_5222\MCUXpresso_IDE_User_Guide.pdf".

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply