System services have not been validated with this version of GCC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

System services have not been validated with this version of GCC

945件の閲覧回数
db_1017
Contributor I

We are getting few warnings while building code for PN7462 kit. and software version PN7462AUPspPackageFull-v05_22_01.

1.. "System services have not been validated with this version of GCC"  

Is this warning critical and should be corrected or can be ignored?  I tried updating MCUxpresso its latest version : MCUXpresso IDE v11.3.0 [Build 5222] [2021-01-11]

 

2. Here are screenshot of all the warnings 

 

db_1017_0-1613130331042.png

 

3. When i clicked on each warning it took to source code:

db_1017_1-1613130395980.png

 

 

db_1017_2-1613130412258.png

 

 

db_1017_3-1613130425146.png

 

 

db_1017_4-1613130436974.png

 

 

db_1017_5-1613130456045.png

 

 

 

4. What is this "Info" ?

db_1017_6-1613130480898.png

 

 

 

ラベル(1)
0 件の賞賛
返信
1 返信

933件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @db_1017 ,

 

1.. "System services have not been validated with this version of GCC"  

- It is not critical, and you may just ignore it or update the source file as below:

gcc system service issue.png 

and from my side, I just see two warnings, and my IDE is MCUXpresso IDE v11.3.0 [Build 5222] [2021-01-11], is it the same with you?

gcc system service issue 1.png

Basically they are not critical either. The demos are validated before release.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信