Raspberry Pi 3 & OM5577/PN7120 Compatibility

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Raspberry Pi 3 & OM5577/PN7120 Compatibility

ソリューションへジャンプ
5,397件の閲覧回数
cacstech
Contributor I

I'm trying to get my OM5577 installed on my Raspberry Pi 3, and I'm not having any luck with this. After installing the linux image for the OM5577 onto the microSD card and plugging it into my Raspberry PI, the Raspberry Pi does not boot. The documentation for the OM5577 isn't very helpful either. Has anyone been able to get their OM5577 to work with a Raspberry Pi 3?

ラベル(1)
タグ(3)
1 解決策
3,957件の閲覧回数
jeremygeslin
NXP Employee
NXP Employee

Hi,

The updated version with added support for Raspberry Pi 3 model is now available for download from the here: OM5577-PN7120S_Rpi_Linux_demo_v1.1.zip - Box .

Regards,

Jeremy.

元の投稿で解決策を見る

5 返答(返信)
3,957件の閲覧回数
yankospassov
Contributor I

And what about WIndows IoT Insider Preview for Raspberry Pi3?

OM5577 on Raspberry Pi 3 with Windows IoT

3,957件の閲覧回数
craighubbard
Contributor I

We would also like to know about this products support for Win 10 IOT on Raspberry Pi 3.

The OM5577 is shown as supported hardware but appears that it is not from this and other posts.

0 件の賞賛
返信
3,957件の閲覧回数
jeremygeslin
NXP Employee
NXP Employee

Hi,

Indeed, the current OM5577 Raspberry Pi demo image only support previous models.

We are working on providing a new image supporting the new Raspberry Pi 3 model.

It should be published soon.

Regards,

Jeremy.

0 件の賞賛
返信
3,958件の閲覧回数
jeremygeslin
NXP Employee
NXP Employee

Hi,

The updated version with added support for Raspberry Pi 3 model is now available for download from the here: OM5577-PN7120S_Rpi_Linux_demo_v1.1.zip - Box .

Regards,

Jeremy.

3,957件の閲覧回数
cacstech
Contributor I

Hi Jeremy,

Thank you so much for getting me the updated version!

Sincerely,

Steven

0 件の賞賛
返信