Problem with PN7150 NFC Antenna Simulation using RFSim99

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem with PN7150 NFC Antenna Simulation using RFSim99

Jump to solution
8,096 Views
Franz75
Contributor I

Hello,

I read some app. Note for RFID matching and I've followed NFC Antenna Design training in particular part 2.

But my theoretical simulation with RFSim99 doesn't look like what I read on the instrument, I certainly did something wrong, but what?

My steps are:
First I calibrate the VNA with a coaxial cable.

1_20231102_160351.jpg

 

I measure the parameters and resonance frequency of the antenna directly on the dump resistors.

2_20231102_160420.jpg

The parameters read by the VNA are:

antenna nuda SELFRES.jpg

 

L = 1.68uH

R = 6.74Ω

Franz75_0-1698940603689.png

Ca= 1/ ((2*3.14*55.345E6)^2*1.68e-6=4.92pF

 

Franz75_1-1698941107070.png

The simulation:

Franz75_3-1698941344168.png

 

 

But I measured:

 

Franz75_4-1698941401883.png

 

What am I doing wrong?

thanks in advance.

Francesco

 

0 Kudos
Reply
1 Solution
7,990 Views
Tomas_Parizek
NXP Employee
NXP Employee

Hello Francesco, 

 

I tried to simulate your circuit and I can see approx. the same:

Tomas_Parizek_0-1699945477530.png

btw. I always put something like 1.25Ohms in front of the inductors which simulate the inductors and connection losses. 

About your topic, I see the resistance of your antenna is 6.72 Ohms. That is quite a lot. Do you really measure the antenna itself? Or did you include the damping resistors as well? 

 

Once I decreased the Rs of the antenna, the results were more realistic 

Tomas_Parizek_1-1699945685092.png

BR

Tomas 

View solution in original post

4 Replies
7,991 Views
Tomas_Parizek
NXP Employee
NXP Employee

Hello Francesco, 

 

I tried to simulate your circuit and I can see approx. the same:

Tomas_Parizek_0-1699945477530.png

btw. I always put something like 1.25Ohms in front of the inductors which simulate the inductors and connection losses. 

About your topic, I see the resistance of your antenna is 6.72 Ohms. That is quite a lot. Do you really measure the antenna itself? Or did you include the damping resistors as well? 

 

Once I decreased the Rs of the antenna, the results were more realistic 

Tomas_Parizek_1-1699945685092.png

BR

Tomas 

7,966 Views
Franz75
Contributor I

Hi Tomas,
the rs value was actually very high and as you can see from the photograph the dump resistors were not present. but by doing the same things again with the same "instrument" I now read 3 ohm... most likely the small VNA is of poor quality. Now everything works.
Thank you very much

0 Kudos
Reply
7,994 Views
Franz75
Contributor I

Danielchen thank you for your response,
but maybe I explained myself wrong.
The actual circuit was made as NXP specification with ground connected on C0 and C2, but in the simulation the ground is connected only on TX2.
I ran the simulation on the PC then to redo it in practice with the VNA I reproduced just simulated.
My DUT is connected between TX1 and TX2 and capacitors C0 and C2 are NOT at GND and the GND trace was cut to everything else in the circuit.
I look forward to hearing from you.
Thank you

Francesco

 

.

 

0 Kudos
Reply
8,027 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi

 

There is a difference between the real circuit and the simulation,  I would suggest you refer to below link for RFSim99 

https://community.nxp.com/t5/NFC/PN7150-NFC-Antenna-Simulation-using-RFSim99-Simulation-Tool/td-p/14...

 

 

0 Kudos
Reply