Problem with PN7150 NFC Antenna Simulation using RFSim99

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem with PN7150 NFC Antenna Simulation using RFSim99

ソリューションへジャンプ
8,067件の閲覧回数
Franz75
Contributor I

Hello,

I read some app. Note for RFID matching and I've followed NFC Antenna Design training in particular part 2.

But my theoretical simulation with RFSim99 doesn't look like what I read on the instrument, I certainly did something wrong, but what?

My steps are:
First I calibrate the VNA with a coaxial cable.

1_20231102_160351.jpg

 

I measure the parameters and resonance frequency of the antenna directly on the dump resistors.

2_20231102_160420.jpg

The parameters read by the VNA are:

antenna nuda SELFRES.jpg

 

L = 1.68uH

R = 6.74Ω

Franz75_0-1698940603689.png

Ca= 1/ ((2*3.14*55.345E6)^2*1.68e-6=4.92pF

 

Franz75_1-1698941107070.png

The simulation:

Franz75_3-1698941344168.png

 

 

But I measured:

 

Franz75_4-1698941401883.png

 

What am I doing wrong?

thanks in advance.

Francesco

 

0 件の賞賛
返信
1 解決策
7,961件の閲覧回数
Tomas_Parizek
NXP Employee
NXP Employee

Hello Francesco, 

 

I tried to simulate your circuit and I can see approx. the same:

Tomas_Parizek_0-1699945477530.png

btw. I always put something like 1.25Ohms in front of the inductors which simulate the inductors and connection losses. 

About your topic, I see the resistance of your antenna is 6.72 Ohms. That is quite a lot. Do you really measure the antenna itself? Or did you include the damping resistors as well? 

 

Once I decreased the Rs of the antenna, the results were more realistic 

Tomas_Parizek_1-1699945685092.png

BR

Tomas 

元の投稿で解決策を見る

4 返答(返信)
7,962件の閲覧回数
Tomas_Parizek
NXP Employee
NXP Employee

Hello Francesco, 

 

I tried to simulate your circuit and I can see approx. the same:

Tomas_Parizek_0-1699945477530.png

btw. I always put something like 1.25Ohms in front of the inductors which simulate the inductors and connection losses. 

About your topic, I see the resistance of your antenna is 6.72 Ohms. That is quite a lot. Do you really measure the antenna itself? Or did you include the damping resistors as well? 

 

Once I decreased the Rs of the antenna, the results were more realistic 

Tomas_Parizek_1-1699945685092.png

BR

Tomas 

7,937件の閲覧回数
Franz75
Contributor I

Hi Tomas,
the rs value was actually very high and as you can see from the photograph the dump resistors were not present. but by doing the same things again with the same "instrument" I now read 3 ohm... most likely the small VNA is of poor quality. Now everything works.
Thank you very much

0 件の賞賛
返信
7,965件の閲覧回数
Franz75
Contributor I

Danielchen thank you for your response,
but maybe I explained myself wrong.
The actual circuit was made as NXP specification with ground connected on C0 and C2, but in the simulation the ground is connected only on TX2.
I ran the simulation on the PC then to redo it in practice with the VNA I reproduced just simulated.
My DUT is connected between TX1 and TX2 and capacitors C0 and C2 are NOT at GND and the GND trace was cut to everything else in the circuit.
I look forward to hearing from you.
Thank you

Francesco

 

.

 

0 件の賞賛
返信
7,998件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi

 

There is a difference between the real circuit and the simulation,  I would suggest you refer to below link for RFSim99 

https://community.nxp.com/t5/NFC/PN7150-NFC-Antenna-Simulation-using-RFSim99-Simulation-Tool/td-p/14...

 

 

0 件の賞賛
返信