PN7362 Custom Board EEPROM Program using MCUXpresso LPC-LINK2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN7362 Custom Board EEPROM Program using MCUXpresso LPC-LINK2

ソリューションへジャンプ
3,909件の閲覧回数
kashyap_gada
Contributor II

Dear Sir,

We have created custom boards using PN7362 RFID Controller. It is understood from the Quick Start Manual, UM10883, Section 6.9 The EEPROM has to be updated first before using any NXP Examples. The flashing of eeprom bin file is failing for me with error attached.

On the same side, Flash Programming works fine. Output Attached.

 

ラベル(2)
0 件の賞賛
返信
1 解決策
3,886件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hello @kashyap_gada ,

 

Is it possible to provide a snapshot to show how you configure the programming? As I know, the base address should be 0x201200 for EEPROM program.

 

Thanks for your patience!

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,879件の閲覧回数
kashyap_gada
Contributor II

Dear Kan,

Thank for your reply.

I was following UM10883, but I didn't double check the EEPROM Address. I corrected the address and then program ran normally.

Thank you for your prompt reply!!!

Regards

0 件の賞賛
返信
3,887件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hello @kashyap_gada ,

 

Is it possible to provide a snapshot to show how you configure the programming? As I know, the base address should be 0x201200 for EEPROM program.

 

Thanks for your patience!

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信