PN7160

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 
16,834 Views
PatelKrina
Contributor II

PatelKrina_0-1678429994857.pngPatelKrina_1-1678430012147.png

PatelKrina_2-1678430026684.png

PatelKrina_3-1678430038130.png

Hello 

I attached photo for PN7160 Controller Board file 

 is this right placement ? 

I will use NFC section for data reader/write and payload so this placement is right 

 

0 Kudos
Reply
1 Solution
16,813 Views
Tomas_Parizek
NXP Employee
NXP Employee

Dear Patel, 

The EMC Filter (L13 + C87 and L14+C90) is too far from the PN7160 Tx pins. It may cause EMI issues. 

See the correct EMC filter placement (NXP PN7160 development kit).

For more details about the placement of the components, look at this document:https://www.nxp.com/docs/en/application-note/AN12988.pdf

Best Regards

Tomas 

 

View solution in original post

4 Replies
16,733 Views
Tomas_Parizek
NXP Employee
NXP Employee

Hello Patel, 

It looks OK now ! 

Thank you for choosing our product. Do not hesitate to contact us if you need any assistance.

Best Regards

Tomas 

 

 

0 Kudos
Reply
16,814 Views
Tomas_Parizek
NXP Employee
NXP Employee

Dear Patel, 

The EMC Filter (L13 + C87 and L14+C90) is too far from the PN7160 Tx pins. It may cause EMI issues. 

See the correct EMC filter placement (NXP PN7160 development kit).

For more details about the placement of the components, look at this document:https://www.nxp.com/docs/en/application-note/AN12988.pdf

Best Regards

Tomas 

 

16,708 Views
PatelKrina
Contributor II
Hello

I updated placement The EMC Filter (L13 + C87 and L14+C90), it the close PN7160

I attached image
check Reply
0 Kudos
Reply
16,709 Views
PatelKrina
Contributor II

Hello 

I updated placement The EMC Filter (L13 + C87 and L14+C90), it the close PN7160 

I attached image 

0 Kudos
Reply