PN7160

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
16,835件の閲覧回数
PatelKrina
Contributor II

PatelKrina_0-1678429994857.pngPatelKrina_1-1678430012147.png

PatelKrina_2-1678430026684.png

PatelKrina_3-1678430038130.png

Hello 

I attached photo for PN7160 Controller Board file 

 is this right placement ? 

I will use NFC section for data reader/write and payload so this placement is right 

 

0 件の賞賛
返信
1 解決策
16,814件の閲覧回数
Tomas_Parizek
NXP Employee
NXP Employee

Dear Patel, 

The EMC Filter (L13 + C87 and L14+C90) is too far from the PN7160 Tx pins. It may cause EMI issues. 

See the correct EMC filter placement (NXP PN7160 development kit).

For more details about the placement of the components, look at this document:https://www.nxp.com/docs/en/application-note/AN12988.pdf

Best Regards

Tomas 

 

元の投稿で解決策を見る

4 返答(返信)
16,734件の閲覧回数
Tomas_Parizek
NXP Employee
NXP Employee

Hello Patel, 

It looks OK now ! 

Thank you for choosing our product. Do not hesitate to contact us if you need any assistance.

Best Regards

Tomas 

 

 

0 件の賞賛
返信
16,815件の閲覧回数
Tomas_Parizek
NXP Employee
NXP Employee

Dear Patel, 

The EMC Filter (L13 + C87 and L14+C90) is too far from the PN7160 Tx pins. It may cause EMI issues. 

See the correct EMC filter placement (NXP PN7160 development kit).

For more details about the placement of the components, look at this document:https://www.nxp.com/docs/en/application-note/AN12988.pdf

Best Regards

Tomas 

 

16,709件の閲覧回数
PatelKrina
Contributor II
Hello

I updated placement The EMC Filter (L13 + C87 and L14+C90), it the close PN7160

I attached image
check Reply
0 件の賞賛
返信
16,710件の閲覧回数
PatelKrina
Contributor II

Hello 

I updated placement The EMC Filter (L13 + C87 and L14+C90), it the close PN7160 

I attached image 

0 件の賞賛
返信