PN7150 OOB Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,258件の閲覧回数
Karyliu
Contributor II

Hi NXP,

Does PN7150 support pairing BLE devices through NFC OOB (out of band) in andoird?

Thank you.

 

0 件の賞賛
返信
1 解決策
1,254件の閲覧回数
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @Karyliu

Hope you are doing well.

Please consider that PN7150 is Not Recommended for New Designs; we recommend using PN7160 instead.

Out Of Band through NFC requires to distribute the keys through a specific NDEF structure, which is defined by NFC Forum. PN7150 would be able to read the pairing information from an NFC tag and provide it to the BLE device.

On the other side, PN7150 supports Card Emulation (from host), which should allow to expose the OOB data via the NDEF content by emulating an NFC Forum Type 4 Tag.

Regards,
Eduardo.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,255件の閲覧回数
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @Karyliu

Hope you are doing well.

Please consider that PN7150 is Not Recommended for New Designs; we recommend using PN7160 instead.

Out Of Band through NFC requires to distribute the keys through a specific NDEF structure, which is defined by NFC Forum. PN7150 would be able to read the pairing information from an NFC tag and provide it to the BLE device.

On the other side, PN7150 supports Card Emulation (from host), which should allow to expose the OOB data via the NDEF content by emulating an NFC Forum Type 4 Tag.

Regards,
Eduardo.

0 件の賞賛
返信