Reading ISO 14443 B' and SRT512

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reading ISO 14443 B' and SRT512

2,186 Views
benoîtdenis
Contributor I

 I am able to read ISO 14443 A and B cards but for a project I have to read ISO 14443 B' (B prime) tags and SRT 512 tags.
NXP sent me a scrypt to read ISO A4443B' tags but i cannot make it work.
For SRT512 tags they are supposed to work as ISO 14443 B but my NFC_Detect(); command doesn't detect the tag.
Attached the functions in C i use and the scrypt NXP sent me.
I can also send the entire LPC Xpresso project if needed.

 

Thank you for your help

Original Attachment has been moved to: TypeBprime_reader.jcf.zip

Original Attachment has been moved to: Bprime.c.zip

0 Kudos
2 Replies

1,154 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Benoît DENIS,

I am checking with our AE team for your issue, and will let you know when I have any more information.

Thanks for your patience!

Have a great day,
Kan Li

0 Kudos

1,154 Views
benoîtdenis
Contributor I

Hi Kan_Li,

Thank you for your answer. ISO 14443B' is also known as INNOVATRON. I have the right datasheet from Calypso specifications but i am not able to detect such a card, before sending the ATTRIB command.

Thank you for your help,

Regards

Benoît DENIS

0 Kudos