PN532 error 0x0B - RF protocol error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN532 error 0x0B - RF protocol error

1,806件の閲覧回数
gustaf
Contributor I

Hi,

Is there any good explanation for the error code "0x0b"? One of our PN532's, while communicating with a Mifare FOB, is returning 0x0b and 0x06. The communication looks to be working fine for a couple of communications but after a couple of seconds, we see a bunch of these errors.

I should mention that we are toggling the RF field on and off every 50 ms unless there is a communication ongoing.

 

0 件の賞賛
返信
1 返信

1,799件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hello @gustaf ,

 

I am not sure how you test , did the card stay on the antenna whenever RF is on/off? maybe there is some noise during the RF on, you may try to delay the polling a little bit longer after RF on. 

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信