NHS3152 not powering on over NFC while running demo applications or custom code

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

NHS3152 not powering on over NFC while running demo applications or custom code

跳至解决方案
2,134 次查看
acuom
Contributor III

I have been using the NHS3152 dev boards to prototype for a project and while I am able to flash and run my code while it is connected to my laptop (and transmit data over NFC onto my android phone), it stops working as soon as I disconnect from the laptop.

This behaviour is observed with my own code running on the board and the demo applications supplied. I have already disabled semi hosting. The Blinky application runs (as in debugger shows it is running) but the LED doesn't light up.

Basically, as soon as I disconnect the board, it is no longer recognised by my phone (even though the phone recognises other passive tags). I also connected a source meter to monitor the voltage between Vdd and GND and it falls to 0 even with the NFC field present.

Is the board beyond rescue or can some sort of reset help?

标记 (2)
0 项奖励
回复
1 解答
2,113 次查看
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Did you order the dev board from local distributor? If yes. You may try to Dev Tool Warranty Return Request Form as the link.
URL:https://www.nxp.com/support/sample-and-buy/buy-direct/dev-tool-warranty-return-request-form:WTB_DTD_...

 

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,069 次查看
acuom
Contributor III

Thank you for this. Will follow it up with them!

0 项奖励
回复
2,114 次查看
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Did you order the dev board from local distributor? If yes. You may try to Dev Tool Warranty Return Request Form as the link.
URL:https://www.nxp.com/support/sample-and-buy/buy-direct/dev-tool-warranty-return-request-form:WTB_DTD_...

 

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 项奖励
回复