NFC tag

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NFC tag

7,403件の閲覧回数
Vilgot
Contributor I

 

I have some nfc tags right now witch I am trying to get WiFi to but it’s not going to well and I need some advice on what do do?

I have the TagWriter app but don’t know what to put on authentication and encryption and if there could be something wrong with my WiFi cause I feel like I have tried all the options 

0 件の賞賛
返信
6 返答(返信)

7,384件の閲覧回数
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @Vilgot

Hope you are doing well.

The Authentication Type and Encryption Type will depend on the characteristics defined by your Wi-Fi Access Point and it is something you may need to check in its configuration.

If your device is within the Wi-Fi range, TagWriter should list the network under "Available Wifi Networks", and those fields should be filled by default.

Regards,
Eduardo.

0 件の賞賛
返信

7,378件の閲覧回数
Vilgot
Contributor I
Hi Eduardo
Thanks for Your reply but I am still not getting it to work.
I feel like I’m getting the right info into the nfc but it’s never worked just putting my phone on the nfc tag for WiFi.
It’s has worked with other functions but not with WiFi.
Because if I haven’t gotten it wrong I understand that I shouldn’t need any applications to get the WiFi on the nfc.
Do you have any idea of what the problem is ?
And also it would be easier if I could send a video of it not working, is this possible? Maybe on another platform?
Thank you/ Vilgot
0 件の賞賛
返信

7,336件の閲覧回数
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello,

Could you please provide more details on your setup?

What is the tag you are using for the test? What is the mobile device you are using to read de tag with the WiFi credentials? 

If needed, you can attach the files to your post.

Regards,
Eduardo.

0 件の賞賛
返信

7,295件の閲覧回数
Vilgot
Contributor I

Hello 

this is the info  I get if I use the NFC TagInfo app

0 件の賞賛
返信

7,309件の閲覧回数
Vilgot
Contributor I

Hello

Im using an iPhone 13 and have tags from a small company called chipster and they are named NTAG213-tagg  

the picture I put in files shows the tags I have, well I have three of them but they are all called the same thing so I think they are the sam but just different amounts of storage and size 

0 件の賞賛
返信

7,275件の閲覧回数
EduardoZamora
NXP TechSupport
NXP TechSupport

Hi,

Application launch after reading a tag may have some limitations or restrictions in iOS devices. I will recommend you redirecting your inquiry to the corresponding iOS support documentation and forums.

I apologize for the inconvenience.

Regards,
Eduardo.

0 件の賞賛
返信