NFC TagWriter fails in programming NTAG 413 DNA

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

NFC TagWriter fails in programming NTAG 413 DNA

跳至解决方案
2,074 次查看
stefano_dellava
Contributor II

Hi, I'm having problems programming an NTAG 413 DNA using the Android app TagWriter.
Programming the UID mirror is working properly. Programming the UID plus the Counter works, but adding the SDM field does not work.

The problem seems to me caused by the wrong calculation of the offset where the app has to write the SDM field.

my set is as follows:


URL type: https://
URL: productid.info?uid=0000000000000000x000000x0000000000000000000000
UID offset: 26
Counter offset: 41
SDM MAC offset input: 47
SDM MAC offset: 7

The problem is that the app do not allow to change the SDM MAC offset value and 7 is clearly wrong.

Please help. Stefano

标记 (1)
0 项奖励
回复
1 解答
1,742 次查看
stefano_dellava
Contributor II

Hi Kan_Li, upgraded the app, now it works. Thank for the suggestion.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,742 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Stefano,

I am sorry, but are you using the latest TagWriter App? The version on my hands works fine and doesn't require input the offset data, just click to select the options. Please kindly clarify. and URL info should start with something like https://www.nxp.com .

Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,743 次查看
stefano_dellava
Contributor II

Hi Kan_Li, upgraded the app, now it works. Thank for the suggestion.

0 项奖励
回复