NFC TagWriter fails in programming NTAG 413 DNA

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NFC TagWriter fails in programming NTAG 413 DNA

ソリューションへジャンプ
2,666件の閲覧回数
stefano_dellava
Contributor II

Hi, I'm having problems programming an NTAG 413 DNA using the Android app TagWriter.
Programming the UID mirror is working properly. Programming the UID plus the Counter works, but adding the SDM field does not work.

The problem seems to me caused by the wrong calculation of the offset where the app has to write the SDM field.

my set is as follows:


URL type: https://
URL: productid.info?uid=0000000000000000x000000x0000000000000000000000
UID offset: 26
Counter offset: 41
SDM MAC offset input: 47
SDM MAC offset: 7

The problem is that the app do not allow to change the SDM MAC offset value and 7 is clearly wrong.

Please help. Stefano

タグ(1)
0 件の賞賛
返信
1 解決策
2,334件の閲覧回数
stefano_dellava
Contributor II

Hi Kan_Li, upgraded the app, now it works. Thank for the suggestion.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,334件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Stefano,

I am sorry, but are you using the latest TagWriter App? The version on my hands works fine and doesn't require input the offset data, just click to select the options. Please kindly clarify. and URL info should start with something like https://www.nxp.com .

Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,335件の閲覧回数
stefano_dellava
Contributor II

Hi Kan_Li, upgraded the app, now it works. Thank for the suggestion.

0 件の賞賛
返信