MFRC522 Multiple SPI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MFRC522 Multiple SPI

跳至解决方案
3,399 次查看
kita
Contributor I

#MFRC522  Multi SPI

Connect SPI communication (MISO / MOSI / SCK / SS) with the microcomputer
I would like to do multi-control,
When multiple units are connected,
Even if you select the device you want to communicate with the SS terminal,
Other If the MISO port of the device is output "Low"
If the selected MISO output level goes down and the communication
It will not be possible.

Is MFRC 522 supported only 1: 1 SPI?

标记 (1)
0 项奖励
回复
1 解答
3,181 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Yes, MFRC522 supports only one SPI interface.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,182 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Yes, MFRC522 supports only one SPI interface.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
3,181 次查看
kita
Contributor I

Hello,

Thank you for answering.

◆When MFRC 522 is used in 1 (Master): N (Slave)
I plan to communicate by switching the SS terminal and MISO port to the device I want to communicate with.
Is there not a problem?

※N (Slave) unit MOSI / SCK / RST ports share.

◆Does MFRC-630 support 1 (Master): N (Slave) communication?

Best Regards,

Kan_Li

0 项奖励
回复