How to generate Hardware interrupt to wake MCU from deep power down when the card is detected?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to generate Hardware interrupt to wake MCU from deep power down when the card is detected?

跳至解决方案
2,623 次查看
mahendrasondaga
Contributor III

Hello freaks,

I'm dealing with the battery  operated NFC based application and i need to conserve the battery as much as i can.

For the card R/W and P2P mode I'm using PN7150. I know about it's Low power card detection mode (LPCD) to significantly reduced power consumption but i also need to put my Host processor in Deep power down and need to wake-up when the card enters in filed (just like NT3H1101 FD pin and PN532 P70_IRQ)  can any one guide me here

Thanks

0 项奖励
回复
1 解答
2,260 次查看
IvanRuiz
NXP Employee
NXP Employee
0 项奖励
回复
2 回复数
2,261 次查看
IvanRuiz
NXP Employee
NXP Employee
0 项奖励
回复
2,260 次查看
mahendrasondaga
Contributor III

Hello there ..
I'm eagerly waiting for the support from nxp community...
can any one help me here

0 项奖励
回复