How to generate Hardware interrupt to wake MCU from deep power down when the card is detected?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to generate Hardware interrupt to wake MCU from deep power down when the card is detected?

ソリューションへジャンプ
2,664件の閲覧回数
mahendrasondaga
Contributor III

Hello freaks,

I'm dealing with the battery  operated NFC based application and i need to conserve the battery as much as i can.

For the card R/W and P2P mode I'm using PN7150. I know about it's Low power card detection mode (LPCD) to significantly reduced power consumption but i also need to put my Host processor in Deep power down and need to wake-up when the card enters in filed (just like NT3H1101 FD pin and PN532 P70_IRQ)  can any one guide me here

Thanks

0 件の賞賛
返信
1 解決策
2,301件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee
0 件の賞賛
返信
2 返答(返信)
2,302件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee
0 件の賞賛
返信
2,301件の閲覧回数
mahendrasondaga
Contributor III

Hello there ..
I'm eagerly waiting for the support from nxp community...
can any one help me here

0 件の賞賛
返信