How can I upload a chip coding into the NFC chips (NHS3152 or NHS3152 UK) without PCB-LPC-Link2?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can I upload a chip coding into the NFC chips (NHS3152 or NHS3152 UK) without PCB-LPC-Link2?

1,207 Views
jihunpark
Contributor I

I bought NFC chips (NHS3152 and NHS3152UK) for the demonstration of IoT. For the demo PCB based on NHS 3152 (such as, NHS3152 General Starter Kit), the chip coding can be uploaded using LPC-Link2.

But, I need to use the NFC chips, not demo PCBs. If so how can I upload a chip coding to the NFC chips (NHS3152 or NHS3152 UK) without PCB-LPC-Link2?

0 Kudos
Reply
1 Reply

1,004 Views
driesmoors
NXP Employee
NXP Employee

Hi,

Please have a look AN_NHS31xx_Flashing.pdf, available in the SDK under the docs folder. It describes the different ways to load firmware into the chip. Any wired approach will make use of the LPC-Link2 board, but we also provide a one-time wireless download using the NFC interface and an Android APP or a PC-based Python script.

Best,
Dries.

0 Kudos
Reply