How can I upload a chip coding into the NFC chips (NHS3152 or NHS3152 UK) without PCB-LPC-Link2?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How can I upload a chip coding into the NFC chips (NHS3152 or NHS3152 UK) without PCB-LPC-Link2?

1,269 次查看
jihunpark
Contributor I

I bought NFC chips (NHS3152 and NHS3152UK) for the demonstration of IoT. For the demo PCB based on NHS 3152 (such as, NHS3152 General Starter Kit), the chip coding can be uploaded using LPC-Link2.

But, I need to use the NFC chips, not demo PCBs. If so how can I upload a chip coding to the NFC chips (NHS3152 or NHS3152 UK) without PCB-LPC-Link2?

0 项奖励
回复
1 回复

1,066 次查看
driesmoors
NXP Employee
NXP Employee

Hi,

Please have a look AN_NHS31xx_Flashing.pdf, available in the SDK under the docs folder. It describes the different ways to load firmware into the chip. Any wired approach will make use of the LPC-Link2 board, but we also provide a one-time wireless download using the NFC interface and an Android APP or a PC-based Python script.

Best,
Dries.

0 项奖励
回复