HCE T4T (pn5180) without multi-thread?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

HCE T4T (pn5180) without multi-thread?

跳至解决方案
3,211 次查看
ldw
Contributor I

Hello.
In an environment that doesn't use multithreading, I want to implement all the features provided by Ex8_HCE_T4T.

I tried to simply process the contents of the functions (TApplication,TReaderLibrary) provided as example code as a loop, but it failed. (I think it is because the message exchange is not handled.)

Please give a hint if there is a way I can try next.
Or I want to know about the information I can refer to.

Thank you.

标签 (1)
标记 (4)
0 项奖励
回复
1 解答
3,144 次查看
nxf58474
NXP Employee
NXP Employee

Hi,

 

Hope you are doing well. Unfortunately this example is only implemented in FreeRTOS, and there is not documentation available for use in NullOS.

 

Sorry for the inconveniences this might cause you.

 

Regards,

Ricardo

在原帖中查看解决方案

2 回复数
3,145 次查看
nxf58474
NXP Employee
NXP Employee

Hi,

 

Hope you are doing well. Unfortunately this example is only implemented in FreeRTOS, and there is not documentation available for use in NullOS.

 

Sorry for the inconveniences this might cause you.

 

Regards,

Ricardo

2,679 次查看
jr_hernandez
Contributor II

Hi,

I understand there is no documetation available for HCE with NullOs. But I would like to know if there is any chance HCE can work with NullOs implementation.

Regards, Ramon

0 项奖励
回复