HCE T4T (pn5180) without multi-thread?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HCE T4T (pn5180) without multi-thread?

Jump to solution
3,203 Views
ldw
Contributor I

Hello.
In an environment that doesn't use multithreading, I want to implement all the features provided by Ex8_HCE_T4T.

I tried to simply process the contents of the functions (TApplication,TReaderLibrary) provided as example code as a loop, but it failed. (I think it is because the message exchange is not handled.)

Please give a hint if there is a way I can try next.
Or I want to know about the information I can refer to.

Thank you.

Labels (1)
0 Kudos
Reply
1 Solution
3,136 Views
nxf58474
NXP Employee
NXP Employee

Hi,

 

Hope you are doing well. Unfortunately this example is only implemented in FreeRTOS, and there is not documentation available for use in NullOS.

 

Sorry for the inconveniences this might cause you.

 

Regards,

Ricardo

View solution in original post

2 Replies
3,137 Views
nxf58474
NXP Employee
NXP Employee

Hi,

 

Hope you are doing well. Unfortunately this example is only implemented in FreeRTOS, and there is not documentation available for use in NullOS.

 

Sorry for the inconveniences this might cause you.

 

Regards,

Ricardo

2,671 Views
jr_hernandez
Contributor II

Hi,

I understand there is no documetation available for HCE with NullOs. But I would like to know if there is any chance HCE can work with NullOs implementation.

Regards, Ramon

0 Kudos
Reply