HCE T4T (pn5180) without multi-thread?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HCE T4T (pn5180) without multi-thread?

ソリューションへジャンプ
3,213件の閲覧回数
ldw
Contributor I

Hello.
In an environment that doesn't use multithreading, I want to implement all the features provided by Ex8_HCE_T4T.

I tried to simply process the contents of the functions (TApplication,TReaderLibrary) provided as example code as a loop, but it failed. (I think it is because the message exchange is not handled.)

Please give a hint if there is a way I can try next.
Or I want to know about the information I can refer to.

Thank you.

ラベル(1)
タグ(4)
0 件の賞賛
返信
1 解決策
3,146件の閲覧回数
nxf58474
NXP Employee
NXP Employee

Hi,

 

Hope you are doing well. Unfortunately this example is only implemented in FreeRTOS, and there is not documentation available for use in NullOS.

 

Sorry for the inconveniences this might cause you.

 

Regards,

Ricardo

元の投稿で解決策を見る

2 返答(返信)
3,147件の閲覧回数
nxf58474
NXP Employee
NXP Employee

Hi,

 

Hope you are doing well. Unfortunately this example is only implemented in FreeRTOS, and there is not documentation available for use in NullOS.

 

Sorry for the inconveniences this might cause you.

 

Regards,

Ricardo

2,681件の閲覧回数
jr_hernandez
Contributor II

Hi,

I understand there is no documetation available for HCE with NullOs. But I would like to know if there is any chance HCE can work with NullOs implementation.

Regards, Ramon

0 件の賞賛
返信