Does Ucode8 support self-serialization?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does Ucode8 support self-serialization?

2,744件の閲覧回数
davide1
Contributor I

Hello - We have a customer which has been using Ucode7 RFID tags for some time in a self-serialization workflow. However, when they tried to use Ucode8 tags in the same capacity, the EPCs always seems to encode as a "0" (see attached). Can anyone here confirm or deny if self-serialization (may "auto-serialization" is the correct term) is supported with the Ucode8 tags? I see that the memory mapping is a bit different on the chips but it looks like there should still be enough room for our 96-bit EPC.

The customer is using Impinj ItemEncode 2.4.3.240, but when I asked Impinj, they were under the impression that the tags themselves performed the serialization, not the encoders. 

Thanks in advance all for your help!

0 件の賞賛
返信
1 返信

2,673件の閲覧回数
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Dear David Endahl,

Hope you are doing great, pre-serialization means that  NXP pre program the TID and mirror that into the EPC memory this is usually how we deliver products, we are not 100% sure what you mean by "auto-serialization", the only main difference that comes right to my minds is the parallel encoding.

BR

Jonathan

0 件の賞賛
返信