Does Ucode8 support self-serialization?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does Ucode8 support self-serialization?

2,720 Views
davide1
Contributor I

Hello - We have a customer which has been using Ucode7 RFID tags for some time in a self-serialization workflow. However, when they tried to use Ucode8 tags in the same capacity, the EPCs always seems to encode as a "0" (see attached). Can anyone here confirm or deny if self-serialization (may "auto-serialization" is the correct term) is supported with the Ucode8 tags? I see that the memory mapping is a bit different on the chips but it looks like there should still be enough room for our 96-bit EPC.

The customer is using Impinj ItemEncode 2.4.3.240, but when I asked Impinj, they were under the impression that the tags themselves performed the serialization, not the encoders. 

Thanks in advance all for your help!

0 Kudos
Reply
1 Reply

2,649 Views
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Dear David Endahl,

Hope you are doing great, pre-serialization means that  NXP pre program the TID and mirror that into the EPC memory this is usually how we deliver products, we are not 100% sure what you mean by "auto-serialization", the only main difference that comes right to my minds is the parallel encoding.

BR

Jonathan

0 Kudos
Reply