Decryption of SDMENCFileData is incorrect about NTAG424DNA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Decryption of SDMENCFileData is incorrect about NTAG424DNA

4,226 Views
long19890829
Contributor II
Hi,
   I have a trouble in decryption of SDMENCFileData, I could get the same data with the Table 4 of 4.4.3.2 Decryption of SDMENCFileData of AN12196, while when I write the demo url = https://my424dna.com/?picc_data=00000000000000000000000000000000&enc=7878787878787878787878787878787... into the tag,enable the mirror feature, and read the tag,I got the new url = https://my424dna.com/?picc_data=E704C53A168DCD09F9E9A86D93BA3037&enc=570296360EBE9656E25A734840C5439.... After the same decryption process, and I get the decryption SDMENCFileData = 37383738373837383738373837383738, which is not equal raw enc=78787878787878787878787878787878, and is the ASCII format. Even I transform the data "37383738373837383738373837383738" into ASCII format "7878787878787878", it only 8 byte length and only the half of the raw enc. Below is my computational process and tag setting, could you help me work out the problem.

Original Demo URL:

Read URL from Tag:

My computational process:

Step

Command

Data Message

1

SDMENCFileData

570296360EBE9656E25A734840C5439F

2

SDMMetaReadKey

’00000000000000000000000000000000

3

SDMFileReadKey

‘00000000000000000000000000000000

4

PICCData

E704C53A168DCD09F9E9A86D93BA3037

5

decrypt UID and counter

UID=0454a292766380; counter=010000

Session Key generation

6

SV1 =C33C 0001 0080 [UID] [SDMReadCtr] [ZeroPadding]

c33c000100800454a292766380010000

7

KSesSDMFileReadENC

cb7b614e2c69e0663bea3135d9dcbe0e

8

IVe = E(KSesSDMFileReadENC; SDMReadCtr || ZeroPadding)

1bdbda6eacb46add1c8a5dae7d526434

9

D(KSesSDMFileReadENC, IVe, SDMENCFileData)

37383738373837383738373837383738

Tag Setting:

tag_setting01.jpg

Thanks!

ZhuLong

Tags (1)
0 Kudos
Reply
3 Replies

3,792 Views
vijayhues
Contributor I

Were you able to resolve this issue? I'm running into the same issue and the steps mentioned in the application note & data sheet don't help. The example value provided in the application note works fine though. Any inputs?

0 Kudos
Reply

4,104 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Long,

How did you write to the tag for the Mirroring features? I may try to reproduce this issue here.

pastedImage_1.png

Thanks for your patience!

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

4,103 Views
long19890829
Contributor II

Hi Kan,

  Thanks for your reply, please refer to the attachment for tag writting log, and my concern is that why the plaintext(after decryption) of SDMENCFileData is ASCII format, and only the half of the raw data.  

  Thanks!

  Long

0 Kudos
Reply