CLRC663 imbalanced RXN and RXP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CLRC663 imbalanced RXN and RXP

2,011件の閲覧回数
tomkuestersteff
Contributor I

I have a design using CLRC66303 (CLRC663+).  Our antenna design and interface follows the schematic and guidelines in the datasheet, app notes and webinars.  We have achieved acceptable results, but have noticed that the signal amplitude at RXN and RXP are not symmetrical even though the entire TX and RX path have symmetrical components.  With NFC field on, I see signal level of 0.124V - 1.672V (1.548 VPP) at RXN and only 0.376V - 1.420V (1.044 VPP) at RXP.

Is this to be expected?  Is the input impedance of RXN and RXP imbalanced?

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 返信

1,900件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

I think it is related with the PCB layout. The Rx input has a quite high impedance, and the Tx signal is strong, so I have seen a lot of cross talking between Tx and Rx. That might happen on one side more than on the other side.

Have a great day,
Kan

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信