CLRC663 PDOWN pin spec.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CLRC663 PDOWN pin spec.

ソリューションへジャンプ
1,685件の閲覧回数
watanabe_daigo
Contributor I

Hello!

Can I use VIH(High Level input voltage)/VIL(Low Level input voltage) described in the CLRC663 datasheet as the PDOWN pin specification? The datasheet does not show it clearly. 

with best regards,

dee 

ラベル(1)
0 件の賞賛
返信
1 解決策
1,512件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Dee,

Here is the specification of CLRC663 PDOWN pin:

PDOWN                                                                             min                       typ                                       max      

VIL         low-level input voltage                                0                            0                                           0.4

VIH        high-level input voltage                               0.6 x PVDD          VDD(PVDD)                           VDD(PVDD)


Hope that helps,
Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,513件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Dee,

Here is the specification of CLRC663 PDOWN pin:

PDOWN                                                                             min                       typ                                       max      

VIL         low-level input voltage                                0                            0                                           0.4

VIH        high-level input voltage                               0.6 x PVDD          VDD(PVDD)                           VDD(PVDD)


Hope that helps,
Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信