CLRC663 PDOWN pin spec.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CLRC663 PDOWN pin spec.

Jump to solution
1,698 Views
watanabe_daigo
Contributor I

Hello!

Can I use VIH(High Level input voltage)/VIL(Low Level input voltage) described in the CLRC663 datasheet as the PDOWN pin specification? The datasheet does not show it clearly. 

with best regards,

dee 

Labels (1)
0 Kudos
Reply
1 Solution
1,525 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Dee,

Here is the specification of CLRC663 PDOWN pin:

PDOWN                                                                             min                       typ                                       max      

VIL         low-level input voltage                                0                            0                                           0.4

VIH        high-level input voltage                               0.6 x PVDD          VDD(PVDD)                           VDD(PVDD)


Hope that helps,
Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,526 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Dee,

Here is the specification of CLRC663 PDOWN pin:

PDOWN                                                                             min                       typ                                       max      

VIL         low-level input voltage                                0                            0                                           0.4

VIH        high-level input voltage                               0.6 x PVDD          VDD(PVDD)                           VDD(PVDD)


Hope that helps,
Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply