Hi Jorge:
- Is the board getting programmed? I mean, can you run the debug session without errors?
Yes, I could, even I could measure MOSI signal while SPI module is driven.
I checked the project compile and setting, debug setting, all seems fine.
actually I have LPC1769 LPCXpresso-LPC1769-CMSIS-DAP board on hand, same issues while debug.
- What do you see in the console output when running the application?
while run DEBUG_PRINTF("\nReader chip RC663: 0x%02x\n", bDataBuffer[0]);
the version always return : 0x00
- What LPCXpresso IDE version you have? (I use LPCXpresso v8.1.4)
I test on IDE 8.1.4, and latest 8.2.2,
NFC library is CLEV663B-LPC1769_NFC-Reader-Library-v3.092_0 and latest sw297839 NFC-Reader-Library-V4040050011646.
So I think which is not related with SW package and IDE, what next step should I test on board? or what step maybe I missed?