Automate PN7462 programming

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Automate PN7462 programming

Jump to solution
2,680 Views
bojankoce
Contributor I

Hello, guys.

We have a plan to implement PN7462 RFID reader SoC into our future device. We are considering the possibilities of remote/automated code update of PN7462 module. 

If we have PN7462 connected with Raspberry Pi over USB, can we use RESET and DWL_REQ pins of PN7462 to set it into download mode so that we can send new flash files from RPi by using some .sh script, for example?

Thanks in advance for your time and efforts.

Sincerely,

Bojan.

0 Kudos
Reply
1 Solution
2,639 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @bojankoce ,

 

Yes, it is possible. Please kindly refer to 8.10 in https://www.nxp.com/docs/en/user-guide/UM10883.pdf for more details.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
2,640 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @bojankoce ,

 

Yes, it is possible. Please kindly refer to 8.10 in https://www.nxp.com/docs/en/user-guide/UM10883.pdf for more details.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
2,660 Views
bojankoce
Contributor I

Any feedback on this?

0 Kudos
Reply