Automate PN7462 programming

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Automate PN7462 programming

ソリューションへジャンプ
2,732件の閲覧回数
bojankoce
Contributor I

Hello, guys.

We have a plan to implement PN7462 RFID reader SoC into our future device. We are considering the possibilities of remote/automated code update of PN7462 module. 

If we have PN7462 connected with Raspberry Pi over USB, can we use RESET and DWL_REQ pins of PN7462 to set it into download mode so that we can send new flash files from RPi by using some .sh script, for example?

Thanks in advance for your time and efforts.

Sincerely,

Bojan.

0 件の賞賛
返信
1 解決策
2,691件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @bojankoce ,

 

Yes, it is possible. Please kindly refer to 8.10 in https://www.nxp.com/docs/en/user-guide/UM10883.pdf for more details.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,692件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @bojankoce ,

 

Yes, it is possible. Please kindly refer to 8.10 in https://www.nxp.com/docs/en/user-guide/UM10883.pdf for more details.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
2,712件の閲覧回数
bojankoce
Contributor I

Any feedback on this?

0 件の賞賛
返信