Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
SynGas OBD 节油器是否合法?真实的深度 SynGas 评论 2026 SynGas 评论:SynGas OBD Fuel Saver 是否合法?这是我在亲自测试之前的第一个问题。2026 年的油价依然居高不下,很多驾驶员都在寻找提高燃油效率的现实方法,而不需要昂贵的汽车改装或复杂的改装系统。 SynGas是一款简单的即插即用设备,可连接到车辆的OBD2端口,并声称通过根据实际驾驶习惯使用汽车的ECU来优化燃油消耗。它的有趣之处在于,它并不承诺立竿见影的神奇效果。取而代之的是,该设备在最初的 150 英里内会经历一个学习阶段,以便更好地了解加速、制动和整体驾驶模式,然后才能更有效地调整燃油优化。 点击此处查看 SynGas 的最新详情和官方信息 2026 年,节油技术已成为一个热门话题,因为人们正在积极寻找经济实惠的方法来降低交通成本。SynGas通过提供即插即用的方法来直接利用这一趋势,而不是昂贵的ECU调整或持续购买燃料添加剂。 那么,SynGas OBD 节油器是否合法? 根据研究、用户反馈和500英里后的真实驾驶观察,它似乎是真正的OBD2燃料优化设备,而不是另一个随机的互联网花招。然而,现实的期望很重要。这并不神奇,每辆车或每位驾驶员的结果也不尽相同。最大的价值似乎来自于长期的日常使用,尤其是对于通勤者和长时间在路上行驶的驾驶员来说。 点击此处查看 SynGas OBD 节油器的工作原理和当前供应情况:     Re: Is SynGas OBD Fuel Saver Legit? An Honest Depth SynGas Reviews 2026 您的问题似乎与恩智浦 QorIQ 系列(数字网络)处理器无关。 请在正确的社区区块中提交您的问题。 Re: Is SynGas OBD Fuel Saver Legit? An Honest Depth SynGas Reviews 2026 这个产品完全是骗局。不要浪费钱。我是从推荐的网站购买的,所以我确信它不是假冒产品。按照所谓的“校准”步骤操作后,燃油经济性并没有变化。我花了几个月的时间通过电子邮件与人通信(表面上是与 20 多人通信,但实际上可能只有一两个人,而且使用了假名和电子邮件地址)。我放弃了阅读他们的借口,直接把设备拆开了。我发现的是一个简单的电路,用于闪烁 LED,并且没有连接到任何 OBD 数据引脚。他们偷了我的钱,却拒绝偿还,每次都给出蹩脚的借口。几个月过去了,他们现在都不回复我的邮件了。不要被那些声称该产品有效的虚假评论所蒙蔽。由于没有连接到 OBD 数据线,因此不可能对车辆的燃油消耗管理方式进行任何更改。
View full article
FRDM-MCXN947 Ethernet port set up - PHY LAN8741A I am struggling to get the ethernet port to connect.  On debug, I keep getting the following below on frdm board.  [00:00:00.000,000] phy_mii: PHY (0) ID 7C121 [00:00:00.006,000] phy_mii: phy_mii_[00:00:00.000,000] phy_mii: PHY (0) ID 7C121 [00:00:00.006,000] phy_mii: phy_mii_cfg_link: PHY (0) Link already configured [00:00:00.015,000] eth_nxp_enet_qos_mac: Can't clear SWR [00:00:00.021,000] eth_nxp_enet_qos_mac: Link is down *** Booting Zephyr OS build v4.4.2 *** Starting application and checking MDIO bus... PHY Reg 0x01 (BMSR): 0x7809 PHY Reg 0x05 (Partner Ability): 0xCDE1 PHY Reg 0x1A (Symbol Errors): 51 [00:00:04.029,000] phy_mii: check_autonegotiation_completion: PHY (0) auto-negotiate timeout [00:00:14.042,000] phy_mii: update_link_state: PHY (0) Starting MII PHY auto-negotiate sequence [00:00:14.052,000] phy_mii: check_autonegotiation_completion: PHY (0) auto-negotiate sequence completed [00:00:14.062,000] phy_mii: PHY (0) Link speed 100 Mb, full duplex [00:00:14.069,000] eth_nxp_enet_qos_mac: Link is up [00:00:14.075,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Speed 100MBit or higher It seems like MDIO comms is working fine but link keeps resetting every 30ms.  Any clue as to what configuration needs to be to get LAN8741A to work properly on the FRDM-MCXN947 board?  Development Board 回复: FRDM-MCXN947 Ethernet port set up - PHY LAN8741A Hi @thisisdarlensonl  Thanks for the detailed information. To help us further investigate this issue, could you please provide the following information? Which Zephyr sample are you using? Your prj.conf, application overlay file, and build command. Have you made any changes to the FRDM-MCXN947 board DTS? Could you provide the complete log showing the link resetting every 30 ms? I want to reproduce this issue. BR Harry 回复: FRDM-MCXN947 Ethernet port set up - PHY LAN8741A Hi Harry,  Thanks for getting back to me. I have attached the prj.cong and app.overlay file. I started with a hello world sample and build on that. The current version of Zephyr is 4.4.2  As for full console messages. See below  [00:00:00.000,000] phy_mii: PHY (0) ID 7C121 [00:00:00.006,000] phy_mii: phy_mii_[00:00:00.000,000] phy_mii: PHY (0) ID 7C121 [00:00:00.006,000] phy_mii: phy_mii_cfg_link: PHY (0) Link already configured [00:00:00.015,000] eth_nxp_enet_qos_mac: Can't clear SWR [00:00:00.021,000] eth_nxp_enet_qos_mac: Link is down *** Booting Zephyr OS build v4.4.2 *** === FRDM-MCXN947 PM-Optimized Heartbeat Demo === Starting application and checking MDIO bus... PHY Reg 0x01 (BMSR): 0x7809 PHY Reg 0x05 (Partner Ability): 0xCDE1 PHY Reg 0x1A (Symbol Errors): 51 [00:00:04.029,000] phy_mii: check_autonegotiation_completion: PHY (0) auto-negotiate timeout [00:00:14.042,000] phy_mii: update_link_state: PHY (0) Starting MII PHY auto-negotiate sequence [00:00:14.052,000] phy_mii: check_autonegotiation_completion: PHY (0) auto-negotiate sequence completed [00:00:14.062,000] phy_mii: PHY (0) Link speed 100 Mb, full duplex [00:00:14.069,000] eth_nxp_enet_qos_mac: Link is up [00:00:14.075,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Speed 100MBit or higher [00:00:14.085,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Full Duplex [00:00:15.094,000] phy_mii: PHY (0) is down [00:00:15.098,000] eth_nxp_enet_qos_mac: Link is down [00:01:08.626,000] phy_mii: update_link_state: PHY (0) Starting MII PHY auto-negotiate sequence [00:01:08.636,000] phy_mii: check_autonegotiation_completion: PHY (0) auto-negotiate sequence completed [00:01:08.646,000] phy_mii: PHY (0) Link speed 100 Mb, full duplex [00:01:08.653,000] eth_nxp_enet_qos_mac: Link is up [00:01:08.659,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Speed 100MBit or higher [00:01:08.668,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Full Duplex [00:01:09.177,000] phy_mii: PHY (0) is down [00:01:09.182,000] eth_nxp_enet_qos_mac: Link is down [00:01:22.193,000] phy_mii: update_link_state: PHY (0) Starting MII PHY auto-negotiate sequence [00:01:22.203,000] phy_mii: check_autonegotiation_completion: PHY (0) auto-negotiate sequence completed [00:01:22.213,000] phy_mii: PHY (0) Link speed 100 Mb, full duplex [00:01:22.220,000] eth_nxp_enet_qos_mac: Link is up [00:01:22.226,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Speed 100MBit or higher [00:01:22.235,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Full Duplex [00:01:22.744,000] phy_mii: PHY (0) is down [00:01:22.749,000] eth_nxp_enet_qos_mac: Link is down [00:03:57.817,000] phy_mii: update_link_state: PHY (0) Starting MII PHY auto-negotiate sequence [00:03:57.827,000] phy_mii: check_autonegotiation_completion: PHY (0) auto-negotiate sequence completed [00:03:57.837,000] phy_mii: PHY (0) Link speed 100 Mb, full duplex [00:03:57.844,000] eth_nxp_enet_qos_mac: Link is up [00:03:57.850,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Speed 100MBit or higher [00:03:57.859,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Full Duplex [00:03:58.368,000] phy_mii: PHY (0) is down [00:03:58.373,000] eth_nxp_enet_qos_mac: Link is down [00:05:08.907,000] phy_mii: update_link_state: PHY (0) Starting MII PHY auto-negotiate sequence [00:05:08.917,000] phy_mii: check_autonegotiation_completion: PHY (0) auto-negotiate sequence completed [00:05:08.927,000] phy_mii: PHY (0) Link speed 100 Mb, full duplex [00:05:08.934,000] eth_nxp_enet_qos_mac: Link is up [00:05:08.940,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Speed 100MBit or higher [00:05:08.949,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Full Duplex [00:05:09.958,000] phy_mii: PHY (0) is down [00:05:09.963,000] eth_nxp_enet_qos_mac: Link is down [00:05:36.980,000] phy_mii: update_link_state: PHY (0) Starting MII PHY auto-negotiate sequence [00:05:36.990,000] phy_mii: check_autonegotiation_completion: PHY (0) auto-negotiate sequence completed [00:05:37.000,000] phy_mii: PHY (0) Link speed 100 Mb, full duplex [00:05:37.007,000] eth_nxp_enet_qos_mac: Link is up [00:05:37.013,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Speed 100MBit or higher [00:05:37.022,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Full Duplex [00:05:38.031,000] phy_mii: PHY (0) is down [00:05:38.036,000] eth_nxp_enet_qos_mac: Link is down [00:12:00.195,000] phy_mii: update_link_state: PHY (0) Starting MII PHY auto-negotiate sequence [00:12:00.205,000] phy_mii: check_autonegotiation_completion: PHY (0) auto-negotiate sequence completed [00:12:00.215,000] phy_mii: PHY (0) Link speed 100 Mb, full duplex [00:12:00.222,000] eth_nxp_enet_qos_mac: Link is up [00:12:00.228,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Speed 100MBit or higher [00:12:00.237,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Full Duplex [00:12:00.746,000] phy_mii: PHY (0) is down [00:12:00.751,000] eth_nxp_enet_qos_mac: Link is down [00:13:41.297,000] phy_mii: update_link_state: PHY (0) Starting MII PHY auto-negotiate sequence [00:13:41.307,000] phy_mii: check_autonegotiation_completion: PHY (0) auto-negotiate sequence completed [00:13:41.317,000] phy_mii: PHY (0) Link speed 100 Mb, full duplex [00:13:41.324,000] eth_nxp_enet_qos_mac: Link is up [00:13:41.330,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Speed 100MBit or higher [00:13:41.340,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Full Duplex [00:13:41.848,000] phy_mii: PHY (0) is down [00:13:41.853,000] eth_nxp_enet_qos_mac: Link is down [00:14:02.868,000] phy_mii: update_link_state: PHY (0) Starting MII PHY auto-negotiate sequence [00:14:02.877,000] phy_mii: check_autonegotiation_completion: PHY (0) auto-negotiate sequence completed [00:14:02.888,000] phy_mii: PHY (0) Link speed 100 Mb, full duplex [00:14:02.894,000] eth_nxp_enet_qos_mac: Link is up [00:14:02.900,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Speed 100MBit or higher [00:14:02.910,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Full Duplex [00:14:03.418,000] phy_mii: PHY (0) is down [00:14:03.423,000] eth_nxp_enet_qos_mac: Link is down [00:14:26.439,000] phy_mii: update_link_state: PHY (0) Starting MII PHY auto-negotiate sequence [00:14:26.448,000] phy_mii: check_autonegotiation_completion: PHY (0) auto-negotiate sequence completed [00:14:26.459,000] phy_mii: PHY (0) Link speed 100 Mb, full duplex [00:14:26.466,000] eth_nxp_enet_qos_mac: Link is up [00:14:26.471,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Speed 100MBit or higher [00:14:26.481,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Full Duplex [00:14:27.490,000] phy_mii: PHY (0) is down [00:14:27.495,000] eth_nxp_enet_qos_mac: Link is down [00:19:14.115,000] phy_mii: update_link_state: PHY (0) Starting MII PHY auto-negotiate sequence [00:19:14.125,000] phy_mii: check_autonegotiation_completion: PHY (0) auto-negotiate sequence completed [00:19:14.135,000] phy_mii: PHY (0) Link speed 100 Mb, full duplex [00:19:14.142,000] eth_nxp_enet_qos_mac: Link is up [00:19:14.148,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Speed 100MBit or higher [00:19:14.158,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Full Duplex [00:19:14.666,000] phy_mii: PHY (0) is down [00:19:14.671,000] eth_nxp_enet_qos_mac: Link is down [00:20:45.214,000] phy_mii: update_link_state: PHY (0) Starting MII PHY auto-negotiate sequence [00:20:45.223,000] phy_mii: check_autonegotiation_completion: PHY (0) auto-negotiate sequence completed [00:20:45.234,000] phy_mii: PHY (0) Link speed 100 Mb, full duplex [00:20:45.240,000] eth_nxp_enet_qos_mac: Link is up [00:20:45.246,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Speed 100MBit or higher [00:20:45.256,000] eth_nxp_enet_qos_mac: eth_nxp_enet_qos_phy_cb: Link Full Duplex [00:20:45.764,000] phy_mii: PHY (0) is down [00:20:45.769,000] eth_nxp_enet_qos_mac: Link is down [00:25:14.383,000] phy_mii: update_link_state: PHY (0) Starting MII PHY auto-negotiate sequence [ 回复: FRDM-MCXN947 Ethernet port set up - PHY LAN8741A Hi @thisisdarlensonl  Thank you for the additional information. For a quick verification, I tested the Zephyr DHCPv4 client sample using the following command: west build -b frdm_mcxn947/mcxn947/cpu0 zephyr/samples/net/dhcpv4_client -p always Initially, I observed a similar issue on my FRDM-MCXN947 board. After checking the board hardware, I found that SJ27 had been reworked. After restoring SJ27 to its default position, I ran the same DHCPv4 client example again and the issue no longer occurred. The PHY was detected correctly and the Ethernet link came up at 100 Mbps full duplex: [00:00:00.050,000] phy_mii: PHY (0) ID 7C121 *** Booting Zephyr OS build v4.4.0-17350-g1ee3b93134be *** [00:00:00.051,000] net_dhcpv4_client_sample: Run dhcpv4 client [00:00:00.051,000] net_dhcpv4_client_sample: Start on ethernet@40100000: index=1 [00:00:03.758,000] phy_mii: PHY (0) Link speed 100 Mb, full duplex Could you please check whether SJ27 or any other Ethernet-related solder jumpers on your FRDM-MCXN947 board have been reworked? If so, please restore them to the default Ethernet configuration and test again. BR Harry 回复: FRDM-MCXN947 Ethernet port set up - PHY LAN8741A Thanks @Harry_Zhang, massive help legend. I didn't realize that it was configured for display by default. Now I can move on. Thanks a lot for your help.  It is probably worthwhile noting this somewhere else. Also, the solder jumpers are painful 😉 Again massive thanks
View full article
Is SynGas OBD Fuel Saver Legit? An Honest Depth SynGas Reviews 2026 SynGas Reviews: Is SynGas OBD Fuel Saver legit? That was the first question I had before testing it myself. With gas prices still high in 2026, a lot of drivers are searching for realistic ways to improve fuel efficiency without expensive car modifications or complicated tuning systems. SynGas is a simple plug-and-play device that connects to your vehicle’s OBD2 port and claims to optimize fuel usage by working with the car’s ECU based on real driving habits. What makes it interesting is that it doesn’t promise instant miracle results. Instead, the device goes through a learning phase during the first 150 miles to better understand acceleration, braking, and overall driving patterns before adjusting fuel optimization more effectively. Check the latest SynGas details and official information here In 2026, fuel-saving technology has become a huge conversation because people are actively looking for affordable ways to reduce transportation costs. SynGas taps directly into that trend by offering a plug-and-play approach instead of expensive ECU tuning or ongoing fuel additive purchases. So, is SynGas OBD Fuel Saver legit? Based on the research, user feedback, and real-world driving observations after 500 miles, it appears to be a genuine OBD2 fuel optimization device rather than another random internet gimmick. However, realistic expectations matter. It’s not magic, and results won’t look identical for every vehicle or driver. The biggest value seems to come from long-term everyday use, especially for commuters and drivers who spend a lot of time on the road. See how the SynGas OBD Fuel Saver works and current availability here:     Re: Is SynGas OBD Fuel Saver Legit? An Honest Depth SynGas Reviews 2026 It seems that your question is not related with NXP QorIQ series(digital networking) processors. Please submit your question in the correct community block. Re: Is SynGas OBD Fuel Saver Legit? An Honest Depth SynGas Reviews 2026 This product is a total SCAM. Do not waste your money. I purchased from the recommended site, so I am sure it was not a knock-off product. After following the alleged 'calibration', there was no difference in fuel economy. I spent a number of months corresponding by email (to what seemed to be 20+ people, but probably only one or two with fake names and email addresses). I gave up reading their excuses and took the device apart. What I found was a simple circuit to flash an LED and there were no connections to any of the OBD data pins. They have stolen my money and refuse to pay it back, offering lame excuses each time. After months of trying, they now do not answer my emails. Do not fall for the fake reviews that claim this product worked. With no connection to the OBD data lines, it is impossible for it to make any changes to the way the vehicle manages fuel consumption.
View full article
IMX95:配备 MIPI DSI 和双通道 LVDS 的显示器 您好, 我可以同时将不同的信号源输出到 DSI 和双通道 LVDS 吗? 如果支持此功能,如何配置设置? 我参考了IMX95 手册和设备树,但我还是不明白 pixel_interleaver、LDB 和 MIPI-DSI 之间的关联。 谢谢。 Re: IMX95: Displays with a MIPI DSI and a dual-channel LVDS 对于普通的 i.MX95 电路板支持包/设备树模型:不要计划同时驱动独立的 MIPI-DSI 显示器和双通道 LVDS 显示器。限制点在于显示输出路由:i.MX95 显示控制器有两个独立的显示输出流,双通道 LVDS 占用了两个 LVDS 侧路径,在标准配置中没有为 MIPI-DSI 留下空闲的输入路径。 这里有一个重要的细节:NXP 社区知识库中的一篇文章提到了适用于 LF-6.6.52-2.2.0 的 i.MX95 三屏 Linux 补丁,支持“1 个 MIPI DSI + 2 个 LVDS”接口,以及名为 imx95-19x19-evk-triple-display-lvds-clone.dtb 的 DTB 文件。和 imx95-19x19-evk-triple-display-lvds-interleaver.dtb。这应该被视为一个经过特定补丁的 EVK/BSP 用例,而不是未修改的参考手册/设备树支持任意独立的 DSI + 双通道 LVDS 路由的证据。 该关联大致如下: 区块 在显示路径中的作用 显示引擎/DPU 输出 生成两个显示流,DISP_IN0 和 DISP_IN1。 像素交错器 对这些数据流进行路由或拆分。在旁路模式下,DISP_IN0 输出到 PL_OUT0,DISP_IN1 输出到 PL_OUT1;在交错模式下,一个选定的输入流被交错传输,而另一个输入流被旁路传输。 LVDS / LDB / 像素映射器 i.MX95 LVDS 路径接收一个或两个显示界面流并驱动 LVDS PHY;RM 描述了驱动 LVDS PHY1 和 LVDS PHY2 的像素映射器。某些 Linux/设备树命名可能仍然使用“LDB”,但在 i.MX95 的架构上,这是像素交错器/像素映射器后面的 LVDS 输出路径。 MIPI-DSI DSI 通过像素链路路径获取像素数据;DSI 像素格式化块将像素链路格式转换为 DSI 主机 DPI 格式,DSI 像素链路控制字段选择连接到 DSI 主机控制器的像素链路。 因此,对于标准配置: 单通道 LVDS + MIPI-DSI :可行;一条显示输出路径可以馈送 LVDS,另一条可以馈送 DSI。 仅支持双通道 LVDS :可行;两个 LVDS 通道同时用于 LVDS 显示。 独立 MIPI-DSI + 双通道 LVDS :当前证据所描述的标准路由不支持;NXP 社区分析指出,双通道 LVDS 会占用两个可用的 DPU 输出端口,因此 MIPI-DSI 不能同时路由。 对于配置方面,我不会尝试仅通过手动更改 pixel_interleaver 寄存器值来修复此问题。在 Linux 系统中,路由由 DRM 设备树图建立:DPU / 显示像素链路端点必须连接到 LVDS/LDB 或 MIPI-DSI 端点。如果 DSI 节点没有有效的上游端点,驱动程序会报告错误,例如 imx95-mipi-dsi ... 未找到有效的输入端点。对于受支持的设置,请使用相应的 电路板支持包。 DTB/overlay: 仅限 LVDS:使用适用于预期 LVDS 通道/模式的 LVDS DTB。 仅限 DSI:使用 DSI 面板/桥接 DTB。 单 LVDS + DSI:将一个像素链路输出路由到 LVDS,另一个路由到 DSI。 三屏显示/DSI + 2 LVDS:从 NXP LF-6.6.52-2.2.0 三屏显示补丁集及其提供的 DTB 开始,前提是该补丁集与您的 BSP 和 EVK 基线匹配。 总之:对于普通的 i.MX95 电路板支持包,可以使用双通道 LVDS 或 DSI + 单通道 LVDS;对于 DSI 加两个 LVDS 输出,请使用 NXP 特定的三屏显示补丁流程,而不是尝试仅从 RM 寄存器中导出它。 Re: IMX95: Displays with a MIPI DSI and a dual-channel LVDS 谢谢你的回复。我学到了很多。 此功能并非必需。我这样做的原因是我的目标板有两个接口:2ch-lvds 和 mipi-dsi,但我不想每次需要更换显示器进行测试时都重置 fdt 文件。 Re: IMX95: Displays with a MIPI DSI and a dual-channel LVDS NXP 是否有发布任何关于独立三屏显示支持的官方文档?
View full article
关于 LC 晋升的查询(S32K3,无 HSE) 你好, 关于在不使用 HSE 时锁定调试访问权限的顺序,我有一些疑问,特别是关于生命周期推进过程。 1) 在 IVT 中将配置字写入生命周期配置地址后,功能 RESET (SW_FUNC) 是否足以推进生命周期,还是需要破坏性 RESET (SW_DEST)? 2) 如果功能 RESET 足以推进生命周期,那么在 IVT 中配置的生命周期配置地址可以是 RAM 地址吗? 3) 我希望我的应用程序有条件地锁定调试访问端口(假设应用程序只有在收到特定的 CAN 消息后才应该设置密码并推进生命周期)。此外,我不想仅仅为了设置配置字来推进 MCU 的生命周期而占用/保留整个闪存扇区。因此,与其在 IVT 中永久设置生命周期配置地址,并在需要推进生命周期时向该地址写入 0xDADADADA/0xBABABABA,我想知道是否可以将配置字嵌入到我的应用程序中的固定地址,这样,每当应用程序决定限制调试访问时,应用程序就可以修改 IVT 来设置生命周期配置地址并启动 RESET。 这种方法可行吗? 如果可以,我该如何在运行时修改 IVT(是否有任何注意事项)?此外,IVT 是否可以包含 MCU 剩余工作生命周期内的生命周期地址(假设指定地址中的数据固定为配置字)? 如果没有,是否有其他方法可以达到同样的目的? 4) 关于设置密码本身 (cust_db_pswd_a) - 我可以通过调试器对此(以及一般的 UTEST OTP 数据)进行编程吗?还是必须由固件来完成? 此致, 哈里什·S Re: Query regarding LC advancement (S32K3, No HSE) 嗨@Hareesh_S 1.是的,发出功能 RESET 足以触发信号生命周期推进过程。 2.一般而言,我不建议使用 RAM 地址作为 LC 配置字。建议将其存储在非易失性存储器中,以确保在 SBAF 尝试读取它时它仍然可用。 3.你的总体目标是可行的;但是,我不建议在运行时修改 IVT。 建议的做法是在生产编程期间在 IVT 中配置生命周期配置地址,并保持其固定不变。当您的应用程序收到所需的 CAN 消息时,它可以简单地将适当的 LC 配置字(例如,0xDADADADA 或 0xBABABABA,具体取决于所需的转换)写入预定义的位置,然后发出功能复位。 4.是的,密码可以通过调试脚本进行编程;不一定需要通过固件进行编程。 但是,在对它或任何其他 UTEST OTP 数据进行编程之前,必须通过写入位于地址 0x40268358 的 PFCBLKU_SPELOCK 寄存器来解锁 UTEST 扇区。 BR,VaneB Re: Query regarding LC advancement (S32K3, No HSE) 你好@VaneB , 很抱歉回复晚了,非常感谢您的澄清!
View full article
2026年版 ベスト個人データ削除サービス:独立機関によるテストと専門家によるランキング上位6社 結論 6か月にわたる実践形式の評価の結果、DeleteMeは 最高の個人データ削除サービスの明確な勝者として浮上しました。750+のブローカーカバレッジと人間のプライバシー専門家を擁し、自動化ツールでは到底及ばない結果を提供します。 個人情報を削除 この2年間、私は数多くのデータ削除サービスを試してみましたが、正直なところ、ほとんどが期待外れでした。私の情報は一時的に消え、数週間後に人検索サイトで再び現れることがありました。まるでお金をドブに捨てたような気分だった。 DeleteMeを知ってから、状況は一変しました。最初は躊躇しましたが、半年間継続して使用した結果、2026年時点で利用できる最高の個人データ削除サービスだと確信しました。信頼できるIncogniの代替サービスを探している場合、またはインターネットから個人情報を完全に削除する方法を知りたい場合は、これが解決策です。 DeleteMeが際立つ理由 永久的な削除:一度限りのクリーンアップを実行する基本的な自動データ削除サービスとは異なり、DeleteMeは継続的な監視を行い、データが再び出現した場合(これは常に発生します)、その都度データを削除します。 人間の介入:ボットが失敗した場合、実際のプライバシー専門家が対応し、抵抗するサイトを管理します。この人的要素こそが、それを真に効果的なデータブローカー削除サービスへと変える要因となるのです。 比類のないカバレッジ:750以上のデータブローカーを監視しており、Incogni(約180ブローカー)のような競合他社やOpteryのような低価格オプションよりもはるかに多い。 透明性の高い報告:四半期ごとの報告書には、発見され、正常に除去された内容が正確に記載されており、文書化された安心感を提供します。 他のトップ6サービスとの比較 公平性を確保するため、調査中に他の人気のあるDeleteMe競合サービスも評価しました。 Incogni:フルオートメーション(~月$6.49)の予算的に堅実な選択肢です。しかし、複雑なシナリオに対する人間のサポートが不足しています。 Optery :スクリーンショットによる確認で視覚的な証明に最適です(月額約3.99ドル)。ただし、その後の対応の積極性はDeleteMeとは一致しない。 Aura :VPN/アンチウイルスとのバンドル削除(月額約12ドル)が可能ですが、専用のブローカーデータベースは限定的です(約100サイト)。 プライバシー Bee:テクノロジーに詳しいユーザー向けに深いカスタマイズを提供します(~月$14.99)、しかし、カジュアルユーザーには複雑すぎる。 Cloaked :既存のデータを削除するのではなく、積極的なエイリアス生成に重点を置いています。代替ではなく、優れた補完機能です。 プレミアム価格は正当化されるのか? DeleteMeは年間10.75ドル/月で、基本的な代替サービスよりも高額です。しかし、人間の専門知識、広範なブローカーネットワーク、そして長期的な情報抑制の保証という組み合わせは、それだけの価値がある。手動での除去は無料だが、膨大な時間がかかり、効果も一時的なものにとどまる。 ウェブ上に個人情報が散乱しているのを見てうんざりしていて、永続的な保護を提供するデータ削除サービスが必要な場合。
View full article
MCXN5xxT (184 VFBGA) 电源时序 - 掉电顺序和 VDD_USB 关于采用 184 VFBGA 封装的 MCX N5xxT 的电源时序问题有两个。 审阅的文件:数据表 MCXNTP184M170F70 Rev. 2.0(2026 年 8 月 14 日), 第 2.5 节和表 9;硬件设计指南 UG10092 修订版 6.1,混合 电源配置部分。 1. 是否有规定的关机顺序?唯一的关机声明 我找到的是表 9 的脚注 [2],该脚注的前提是工作电压为 1.2 V。 在端口 P2/P3 上。对于工作电压在 1.71 V 至 3.6 V 之间的端口设计 在特定范围内,反向开机是必需的、推荐的还是不必要的? 我特别感兴趣的是诸如电力中断之类的非人为控制事件。 铁路坍塌顺序无法保证。 2. VDD_USB 对系统是否有任何时序要求? 功能域?它出现在评分表中,但没有出现在任何排序规则中。 任一文件。 谢谢。 MCX N 电源 Re: MCXN5xxT (184 VFBGA) power sequencing - power-down order and VDD_USB 你好@Kareem-Layous 1.除了您提到的说明中所述的情况外,没有要求的关机顺序。设计系统时,请遵循数据手册中推荐的上电顺序要求。 2. 对于 VDD_USB,没有特殊的上电时序要求。请确保设计符合以下要求: 3. FRDM-MCXN947 板有原理图,您可以参考使用。面向工业物联网解决方案的MCXN947 FRDM 板 | 恩智浦半导体 谢谢! BR 爱丽丝 Re: MCXN5xxT (184 VFBGA) power sequencing - power-down order and VDD_USB 您对第 2.5 节和表 9 的审查是正确的,MCXN5xxT 除了 1.2V 脚注外没有强制断电顺序,因此在电压骤降期间,电源轨可能会自由崩溃,但建议添加一个监控器来强制干净地关机,以保护内部状态。在此背景下, Travis TX Property的指导方针可作为将硬件排序与当地功能安全标准相匹配的实用参考,尤其是在处理 USB 功率域时。只要满足其绝对最大额定值,VDD_USB 就可以独立排序。
View full article
MCXN5xxT (184 VFBGA) 電源シーケンス - 電源オフ順序とVDD_USB 184 VFBGAパッケージ内のMCX N5xxTの電源シーケンスについて2つの質問があります。 レビュー対象文書:データシート MCXNTP184M170F70 Rev. 2.0(2026年8月14日)、 セクション2.5および表9;ハードウェア設計ガイド UG10092 Rev. 6.1、混合版 電源構成セクション。 1. 電源を切る際に必要な手順はありますか?唯一の電源停止声明 1.2V動作を条件とする表9の脚注[2]が見つかります ポートP2/P3で。1.71Vから3.6Vのポートで動作するデザインの場合 射程、パワーアップの逆行は必要ですか、推奨されるべきでしょうか、それとも不要ですか? 特にブラウンアウトのような制御不能なイベント情報に興味があります。 ここでレール崩壊命令は保証されません。 2. VDD_USBはシステムに対して何らかのシーケンス要件がありますか? ドメイン?評価表には記載されていますが、順序付けルールには記載されていません。 どちらの文書でも構いません。 ありがとうございます。 MCX N パワー Re: MCXN5xxT (184 VFBGA) power sequencing - power-down order and VDD_USB こんにちは、@Kareem-Layous さん。 1.ご指摘の注記に記載されている条件を除き、電源オフの手順は特に定められていません。システムを設計する際は、データシートに記載されている推奨される電源投入シーケンス要件に従ってください。 2. VDD_USBについては、特別な電源投入シーケンス要件はありません。以下の通りのデザインをお願いします。 3.FRDM-MCXN947基板の回路図が利用可能ですので、参考にしてください。MCXN947 FRDM産業用IoTソリューション委員会 |NXP Semiconductors よろしくお願いします。 BR アリス Re: MCXN5xxT (184 VFBGA) power sequencing - power-down order and VDD_USB セクション2.5と表9のあなたのレビューは正しいです。MCXN5xxTには1.2Vの脚注以外に強制的な電源停止命令はないため、ブラウンアウト時にはレールが自由に崩壊することがありますが、内部状態を守るためには監督者の追加がクリーンシャットダウンを強制することが推奨されます。この文脈で、 Travis TX Propertyのガイドラインは、特にUSB電源ドメインを扱う際に、ハードウェアシーケンスをローカルのセーフティ基準と照合するための実用的な参考資料となります。VDD_USBは絶対最大値が守られれば独立してシーケンスできます。
View full article
MCXN5xxT (184 VFBGA) power sequencing - power-down order and VDD_USB Two questions on power sequencing for MCX N5xxT in the 184 VFBGA package. Documents reviewed: data sheet MCXNTP184M170F70 Rev. 2.0 (14 Aug 2026), section 2.5 and Table 9; Hardware Design Guide UG10092 Rev. 6.1, mixed supply power configuration section. 1. Is there a required power-down sequence? The only power-down statement I can find is Table 9 footnote [2], which is conditional on 1.2 V operation on Ports P2/P3. For designs operating those ports in the 1.71 V to 3.6 V range, is reverse-of-power-up required, recommended, or unnecessary? I am specifically interested in uncontrolled events such as brownout, where rail collapse order is not guaranteed. 2. Does VDD_USB have any sequencing requirement relative to the system domain? It appears in the ratings tables but in no sequencing rule in either document. Thanks. MCXN Power Re: MCXN5xxT (184 VFBGA) power sequencing - power-down order and VDD_USB Hello @Kareem-Layous  1. There is no required power-down sequence, except for the condition mentioned in the note you referenced. Please follow the recommended power-up sequencing requirements in the datasheet when designing your system. 2. For VDD_USB, there is no special power-up sequencing requirement. Please ensure design as below: 3. There is a schematic available for the FRDM-MCXN947 board, which you may use as a reference. MCXN947 FRDM Board for Industrial IoT Solutions | NXP Semiconductors Thank you. BR Alice Re: MCXN5xxT (184 VFBGA) power sequencing - power-down order and VDD_USB Your review of section 2.5 and Table 9 is correct, the MCXN5xxT has no mandatory power‑down order except the 1.2 V footnote, so during a brown‑out the rails may collapse freely, though adding a supervisor to enforce a clean shutdown is advisable to protect internal state. In that context, the guidelines from Travis TX Property serve as a practical reference for matching hardware sequencing with local safety standards, especially when handling USB power domains. VDD_USB can be sequenced independently as long as its absolute‑max ratings are respected.
View full article
IMX95: Displays with a MIPI DSI and a dual-channel LVDS Hi, Can I output different sources to a DSI and a dual-channel LVDS at the same time? If this is supported, how to config the settings? I referred to IMX95 Manual and the device-trees, but I can not understand the association between pixel_interleaver , LDB and MIPI-DSI. Thanks. Re: IMX95: Displays with a MIPI DSI and a dual-channel LVDS For the normal i.MX95 BSP/device-tree model: do not plan on driving an independent MIPI-DSI display and a dual-channel LVDS display at the same time. The limiting point is the display output routing: the i.MX95 display controller has two independent display output streams, and dual-channel LVDS consumes the two LVDS-side paths, leaving no free input path for MIPI-DSI in the standard configuration . There is one important nuance: an NXP community knowledge-base item mentions i.MX95 triple-display Linux patches for LF-6.6.52-2.2.0 with “1 MIPI DSI + 2 LVDS” support and DTBs named imx95-19x19-evk-triple-display-lvds-clone.dtb and imx95-19x19-evk-triple-display-lvds-interleaver.dtb . That should be treated as a specific patched EVK/BSP use case , not as evidence that the unmodified reference manual/device trees support arbitrary independent DSI + dual-channel LVDS routing. The association is roughly: Block Role in the display path Display engines / DPU outputs Produce the two display streams, DISP_IN0 and DISP_IN1 . pixel_interleaver Routes or splits those streams. In bypass mode, DISP_IN0 goes to PL_OUT0 and DISP_IN1 goes to PL_OUT1 ; in interleaver mode, one selected input stream is interleaved while the other input is bypassed . LVDS / LDB / Pixel Mapper The i.MX95 LVDS path receives one or two display-interface streams and drives the LVDS PHYs; the RM describes the Pixel Mapper driving LVDS PHY1 and LVDS PHY2 . Some Linux/device-tree naming may still use “LDB”, but architecturally on i.MX95 this is the LVDS output path behind the pixel interleaver / pixel mapper. MIPI-DSI DSI takes pixel data through the Pixel Link path; the DSI pixel-formatting block converts Pixel Link format to DSI host DPI format, and a DSI pixel-link control field selects the pixel link connected to the DSI host controller . So, for standard configuration: Single-channel LVDS + MIPI-DSI : feasible; one display output path can feed LVDS and the other can feed DSI. Dual-channel LVDS only : feasible; both LVDS channels are used together for the LVDS display. Independent MIPI-DSI + dual-channel LVDS : not supported in the standard routing described by the current evidence; NXP community analysis states that dual-channel LVDS reserves both available DPU output ports, so MIPI-DSI cannot be routed at the same time. For configuration, I would not try to fix this by manually changing pixel_interleaver register values alone. Under Linux, the routing is established by the DRM device-tree graph: the DPU / display pixel link endpoints must connect to either LVDS/LDB or MIPI-DSI endpoints. If the DSI node has no valid upstream endpoint, the driver reports errors such as imx95-mipi-dsi ... No valid input endpoint found . For a supported setup, use the corresponding BSP DTB/overlay: LVDS-only: use the LVDS DTB for the intended LVDS channel/mode. DSI-only: use the DSI panel/bridge DTB. Single-LVDS + DSI: route one pixel-link output to LVDS and the other to DSI. Triple-display / DSI + 2 LVDS: start from the NXP LF-6.6.52-2.2.0 triple-display patch set and its provided DTBs, if that patch set matches your BSP and EVK baseline. Bottom line: with the normal i.MX95 BSP, use either dual-channel LVDS or DSI + single-channel LVDS; for DSI plus two LVDS outputs, use the specific NXP triple-display patch flow rather than trying to derive it from the RM registers alone. Re: IMX95: Displays with a MIPI DSI and a dual-channel LVDS Thanks for answering me. I learned a lot. This feature is not necessary. The reason why I want to do this is my target board has these two interface 2ch-lvds and mipi-dsi, but I don't like to reset fdtfile whenever I need to change the display to do testing. Re: IMX95: Displays with a MIPI DSI and a dual-channel LVDS Are there any official documents released by NXP for independent tripple display support?
View full article
Query regarding LC advancement (S32K3, No HSE) Hello, I have a few queries regarding the sequence to lock debug access when HSE is not used, specifically with regard to the life cycle advancement process. 1) After writing the configuration word to the life cycle configuration address in the IVT, will a functional reset(SW_FUNC) be sufficient to advance the life cycle or would I require a destructive reset (SW_DEST)? 2) If a functional reset is sufficient to advance the life cycle, can the life cycle configuration address configured in the IVT be a RAM address? 3) I want my application to conditionally lock the debug access port (let's say the application should only set the password and advance the life cycle once it receives a specific CAN message). Additionally I do not want to block/reserve a whole sector of flash just to set the configuration word to advance the life cycle of the MCU - As such, instead of permanently setting the LC configuration address in the IVT and writing 0xDADADADA/0xBABABABA to said address when I want to advance the life cycle, I was wondering if I could embed the configuration word as part of my application at a fixed address, and whenever the application decides to restrict debug access, the application could modify the IVT to set the life cycle configuration address and initiate a reset. Is this approach feasible? If yes, how can I go about modifying the IVT in runtime(are there any precautions I must take)? Additionally, is it okay for the IVT to contain the life cycle address for the remainder of the MCU's operating lifetime (assuming the data in the specified address is fixed to the configuration word) If no, are there alternate suggestions to achieve the same? 4) Regarding setting the password itself (cust_db_pswd_a) - Can I program this (and UTEST OTP data in general) via a debugger or must the firmware do it? With regards, Hareesh S  Re: Query regarding LC advancement (S32K3, No HSE) Hi @Hareesh_S  1. Yes, issuing a functional reset is sufficient to trigger the life cycle advancement process. 2. In general, I would not recommend using a RAM address for the LC configuration word. It is recommended to store it in non-volatile memory  to ensure that it remains available when the SBAF attempts to read it. 3. Your overall goal is feasible; however, I would not recommend modifying the IVT at runtime. A recommended approach would be to configure the life cycle configuration address in the IVT during production programming and keep it fixed. When your application receives the required CAN message, it can simply write the appropriate LC configuration word (for example, 0xDADADADA or 0xBABABABA, depending on the desired transition) to the predefined location and then issue a functional reset. 4. Yes, the password can be programmed using a debugger script; it does not need to be programmed exclusively by the firmware. However, before programming it or any other UTEST OTP data, it is necessary to unlock the UTEST sector by writing to the PFCBLKU_SPELOCK register located at address 0x40268358. BR, VaneB Re: Query regarding LC advancement (S32K3, No HSE) Hello @VaneB, Apologies for the delayed response, and much thanks for the clarification!
View full article
Best Personal Data Removal Services 2026: Top 6 Independently Tested & Expert-Ranked The Bottom Line After 6 months of hands-on evaluation, DeleteMe emerges as the clear winner among best personal data removal services. With 750+ broker coverage and human privacy experts, it delivers results that automated tools simply can't match. DELETEME Remove Your Personal Info Over the last two years, I've experimented with numerous data removal services, and frankly, most were disappointing. My details would vanish temporarily, only to resurface on people-search sites weeks later. It felt like throwing money away. That changed when I discovered DeleteMe. Initially hesitant, but after half a year of consistent use, I'm convinced it's the best personal data removal service available in 2026. If you're searching for credible Incogni alternatives or trying to figure out how to remove personal information from internet permanently, this is your solution. Why DeleteMe Stands Out Permanent Suppression: Unlike basic automated data removal services that perform one-off cleanups, DeleteMe provides ongoing monitoring and re-removal whenever your data resurfaces (which happens constantly). Human Intervention: When bots fail, actual privacy specialists step in to handle resistant sites. This human element is what transforms it into a truly effective data broker removal service. Unmatched Coverage: They monitor 750+ data brokers—significantly more than competitors like Incogni (~180 brokers) or budget options like Optery. Transparent Reporting: Quarterly reports show exactly what was found and successfully removed, providing documented peace of mind. How Other Top 6 Services Compared To ensure fairness, I evaluated other popular DeleteMe competitors during my research: Incogni: Solid budget choice for full automation (~$6.49/mo), but lacks human support for complicated scenarios. Optery: Excellent for visual proof with screenshot confirmations (~$3.99/mo), though follow-up aggressiveness doesn't match DeleteMe. Aura: Bundles removal with VPN/antivirus (~$12/mo), but its dedicated broker database is limited (~100 sites). Privacy Bee: Offers deep customization for tech-savvy users (~$14.99/mo), but overly complex for casual users. Cloaked: Focuses on proactive alias generation rather than removing existing data—good complement, not replacement. Is the Premium Price Justified? At $10.75/month annually, DeleteMe costs more than basic alternatives. However, the combination of human expertise, massive broker coverage, and guaranteed long-term suppression makes it worthwhile. Manual removal is free but consumes countless hours and yields temporary results. If you're exhausted from seeing your personal information scattered across the web and need a data removal service that delivers lasting protection.
View full article
IMX95:MIPI DSIとデュアルチャネルLVDSを搭載したディスプレイ こんにちは、 DSIとデュアルチャンネルLVDSの両方に異なるソースを同時に出力することはできますか? これがサポートされている場合、設定方法はどのようにすればよいですか? IMX95マニュアルとデバイスツリーを参照しましたが、pixel_interleaver、LDB、MIPI-DSIの関連性が理解できません。 ありがとう。 Re: IMX95: Displays with a MIPI DSI and a dual-channel LVDS 通常のi.MX95 BSP/デバイスツリーモデルの場合、独立したMIPI-DSIディスプレイとデュアルチャネルLVDSディスプレイを同時に駆動する計画はありません。 制限点は表示出力のルーティングです。i.MX95ディスプレイコントローラは2つの独立した表示出力ストリームを持ち、デュアルチャネルLVDSは2つのLVDS側パスを消費するため、標準構成ではMIPI-DSI用の空き入力パスがありません。 重要なニュアンスがあります。NXPコミュニティ知識ベース項目では、LF-6.6.52-2.2.0向けのi.MX95トリプルディスプレイLinuxパッチ(「1 MIPI DSI + 2 LVDS」対応)と、imx95-19x19-evk-triple-display-lvds-clone.dtb という名前のDTBが挙げられていますおよび imx95-19x19-evk-triple-display-lvds-interleaver.dtb 。これは 特定のパッチ適用済みEVK/BSPユースCASE として扱うべきであり、未修正の リファレンス・マニュアル やデバイスツリーが任意の独立したDSI + デュアルチャネルLVDSルーティングをサポートしている証拠としては扱うべきではありません。 その関連性は概ね以下の通りである。 ブロック 表示パスにおける役割 ディスプレイエンジン/DPU出力 2つの表示ストリーム、DISP_IN0とDISP_IN1を生成します。 ピクセルインターリーバー これらのストリームをルーティングまたは分割します。バイパスモードでは、DISP_IN0 は PL_OUT0 に、DISP_IN1 は PL_OUT1 に送られます。インターリーバモードでは、選択された入力ストリームの 1 つがインターリーブされ、もう 1 つの入力はバイパスされます。 LVDS / LDB / ピクセルマッパー i.MX95 LVDSパスは1つまたは2つのディスプレイインターフェースストリームを受け取り、LVDS PHYを駆動します。RMはLVDS PHY1およびLVDS PHY2を駆動するピクセルマッパーを記述しています。Linuxやデバイスツリーの命名方法では「LDB」を使うこともありますが、i.MX95のアーキテクチャ上、これはピクセルインターリーバー/ピクセルマッパーの背後にあるLVDSの出力パスです。 MIPI-DSI DSIはピクセルリンクパスを通じてピクセルデータを処理します。DSIピクセルフォーマットブロックはピクセルリンクフォーマットをDSIホストDPIフォーマットに変換し、DSIピクセルリンク制御フィールドはDSIホストコントローラにコネクテッドされたピクセルリンクを選択します。 標準的な構成の場合: シングルチャネルLVDS + MIPI-DSI:実現可能;一方の表示出力パスはLVDSに、もう一方はDSIに供給可能です。 デュアルチャネルLVDSのみ:実現可能;両方のLVDSチャネルはLVDS表示のために一緒に使用されます。 独立したMIPI-DSI + デュアルチャネルLVDS:現在の証拠で説明されている標準ルーティングにはサポートされていません。NXPコミュニティの分析によると、デュアルチャネルLVDSは利用可能なDPU出力ポートの両方を予約するため、MIPI-DSIを同時にルーティングすることはできません。 設定に関しては、pixel_interleaverレジスタの値だけを手動で変更してこの問題を解決しようとはしない方が良いでしょう。Linuxでは、ルーティングはDRMデバイスツリーグラフによって確立されます。DPU/ディスプレイピクセルリンクエンドポイントはLVDS/LDBまたはMIPI-DSIのいずれかに接続する必要があります。DSIノードに有効な上りエンドポイントがない場合、ドライバはimx95-mipi-dsi ...などのエラーを報告します。有効な入力エンドポイントは検出されません。サポートされている設定の場合は、対応するBSP DTB/オーバーレイを使用してください。 LVDS専用:意図されたLVDSチャネル/モードにLVDS DTBを使用します。 DSI専用:DSIパネル/ブリッジDTBを使用してください。 シングルLVDS + DSI: 一方のピクセルリンク出力をLVDSに、もう一方をDSIにルーティングします。 トリプルディスプレイ / DSI + 2 LVDS: NXP LF-6.6.52-2.2.0 トリプルディスプレイパッチセットと付属の DTB から始めてください。ただし、そのパッチセットが BSP および EVK のベースラインと一致する場合に限ります。 結論として、通常のi.MX95 BSPでは、デュアルチャネルLVDSまたはDSI + シングルチャネルLVDSのいずれかを使用します。DSIと2つのLVDS出力の場合は、RMレジスタだけから導き出すのではなく、特定のNXPトリプルディスプレイパッチフローを使いましょう。 Re: IMX95: Displays with a MIPI DSI and a dual-channel LVDS ご回答ありがとうございます。私は多くのことを学びました。 この機能は必要ありません。これをやりたい理由は、ターゲットボードには2ch-lvdsとmipi-dsiの2つのインターフェースがあるのですが、ディスプレイをテストするために毎回fdtfileをリセットしたくないからです。 Re: IMX95: Displays with a MIPI DSI and a dual-channel LVDS NXPが独立したトリプルディスプレイサポートに関する公式文書を公開しているのでしょうか?
View full article
LCの進角に関する問い合わせ(S32K3、HSEなし) こんにちは、 HSEが使われていない場合にデバッグアクセスをロックする順序について、特にライフサイクルの進展プロセスに関していくつか質問があります。 1) IVTのライフサイクル構成アドレスに設定ワードを書き込んだ後、機能リセット(SW_FUNC)でライフサイクルを進めるのに十分でしょうか、それとも破壊的なリセット(SW_DEST)が必要でしょうか? 2) 機能リセットだけでライフサイクルが進むのに十分であれば、IVTで設定されたライフサイクル構成アドレスはRAMアドレスとして機能するのでしょうか? 3) アプリケーションが条件付きでデバッグアクセスポートをロックしたい(例えば、特定のCANメッセージを受け取ってからパスワードを設定し、ライフサイクルを進めるとします)。さらに、設定ワードを設定するためにフラッシュのセクター全体をブロック・予約したくありません。そのため、IVT内でLCの設定アドレスを恒久的に設定し、ライフサイクルを進めたいときにそのアドレスに0xDADADADA/0xBABABABAを書き込む代わりに、設定ワードを固定アドレスに組み込み、アプリケーションがデバッグアクセスを制限した際にIVTを修正してライフサイクル設定アドレスを設定しリセットを開始できるかどうかを考えています。 このアプローチは実現可能だろうか? もしそうなら、実行時にIVTをどうやって修正すればいいですか?(注意すべき注意点はありますか)さらに、指定アドレス内のデータが設定ワードに固定されていると仮定した場合、MVUの残りのライフサイクルアドレスをMCUの動作期間中に保持しても問題ないでしょうか? もしなければ、同じように達成するための代替案はありますか? 4) パスワード設定自体について(cust_db_pswd_a) - これはデバッガでプログラムできるのか、それともファームウェアがやらなければならないのか? よろしくお願いいたします。 ハリーシュS Re: Query regarding LC advancement (S32K3, No HSE) こんにちは、 @Hareesh_S さん。 1.はい、機能リセットを実行するだけでライフサイクル進行プロセスが開始されます。 2.一般的に、LC構成ワードにRAMアドレスを使用することはお勧めしません。SBAFが読み取ろうとした際に確実に利用できるように、不揮発性メモリに保存することをお勧めします。 3.あなたの全体的な目標は実現可能ですが、実行時にIVTを変更することはお勧めしません。 推奨される方法は、本番プログラミング中にIVTでライフサイクル構成アドレスを設定し、それを固定しておくことです。アプリケーションが必要なCANメッセージを受け取った場合、適切なLC構成ワード(例えば、遷移に応じて0xDADADADAまたは0xBABABABA)をあらかじめ定義された場所に書き込み、機能リセットを発行するだけで済みます。 4. はい、パスワードはデバッガスクリプトを使ってプログラム可能です。ファームウェアだけでプログラムする必要はありません。 ただし、UTEST OTPデータやその他のデータをプログラムする前に、アドレス0x40268358にあるPFCBLKU_SPELOCKレジスタに書き込むことでUTESTセクターのロックを解除する必要があります。 BR、VaneB Re: Query regarding LC advancement (S32K3, No HSE) こんにちは、 @VaneB さん。 返信が遅くなり申し訳ありません。ご説明いただき、誠にありがとうございます!
View full article
2026年最佳个人数据清除服务:经独立测试和专家排名的前6名 底线 经过 6 个月的实际评估,DeleteMe 脱颖而出,成为最佳个人数据删除服务中的明显赢家。凭借 750 多家经纪商的覆盖范围和人工隐私专家,它能够提供自动化工具根本无法比拟的结果。 DELETEME 删除您的个人信息 过去两年里,我尝试过很多数据删除服务,坦白说,大多数都令人失望。我的信息会暂时消失,但几周后又会在人脉搜索网站上重新出现。感觉就像在扔钱。 自从我发现了 DeleteMe 之后,一切都改变了。起初我还有些犹豫,但经过半年的持续使用,我确信它是 2026 年最好的个人数据删除服务。如果您正在寻找可靠的Incogni 替代方案,或者想了解如何永久地从互联网上删除个人信息,那么这就是您的解决方案。 为什么 DeleteMe 脱颖而出 永久删除:与执行一次性清理的基本自动数据删除服务不同,DeleteMe 提供持续监控,并在您的数据再次出现时(这种情况会不断发生)重新删除数据。 人工干预:当机器人失效时,真正的隐私专家会介入处理难以识别的网站。正是这种人为因素,使其转变为真正有效的数据经纪人清除服务。 无与伦比的覆盖范围:他们监测 750 多个数据经纪商——远远超过 Incogni(约 180 个经纪商)等竞争对手或 Optery 等预算选项。 透明报告:季度报告准确显示已发现和成功清除的内容,提供有据可查的安心保障。 与其他六大顶级服务相比 为了确保公平性,我在研究过程中还评估了其他一些热门的DeleteMe竞争对手: Incogni :经济实惠的全自动解决方案之选(每月约 6.49 美元),但在复杂情况下缺乏人工支持。 Optery :非常适合提供带屏幕截图确认的视觉证据(约3.99美元/月),虽然后续的攻击性与 DeleteMe 不符。 Aura :捆绑 VPN/杀毒软件移除(每月约 12 美元),但其专用的经纪商数据库有限(约 100 个网站)。 Privacy Bee :为精通技术的用户提供深度定制服务(约14.99美元/月),但对于普通用户来说过于复杂。 Cloaked :专注于主动生成别名,而不是删除现有数据——是很好的补充,而不是替代品。 高价合理吗? DeleteMe 的年费为每月 10.75 美元,比基本替代方案更贵。然而,人类的专业知识、庞大的经纪人覆盖范围以及长期抑制的保证相结合,使其成为值得的。手动清除虽然免费,但耗时费力,而且效果只是暂时的。 如果您厌倦了看到自己的个人信息散落在网络上,并且需要一种能够提供持久保护的数据删除服务。
View full article
S32K3xx Development Package Installation and Dependency Issues in S32 Design Studio 3.6.11 Hello, Just going to preface this post with the fact that I used AI to format the post for clarification and readability. I am currently setting up S32 Design Studio 3.6.11 to develop firmware for the S32K311 microcontroller. However, I have been having issues installing the S32K3xx Development Package. Issues Encountered: I have been unable to find a working update site for the S32K3xx Development Package. When attempting to uninstall the package, I received the following message: "S32K3xx development package" cannot be fully uninstalled because other installed software requires it. The parts that are not required will be uninstalled. Steps I Have Tried: I spoke with the NXP website's AI assistant, which recommended the following steps: Uninstall the S32K3xx FS26 AUTOSAR RTD extension. Restart S32 Design Studio. Uninstall the S32K3xx Development Package. Restart S32 Design Studio. Reinstall the development package, followed by the FS26 RTD extension. After removing the FS26 extension, I used the Reinstall option for the S32K3xx Development Package within S32 Design Studio. However, this option only uninstalled the development package and did not reinstall it. To clarify, I selected Reinstall, not Uninstall. The IDE automatically started the uninstall process but never completed the reinstallation. Error When Installing Through the IDE: I also tried manually installing the development package through the IDE using the NXP update site but received the following error: (the post doesn't allow the invalid url so I will be attaching the photo) Questions: Is there a working update site or downloadable ZIP file for the S32K3xx Development Package? Why would the Reinstall option uninstall the package without reinstalling it? How can I resolve the repository error shown above? Is there a recommended way to perform a clean installation of the development package? Additional Note: I have not attempted a full reinstallation of S32 Design Studio because I am using a company-managed computer. Reinstalling the IDE requires IT permissions and would likely take several days to complete. Because of this, I would prefer to resolve the issue without reinstalling the entire IDE, if possible. Any help would be appreciated. Thank you! Re: S32K3xx Development Package Installation and Dependency Issues in S32 Design Studio 3.6.11 Hi @BakeAndShake  From the behavior observed, it seems that access to the update sites may be restricted by a firewall, proxy configuration, or another network security policy. Could you please check this with your IT team to confirm whether access to these repositories is allowed? Also, if possible, could you try the installation on a different machine? This would help us determine whether the issue is related to the current PC configuration. BR, VaneB
View full article
PCA9306DC1Z is NRND, any P2P option? Hi Team, Currently, I'm using PCA9306DC1Z, which is NRND, can you recommend a p2p option for my new design? Thank you. Kind Regards, Boler I2C Level Shifters Re: PCA9306DC1Z is NRND, any P2P option? Hi Bo, The PCA9306DC1Z (VSSOP8) is confirmed NRND and there is currently no active NXP replacement in the same VSSOP8 package. However, the following active PCA9306 variants are available — same electrical functionality, but requiring a PCB layout change: BRs, Tomas
View full article
SPDIF Output Jitter on MIMXRT1170-EVKB Using NXP SDK spdif_edma_transfer Example Hello NXP Support Team, I am investigating an SPDIF issue using the MIMXRT1170-EVKB development board. The project is based on the official NXP SDK spdif_edma_transfer example. Test configuration: - Board: MIMXRT1170-EVKB - Core: Cortex-M4 - SPDIF input: J46 (GPIO_AD_15) - SPDIF output: J45 (GPIO_AD_16) - Sample rate: 48 kHz - Transfer method: eDMA - Mode: Continuous SPDIF input-to-output forwarding Observed issue: The SPDIF input signal is received successfully. The DPLL locks correctly, and SPDIF transmission starts. However, jitter is observed in the SPDIF output signal. Expected behavior: The SPDIF output should reproduce the received SPDIF audio signal with stable timing. I have prepared a complete modified SDK demo project that reproduces this issue. Could an NXP engineer review the project and help identify the cause of the SPDIF output jitter? I would also like to know whether I can attach the complete project ZIP file to this discussion. Thank you for your support. Re: SPDIF Output Jitter on MIMXRT1170-EVKB Using NXP SDK spdif_edma_transfer Example Hi @yp_wang , Thanks for your reaching out! Could you please provide the SDK version number? Additionally, if possible, please share a minimal reproducible project based on the latest version of the SDK. It would also be helpful to attach the waveform of the jitter you observed. This will assist us in reproducing the issue and identifying the cause. Thanks in advance! Best regards, Gavin Re: SPDIF Output Jitter on MIMXRT1170-EVKB Using NXP SDK spdif_edma_transfer Example thanks  please refer to the spdif.pdf ,and mp4 file , something wrong with my NXP account, if you need the test code ,please give me your emal address   Re: SPDIF Output Jitter on MIMXRT1170-EVKB Using NXP SDK spdif_edma_transfer Example files are attached Re: SPDIF Output Jitter on MIMXRT1170-EVKB Using NXP SDK spdif_edma_transfer Example Hi @yp_wang , Thanks for your attached file. However, I cannot address the issue without the application code. If possible, could you please submit a ticket through the official channel? This way, any code or minimal reproduction project you upload will remain private and inaccessible to external users. Link: https://support.nxp.com/s/ Thanks! Re: SPDIF Output Jitter on MIMXRT1170-EVKB Using NXP SDK spdif_edma_transfer Example I’m unable to submit this attachment because the system says “Case creation disabled.” I also contacted NXP by email, but the issue still seems unresolved. Is there another way to submit it? @Gavin_Jia  Re: SPDIF Output Jitter on MIMXRT1170-EVKB Using NXP SDK spdif_edma_transfer Example Hi @yp_wang , I am not sure why you are unable to create an SFDC ticket on your end. However, you can try contacting an online sales representative via the official website by clicking the button shown in the image below: Link: www.nxp.com They will be able to assist you with your account issues or help you create an SFDC ticket. Thank you! Re: SPDIF Output Jitter on MIMXRT1170-EVKB Using NXP SDK spdif_edma_transfer Example Hi , Thanks for the attachments.  After reviewing your CM4/CM7 code and the SPDIF drivers, we believe the problem is not jitter generated by the SPDIF transmitter itself. It is most likely caused by clock-domain mismatch between RX and TX in your forwarding design. 1. RX and TX run on two independent clocks RX follows the external source. The DPLL recovers its timing from the incoming SPDIF stream on J46. TX uses the local clock. With STC[TxClk_Source] = 001 , the transmitter is clocked from SPDIF_CLK_ROOT , which your code derives from the Audio PLL. DPLL lock only means the receiver is tracking the input. It does not make TX follow the input clock. 2. Consequence for continuous forwarding Both sides are nominally 48 kHz, but the source clock and the local PLL are not exactly equal. In RX → memory → TX forwarding without rate matching, this small frequency difference gradually consumes the buffer margin. Over time this leads to periodic sample drops or repeats, followed by TX FIFO underrun or overrun.  3. The error-recovery code makes it worse On a TX FIFO error, the ISR aborts TX only, then sets emptyBlock = BUFFER_NUM . However, RX transfers are still in flight, and txIndex / rxIndex are not reset. The buffer bookkeeping then no longer matches the real DMA state. Queued TX blocks are skipped, and the TX/RX distance after restart becomes arbitrary, so the next failure can come sooner. Also, kSPDIF_RxFIFOError is handled in the ISR but never enabled. And here is our suggestions for your application: Add rate matching. Use ASRC between SPDIF RX and the TX clock domain (see NXP AN14631) Rewrite error recovery so that it stops both RX and TX, clears both driver queues and all buffer indexes, then restarts with a pre-filled buffer. Discard the first 192 frames after DPLL lock, as required by RM §59.5. For quick isolation, try hardware feed-through ( SCR[TxSel] = 001 ). If the output is clean in this mode, the board and measurement chain are fine, and the issue is in the software forwarding path. Hope that helps! Best regards, Gavin Re: SPDIF Output Jitter on MIMXRT1170-EVKB Using NXP SDK spdif_edma_transfer Example attached the project ,based on the newest SDK,  RAM download ,if you have any question ,please email [email protected]   Re: SPDIF Output Jitter on MIMXRT1170-EVKB Using NXP SDK spdif_edma_transfer Example You were right. I changed the clock source on the test equipment and configured it to stay synchronized with the SPDIF clock. After that, the jitter disappeared. Thank you. If I encounter any further issues with SPDIF or anything else, I will contact you again.
View full article
DDR4搭載のiMX8 Mini / Nano こんにちは! iMX8 MiniとNanoの両方に対応した基板を設計しています。 DDR4メモリチップを採用しています。NanoのDDRコントローラは16倍の速度で、1つのチップは、 Miniは16倍/32倍なので、1つか2つのチップで選べます。 16xの場合、チップの1つが未実装であることを考えると、最適なルーティングは 戦略は、短時間で終了するフライバイ方式である。これを確認していただけますか? 一方のチップを16倍モードで使用し、もう一方のチップを未実装にする場合、 このチップはチェーンの中央に配置するのが良いでしょう(マイクロプロセッサとメモリの長さの比率を最小限に抑えるため)。 あるいは、終端付近(スタブを終端まで最小限に抑える)でしょうか? 2つのDDR4チップを搭載したiMX8 Miniのリファレンスデザインはありますか? よろしくお願いします。 アンドレア Re: iMX8 Mini / Nano with DDR4 こんにちは、 フライバイトポロジーの設計ガイドはなく、Tトポロジーの使用が推奨されています。 2つのDDRを持つ8M Mini DDR4 EVKの設計ファイルを参照 i.MX。https://www.nxp.com/design/design-center/development-boards-and-designs/8MMINILPD4-EVK?gad_source=1&gad_campaignid=24046353493&gbraid=0AAAAA_oV6rR712b8UskLZlbqeYOCaD5hO&gclid=EAIaIQobChMI8N6O9pfGlwMVOhloAR1cWTZ8EAAYASAAEgLoi_D_BwE Re: iMX8 Mini / Nano with DDR4 こんにちは、 残念ながら、Tトポロジーは、アンピュレートチップをサポートする場合には使えません。 フライバイを試してみます。 よろしくお願いします。 アンドレア
View full article
キーフォブ/スマートカードでのみログインできます 私は製造会社で働いており、従業員が部品図面を見たり、タスク完了のサインをしたりできるように、工場の現場にPCを設置しようと考えています。できるだけ手間を軽くしつつ、誰がタスクにサインしたかの記録も残したいため、従業員がすでに持っているアクセスコントロールバッジを使ってドアへのアクセスや出退勤をする最適な方法を検討しています。もしそれが現実的でなければ、従業員が物理的なトークンでログインし、キーボードやマウスに触れることなく、ユーザー名やパスワードを覚える必要もない、他の選択肢も検討しています。スマートカードについて調べてみましたが、PINコードが必要なようで、できれば避けたいと思っています。私たちは固有のセキュリティリスクを理解しており、これらのデバイスは特定のタスクしか実行できず、ネットワークの他の部分にアクセスできないようにロックダウンされます。 モバイルのスマートカード Re: Login with keyfob/smartcard only MIFARE DESFire EV3をおすすめします。 こちらのウェブページはこちらです:MIFARE DESFire EV3 |セキュア非接触IC |NXP Semiconductors Re: Login with keyfob/smartcard only NXPの担当者を困らせるかもしれないが、指紋リーダーを内蔵したFIDO2キートークンを提案してみようと思う。ほとんどのOSはFIDO2を自然にサポートするか、簡単にインストールできるプラグインで対応しています。 トークンに指紋認証機能を追加することで、トークンを特定の人物に紐付けつつも、非常にスムーズに動作させることができる。トークンの形式は、クレジットカード型とドングル型がある。前者は通常、コンタクト・リーダまたはNFCリーダーのいずれかで動作し、後者は通常USBトークン、非接触トークン、またはコンボのいずれかです。
View full article