Display not working on IMX 93 FRDM board Hi, I am using an i.MX 93 FRDM board with Linux version 6.6.36 (Scarthgap), the fsl-imx-wayland distribution, and the core-image-weston image. However, the display is not working, and the screen remains blank. The system detects both the display and the HDMI interface, but no output is shown on the screen. Could you please help me identify the possible cause of this issue and suggest steps to troubleshoot it?. Re: Display not working on IMX 93 FRDM board Hi @Zhiming_Liu , One more observation, When I connected the device to my monitor, it worked as expected. However, after connecting it to my waveshare display and rebooting the device , it failed to work. Interestingly, when I reconnected it to the original monitor and rebooted the device, it worked again. Why this behaviour occurs?? With regards Ajil Re: Display not working on IMX 93 FRDM board Hi all, The issue is solved.Changed the required display resolution in /etc/xdg/weston/weston.ini The display is working fine. With regards Ajil Re: Display not working on IMX 93 FRDM board Hi @ap3415 If the hardware connections are working properly, please use imx-image-core for testing. Best Regards, Zhiming Re: Display not working on IMX 93 FRDM board Hi @Zhiming_Liu , Thank you for the suggestion. However, my project requires core-image-weston, so I am testing with this image. Could you please suggest how I can troubleshoot the issue with core-image-weston or help identify any additional configuration required to make it work properly? With regards, Ajil
View full article