Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
需要帮助解决 imx95lpd5evk 启动问题 我刚拿到一块imx95lpd5evk主板,它无法启动,请问如何才能启动? 目前的设置是,我将启动开关 SW7 设置为 0010,以便从 eMMC 启动。 我已将 IMX-MIPI-HDMI 板连接到 Mini SAS 连接器 J14,并通过 HDMI 线连接到监测。 当我将 USB-C 调试线连接到我的电脑时,电脑甚至都检测不到它,设备管理器中甚至没有显示未知设备。 现在我打开板,本以为屏幕上会像快速入门指南里说的那样出现企鹅,但我却没有看到任何企鹅。屏幕只有黑色。开机后我只看到风扇转了,仅此而已。 我有个疑问,即使imx95宕机,调试功能是否也应该正常工作?因为我怀疑我的工作笔记本电脑的USB接口是否被禁用,这才是导致问题的原因。 我这块板上的eMMC芯片是不是空的?因为企鹅并没有如期而至。 请问有人能指导我接下来该怎么做吗? Re: Need help on imx95lpd5evk booting 实际上这是我的失误,现在已经解决了,主板正在启动。 感谢你的回复 Re: Need help on imx95lpd5evk booting 你好, 请您提供一下交换机(SW7)的图片,并按照“连接USB调试线”章节中的步骤操作,然后分享终端的输出结果。
View full article
S32K44とS32K388は何つの直交エンコーダ入力をサポートできますか? https://community.nxp.com/t5/S32K/Quadrature-decoder-on-S32K344/m-p/1507580 とアプリケーションノートも見つけました https://www.nxp.com/design/design-center/development-boards-and-designs/MCSPTE1AK344 しかし、どれだけの直交エンコーダをインスタンス化できるか特定に苦労しています。 理想的には、4つの独立した直交デコーダーを用意したいアプリケーションがあります。S32K344もS32K388もそれをサポートするのでしょうか? Re: How many Quadrature encoder inputs can an S32K44 and an S32K388 support? こんにちは、 S32K3ファミリには専用の直交デコーダペリフェラルは搭載されていません。その代わりに、直交デコーダ機能は、LCU、TRGMUX、およびeMIOSモジュールを組み合わせて実装されています。これはS32K3リファレンス・マニュアルおよびコミュニティThreadで参照されているモータ制御の例で説明されているアプローチです。 リファレンスマニュアルによると、インクリメンタルエンコーダの例では、単一の直交デコーダ実装には2つの論理セル(LC0とLC1)が必要です。S32K344およびS32K388デバイスは、2つのLCUインスタンスを提供します。 しかし、モータ制御チームにもフィードバックを求めました。 できるだけ早く最新情報をお知らせします。 よろしくお願いいたします。 ピーター Re: How many Quadrature encoder inputs can an S32K44 and an S32K388 support? こんにちは、 アップデート: NXPのサンプルで説明されている実装に基づくと、S32K344とS32K388の両方において、実用的な限界は3つの独立した直交デコーダとなる。このソリューションは以下を消費します: TRGMUX入力ピン6本(×A/Bエンコーダ入力3本)、 MCB動作可能な6つのeMIOSチャネル(例:eMIOS0 CH1-CH6)、 3つのロジックセル(1つのLCUインスタンス)。 したがって、示されたアーキテクチャを用いて3つのエンコーダインスタンスを直接実装することができます。 4つ目のエンコーダーは、同じリソースマッピングでは直接サポートされていません。主な制約は、MCBモードで動作する適切なeMIOSチャネルの利用可能性と、TRGMUXおよびLCUを通じた必要な信号ルーティングの提供です。 残ったG型チャネル(例:CH7)とXチャネルを組み合わせ、LCU出力を外部のデバイスピン経由でeMIOS X入力にルーティングします。例えば、S32K344ではPTB2をLCU1_OUT3とeMIOS0_CH8_Xの両方として設定でき、実質的に外部ループバックパスを作成できます。しかし、この方法は追加のパッケージピンを消費し、標準的な実証された解決策には含まれていません。 その結果、3つの直交デコーダは容易に実現可能ですが、4つ目のデコーダは代替のルーティング方式やカスタムの回避策が必要であり、全体のピンおよびペリフェラルのリソース使用量と照らして評価する必要があります。 よろしくお願いいたします。 ピーター Re: How many Quadrature encoder inputs can an S32K44 and an S32K388 support? 私のアプリケーションでは、タイマーを使ってカウントするeMIOSベースの解釈はあまり必要ありません。エンコーダーカウントがあれば十分です。8つのTRGMUX入力と4つのLCUセルを組み合わせて、単にカウントダウンするだけのものをサポートする構成はありますか?
View full article
我应该使用哪个 Matter 分支/版本? 你好, 我有点困惑该选择哪个 Matter 分支。我看到有v1.6.0.0.1版本和一个分支v1.6-branch-imx_matter_2026_q2 ,后者是建议在 Linux 环境下运行的 iMX93 上使用的分支。这两个分支之间有什么需要注意的重大变化吗? __展示 __展示 Re: Which Matter Branch/Release should i use 嗨@pengyong_zhang , 我想了解这个分支的用途,以及它与connectedhomeip除了 ELE 和 groupcast 之外的其他区别,并举几个例子。我看不出它们之间有什么区别,而且v1.6-branch-imx_matter_2026_q2版本看起来比 connectedhomeip 的其他版本要旧。 __展示 __展示 Re: Which Matter Branch/Release should i use 嗨@eldhokk 你应该使用 v1.6-branch-imx_matter_2026_q2。v1.6.0.0.1版本适用于 MCU 平台(FreeRTOS/Zephyr)。 B.R
View full article
Secure Boot Fuse programming I have a question regarding SRK hash fuse protection and secure boot on the i.MX RT1024. The SRK hash is 256 bits, stored across eight 32-bit OCOTP fuse words. Since OTP fuses can only be programmed from 0 to 1, some bits in the expected SRK hash will intentionally remain 0. My concern is that, even after programming all eight SRK hash words correctly, an unintended or unauthorized write could change an intentionally zero bit to 1. This would permanently modify the stored SRK hash and cause HAB authentication to fail. Could you please clarify the following? SRK hash write protection: On the i.MX RT1024, does programming SEC_CONFIG to enable closed mode prevent further programming of the SRK hash fuse words (OCOTP addresses 0x18–0x1F)? Dedicated lock mechanism: Is there a separate fuse or hardware mechanism to permanently prevent further modification of the SRK hash after provisioning? If so, could you please specify the relevant fuse addresses and the procedure to enable this protection? Protection of intentional zero bits: If an SRK hash bit is 0 in the expected hash, what prevents that bit from being unintentionally or maliciously programmed to 1 after the device has been provisioned? Re: Secure Boot Fuse programming Hi @Abhay2080 , Thanks for your questions! 1. Closed mode only tells the ROM to reject images that fail HAB authentication. It does not write-protect OTP fuse. The SRK hash words can still be programmed after the device is closed. 2. Based on internal feedback, SRK_LOCK must not be used on the RT1024, as it can prevent the ROM from correctly reading the SRK hash and cause boot failure. Therefore, we cannot recommend a fuse address or programming procedure for permanently locking this region. Within the RT10xx series, only the RT1010 supports the LOCK function. For the RT11xx series, fuses are generally programmed on a word-by-word basis, and they incorporate ECC protection; therefore, there is no need to worry about bit 0 being altered again. Please check AN12800 for more details. 3. Closed mode alone does not prevent these bits from being programmed to 1. The recommended mitigation is runtime access control and privilege separation: restrict access to the OCOTP programming registers to trusted privileged code and prevent ordinary application code from accessing them. This reduces the risk of unintended or unauthorized programming; it is not a permanent fuse write lock. I hope this clarification helps! Best regards, Gavin
View full article
Guiguider 2.0.1 では C 言語シミュレータを作成できません。 Windows 10にguiguider 2.0.1をインストールしたところ、インストールと実行は正常に完了し、コード生成も正常でした。しかし、Cシミュレータを生成する際に、以下のエラーが発生しました。 私のシステムがWindows 10(Windows 11が必要)だからなのか、それとも他に何か問題があるのか知りたいです。 Re: guiguider2.0.1不能创建C模拟器 こんにちは、 @tbgさん エラーログをご提供いただきありがとうございます。 GUI Guider 2.0.1は公式にWindows 11(64ビット)をサポートしています。 ログから、Cシミュレータが失敗するのは、バンドルされているGCC/MinGWコンパイラがcc1コンポーネントを実行できないためです。 cc.exe: 致命的なエラー: 'cc1' を実行できません: CreateProcess: そのようなファイルやディレクトリはありません したがって、まずWindows 11でGUI Guider 2.0.1をテストすることをお勧めします。同じ問題が依然として起きている場合は、ツールチェーンやインストール環境をさらに調査できます。 BR ハリー
View full article
i.MX 8ULP - M33上のMIPI CSIおよびISI(リアルタイム領域) こんにちは、 私はMIPI CSIカメラを、アプリケーションドメインの関与なしにリアルタイムドメインから完全に使おうとしています。 ほとんど動作させることができましたが、ISIのフレーム補完割り込みはアプリケーションドメインでのみ利用可能であるようです。誰かそれが正しいか確認できますか? 完了したフレームを検出するためにISIチャネルステータスレジスタをポーリングすることはできますが、理想的とは言えません。私は割り込みを直接使用したいです。A35からM33にMU経由で割り込みを転送すると設計の目的が損なわれるので、それは避けたいです。 A35側のハンドラーに頼らずに、M33がフレームの完了を通知される他の方法はありますか? i.MX8ULP Re: i.MX 8ULP - MIPI CSI and ISI on M33 (realtime domain) こんにちは、 残念ながら、Cortex-M33はMIPI-CSI割り込みを扱えず、A35のみが対応可能です。
View full article
Unable to save flash image from target board with MCULink probe W10, Linkserver 26.9.130, MCULink FW 3.174: I want to save a flash image from a LPC804 board using SWD. I have the MCULink probe, I installed the Linkserver package which includes the LinkFlash tool. With this I was able to update the MCULink FW to the latest. Using the LinkFlash GUI I am not able to save the flash image from my target board due to a "Failed on Connect (Ee42)". No probe jumpers are placed (SWD). I have selected "LPC804:" as a device, but I noticed in other examples a more complete part# and an IDE is usually named. Do I need to create a configuration file or install an IDE such as Expresso to get past this, or is it more likely to be cabling and target connection issue? Ns: LinkServer RedlinkMulti Driver v26.9 (Sep 18 2026 19:34:33 - crt_emu_cm_redlink.exe build 1382) Pc: ( 0) Reading remote configuration Wc(03). No cache support. Nc: Found generic directory XML file in C:\Users\T\AppData\Local\Temp\tmps4ueywdg\crt_directory.xml Pc: ( 5) Remote configuration complete Nc: Reconnected to existing LinkServer process. Nc: Connecting to probe 1 core 0 (using server started externally) reports: 'Ee(42). Could not connect to core.' Nc: Retrying... Nc: Reconnected to existing LinkServer process. Nc: Server OK but no connection to probe 1 core 0 (after 3 attempts) - Ee(42). Could not connect to core. Ed:02: Failed on connect: Ee(42). Could not connect to core. Et:31: No connection to chip's debug port Pc: (100) Target Operation Failed Re: Unable to save flash image from target board with MCULink probe I also tried the CL instead of the GUI but it made no difference. Comparing with your output I seem to get stuck on: Nc: Connecting to probe 1 core 0 (using server started externally) reports: 'Ee(42). Could not connect to core.' This seems to be complaining about the probe, not the target. Re: Unable to save flash image from target board with MCULink probe I think you might have a connection (physical cable?) issue. Using it on Ubuntu, but same would apply to Win10: /usr/local/LinkServer_26.9.130/LinkServer flash --probe 4FIQSNVD2MICA LPC804: dump 0x00000000 0x00001000 /tmp/memory.bin INFO: Exact match for LPC804: found INFO: Selected device LPC804:LPCXpresso804 INFO: Selected probe #1 4FIQSNVD2MICA (MCU-LINK Pro (r1CF) CMSIS-DAP V3.174) INFO: MCU-Link firmware update `check`: Probe ([4FIQSNVD2MICA] [MCU-LINK Pro (r1CF) CMSIS-DAP V3.174]) is already running the same firmware version as the included firmware version [3.174] Firmware update `check`: not required - forced update can be performed using: `./LinkServer probe #1 update forced` Ns: LinkServer RedlinkMulti Driver v26.9 (Sep 18 2026 19:46:03 - crt_emu_cm_redlink build 1382) Pc: ( 0) Reading remote configuration Wc(03). No cache support. Nc: Found generic directory XML file in /tmp/tmpuhtfp3bl/crt_directory.xml Pc: ( 5) Remote configuration complete Nc: Reconnected to existing LinkServer process. Nc: Probe Firmware: MCU-LINK Pro (r1CF) CMSIS-DAP V3.174 (NXP Semiconductors) Nc: Serial Number: 4FIQSNVD2MICA Nc: VID:PID: 1FC9:0143 Nc: USB Path: 0005:0013:00 Nc: Using memory from core 0 after searching for a good core Pc: ( 30) Emulator Connected Pc: ( 40) Debug Halt Pc: ( 50) CPU ID Nc: debug interface type = CoreSight DP (DAP DP ID 0BC11477) over SWD TAP 0 Nc: processor type = Cortex-M0+ (CPU ID 00000C60) on DAP AP 0 Nc: number of h/w breakpoints = 4 Nc: number of flash patches = 0 Nc: number of h/w watchpoints = 2 Nc: Probe(0): Connected&Reset. DpID: 0BC11477. CpuID: 00000C60. Info: Nc: Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled. Ns: Content of CoreSight Debug ROM(s): Nc: RBASE E00FF000: CID B105100D PID 04000BB4C0 ROM (type 0x1) Nc: ROM 1 E000E000: CID B105E00D PID 04000BB008 Gen SCS (type 0x0) Nc: ROM 1 E0001000: CID B105E00D PID 04000BB00A Gen DWT (type 0x0) Nc: ROM 1 E0002000: CID B105E00D PID 04000BB00B Gen FPB (type 0x0) Nc: NXP: LPC804 Nc: DAP stride is 1024 bytes (256 words) Nc: Inspected v.2 On-chip Flash Memory LPC80x_32.cfx Nc: Image 'LPC80x (32K) Sep 18 2026 18:35:07' Pc: ( 65) Chip Setup Complete Pc: ( 70) License Check Complete Nt: Dumping 'memory.bin' Binary section 0 at 0x00000000 len 0x1000 Nc: Opening flash driver LPC80x_32.cfx Nc: VECTRESET requested, but not supported on ARMv6-M CPUs. Using SOFTRESET instead. Nc: Using SOFT reset to run the flash driver Nc: Flash device supported (32KB = 32*1K at 0x0) Ps: ( 0) at 00000000: 0 bytes - 0/4096 Ps: (100) at 00000000: 4096 bytes - 4096/4096 Nc: Closing flash driver LPC80x_32.cfx Nt: Dumped 0x1000 bytes in 17ms (about 240kB/s) With the GUI: I hope this help, Erich Re: Unable to save flash image from target board with MCULink probe My diy tc2030 cable did not have the GNDdetect connected. I fixed that and I am now able to read and write flash using either the command line or GUI.  Re: Unable to save flash image from target board with MCULink probe Yes, I see the MCULink kit only had a 10cm cortex cable and adding a tc2030 cable onto that would more than double that length.  BTW, the LPC804 UM mentions that pin0.12 has some ability to recover from a problem state. Is there any further description of how and when to use this feature? Re: Unable to save flash image from target board with MCULink probe Update: It worked fine for an hour but now it is very unreliable. Sometimes I can dump the flash contents but not erase. Sometimes I can dump and erase but not program. Trying to dump, erase, program and verify only worked that one time and never again. I have tried two different tc2030 cables, various wire speeds, and both the CLI and GUI. Even when FlashLink says it succeeded, I usually find when I dump flash that some bytes were not erased or written. I think  a very short cable may be needed.  Re: Unable to save flash image from target board with MCULink probe How long is your cable? It should not exceed ~10 cm. Additionally, what board are you using? Your own/custom one? In that case you might have a connector/trace problem on your board. I hope this helps, Erich Re: Unable to save flash image from target board with MCULink probe A shorter 8cm cable made no difference. When I erase all 0x7F80 bytes and it reports success, I dump all 0x7F80 bytes expecting all 0xFF. Instead the dump is almost all 0x00, so either Flashlink is wrong about the status it reports or there is a HW issue like a partially shorted SWD signal preventing a proper dump of the flash.  
View full article
s32 design studio for arm V2.2 license expired Hello, my S32 Design Studio for ARM v2.2 license has expired 12 Oct 2026. Registration Code:S32DS-IDE-ARM-V2-X_181798567 Product Version: S32 Design Studio for ARM v2.2] Please extend the license. Thank you. Re: s32 design studio for arm V2.2 license expired Hi,  your S32DS license has been extended. Please activate S32DS again with your old code. 
View full article
KW45 automotive bluetooth - drop in module? KiCad? Dear community,  as lesser experienced in the bluetooth radio domain I am looking for your help.  Our projekt needs  bluetooth  connectivity. The KW45 evaluation board has been used for POCs and early tests. Now e want the KW45 right on our board. Using KiCad we are not able to access the NXP reference design. And reading through the documentation lets me humble shrink the size of an ant. Or smaller. Seeing the many Forum posts I wonder if someone could share a ready made design that we could use?  We have a stable 3.3V supply and communicate with UART.  Its an Automotive retrofit application and should be as small as it could be. And thats already everthing we need.  Best regards Michael  KW45  Re: KW45 automotive bluetooth - drop in module? KiCad? Hello @Orbiter, Please note that the KW45 may have less features compared to newer devices. You may also want to consider the KW47 family, which offers several enhancements, including larger memory capacity, a dedicated CM33 radio core running at up to 64 MHz, has a 2.4 GHz Bluetooth Low Energy Core Version 6.x and supports Bluetooth channel sounding. In addition, the KW47 is pin-compatible with the KW45, which can simplify migration efforts. Please refer to AN14796 for more information on the feature differences and migration considerations. We only provide the KW45-EVK design files, along with this community post, which outline the best way to build a PCB first time right with KW45. BR Habib Re: KW45 automotive bluetooth - drop in module? KiCad? I understand its too hard for us. We will move towards a bluetooth modul SOC that basically "bolts on" instead.   Re: KW45 automotive bluetooth - drop in module? KiCad? Hello@Orbiter, If you are interested, you can contact one of our partners, who could help you develop a solution for an automotive environment. Additionally, you can consult the Wi-Fi® + Bluetooth® + 802.15.4 Partner Modules offered by our partners, some of which could also be an option for an automotive environment. However, these modules require a host processor. If this is an option you would like to explore, feel free to provide more information about your application so I can guide you on the available options. BR Habib
View full article
KW45のオートモーティブBluetooth - ドロップインモジュール?KiCad? 親愛なるコミュニティの皆様へ Bluetooth無線分野に関しては経験が浅いため、皆様のご協力をお願いいたします。 私たちのプロジェクトにはBluetoothコネクティビティが必要です。KW45評価ボードはPOCや初期試験に使用されてきました。 今、私たちはKW45を私たちのボードに搭載したいのです。KiCadを使うとNXPのリファレンスデザインにアクセスできません。そしてドキュメントを読むことで、アリの大きさを謙虚に縮めることができます。あるいはもっと小さいサイズ。 フォーラムの投稿が多いのを見て、誰か使える既製のデザインを教えてもらえませんか?安定した3.3V電源を供給し、UARTで通信します。 これはオートモーティブの改修用車なので、できるだけ小さくするべきです。 そして、それだけで私たちに必要なものはすべて揃っている。 よろしくお願いいたします。 マイケル KW45 Re: KW45 automotive bluetooth - drop in module? KiCad? こんにちは、 @Orbiter さん、 KW45は、より新しい機種に比べて機能が少ない場合があることをご了承ください。また、 KW47ファミリ、 も検討すると良いでしょう。これは、より大きなメモリ容量、最大64MHzで動作する専用CM33無線コア、2.4GHzのBluetooth Low Energy Core Version 6.x、Bluetoothチャネルサウンディングのサポートなど、いくつかの強化機能を備えています。さらに、KW47はKW45とピン互換性があり、移行作業を簡素化できます。機能の違いや移行に関する考慮事項の詳細については、 AN14796を参照してください。 私たちは KW45-EVKデザインファイルと、この コミュニティ投稿のみを提供しており、KW45で初めてPCBを作る最良の方法をまとめています。 BR ハビブ Re: KW45 automotive bluetooth - drop in module? KiCad? 私たちには難しすぎることは理解しています。代わりに、基本的に「後付け」できるBluetoothモジュールSoCへと移行していく予定です。 Re: KW45 automotive bluetooth - drop in module? KiCad? こんにちは、 @Orbiter さん、 ご興味があれば、当社の パートナーのいずれかにご連絡ください。オートモーティブ環境向けのソリューション開発をお手伝いいたします。 さらに、パートナーが提供する Wi-Fi® + Bluetooth® + 802.15.4パートナーモジュール もご参照いただけます。これらのモジュールの一部はオートモーティブ環境向けのオプションにも対応可能です。しかし、これらのモジュールはホストプロセッサを必要とします。もしこの選択肢を検討したい場合は、アプリケーションについての詳細をお知らせいただければ、SO私がCAN利用可能な選択肢についてご案内いたします。 BR ハビブ
View full article
WCT-15WTXAUTO Zギャップ こんにちは、NXPサポートチームの皆さん、 情報ありがとうございます。 公開されているドキュメントは確認しましたが、WCT-15WTXAUTOプラットフォームの実際のZギャップ性能データはまだ必要です。 このリファレンスデザインを担当するフィールドアプリケーションエンジニアまたはエンジニアリングチームにつなげていただけますか? 具体的には、Zギャップに対する充電電力の測定値、および石英や花崗岩などの非金属表面を通して動作させた場合のテスト結果を探しています。 私のターゲットアプリケーションは、表面厚さ10〜20mmのカウンタートップ内蔵型ワイヤレス充電器です。 もしこれらのパラメータがWCT-15WTXAUTOで利用できない場合、この用途により適した別のNXP送信機プラットフォームをおすすめしていただけますか? ご協力ありがとうございます。 よろしくお願いいたします。 Re: WCT-15WTXAUTO Z-gap こんにちは、 @Harryk89 さん。 投稿ありがとうございます。このリクエストは、さらなる検討のため、適切なワイヤレス充電開発チームにエスカレーションする必要があります。 サポートプロセスによると、NXPについておよびプロジェクトについて追加情報が必要です。プライバシーを守るために、サポートチケットを作成して、非公開のチャネルでサポートを行うことをお勧めします。 https://support.nxp.com/s/?language=en_US 良い1日を。 BR セレステ
View full article
i.MX 8ULP - MIPI CSI and ISI on M33 (realtime domain) Hello, I'm trying to use a MIPI CSI camera entirely from the real-time domain, with no involvement from the application domain. I've been able to get most of it working, but it looks like the ISI frame completion interrupts are only available in the application domain. Can anyone confirm if that's correct? I can poll the ISI Channel Status register to detect completed frames, but it is not ideal. I would prefer to use the interrupt directly. Forwarding the interrupt from A35 to M33 via the MU would defeat the purpose of the design, so I'd like to avoid that. Is there any other way for M33 to be notified of completed frames without relying on A35-side handlers? i.MX8ULP Re: i.MX 8ULP - MIPI CSI and ISI on M33 (realtime domain) Hello,  Unfortunately, Cortex-M33 cannot handle MIPI-CSI interrupts, only A35 can.
View full article
WCT-15WTXAUTO Z-gap Hello NXP Support Team, Thank you for the information. I have reviewed the publicly available documentation, but I still need the actual Z-gap performance data for the WCT-15WTXAUTO platform. Could you please connect me with a Field Applications Engineer or the engineering team responsible for this reference design? Specifically, I am looking for measured charging power versus Z-gap data and any test results for operation through non-metallic surfaces such as quartz or granite. My target application is a countertop-integrated wireless charger with a surface thickness of 10–20 mm. If these parameters are not available for the WCT-15WTXAUTO, could you recommend another NXP transmitter platform better suited for this application? Thank you for your help. Best regards Re: WCT-15WTXAUTO Z-gap Hello @Harryk89 , Thank you for your post. This request will need to be escalated to the appropriate wireless charging development team for further review. According to our support process, we need some additional information about your company and project. To protect your privacy, I recommend that you create a support ticket so we can assist you through a private channel: https://support.nxp.com/s/?language=en_US  Have a nice day. BR Celeste
View full article
WCT-15WTXAUTO Z型间隙 您好,NXP支持团队, 谢谢你提供的信息。 我已经查阅了公开的文档,但我仍然需要 WCT-15WTXAUTO 平台的实际 Z 间隙性能数据。 请问您能否帮我联系一位现场应用工程师或负责此参考设计的工程团队? 具体来说,我正在寻找测量的充电功率与 Z 间隙数据,以及通过石英或花岗岩等非金属表面进行操作的任何测试结果。 我的目标应用是一款台面集成式无线充电器,表面厚度为 10-20 毫米。 如果 WCT-15WTXAUTO 没有这些参数,您能否推荐另一个更适合此应用的 NXP 发射器平台? 感谢您的帮助。 顺祝商祺! Re: WCT-15WTXAUTO Z-gap 你好@Harryk89 , 感谢您的帖子。该请求需要上报给相应的无线充电开发团队进行进一步审查。 根据我们的支持流程,我们需要一些关于贵公司和项目的其他信息。为了保护您的隐私,我建议您创建支持工单,以便我们通过私密渠道为您提供帮助: https://support.nxp.com/s/?language=en_US 祝你今天过得愉快。 BR 塞莱斯特
View full article
Guiguider 2.0.1 cannot create a C simulator. I installed guiguider 2.0.1 on Windows 10, and it installed and ran normally, and the code generation was also normal. However, when generating the C simulator, I encountered the following error: I want to know if it's because my system is Windows 10 (which requires Windows 11), or if there's some other problem? Re: guiguider2.0.1不能创建C模拟器 HI @tbg  Thanks for providing the error log. GUI Guider 2.0.1 officially supports Windows 11 (64-bit). From the log, the C simulator fails because the bundled GCC/MinGW compiler cannot execute its cc1 component: cc.exe: fatal error: cannot execute 'cc1': CreateProcess: No such file or directory Therefore, I would first recommend testing GUI Guider 2.0.1 on Windows 11. If the same issue still occurs there, we can further investigate the toolchain/installation environment. BR Harry
View full article
i.MX 8ULP - M33 上的 MIPI CSI 和 ISI(实时功能域) 你好, 我正在尝试完全从实时功能域使用 MIPI CSI 摄像头,而无需应用功能域的参与。 大部分功能我已经实现了,但看起来 ISI 帧完成中断仅在应用程序功能域中可用。请问有人能确认一下是否属实吗? 我可以轮询 ISI 通道状态寄存器来检测已完成的帧,但这并不是理想的解决方案。我更倾向于直接使用中断。通过 MU 将 A35 的中断转发到 M33 会违背设计的初衷,所以我希望避免这样做。 除了依赖 A35 端的处理程序之外,还有其他方法可以让 M33 收到帧完成的通知吗? i.MX8ULP Re: i.MX 8ULP - MIPI CSI and ISI on M33 (realtime domain) 你好, 遗憾的是, Cortex-M33 无法处理 MIPI-CSI 中断,只有 A35 可以。
View full article
使用 MCULink 探针无法从目标板保存闪存映像。 W10,链路服务器 26.9.130MCULink 固件 3.174: 我想使用 SWD 从 LPC804 板保存闪存映像。我有一个 MCULink 探针,我安装了包含 LinkFlash 工具的 Linkserver 软件包。这样我就可以将MCULink固件更新到最新版本。 使用 LinkFlash GUI 时,由于出现“连接失败 (Ee42)”错误,我无法从目标板保存闪存映像。未放置探针跳线(SWD)。我选择了“LPC804:”作为设备,但我注意到在其他示例中,通常会指定更完整的部件号和 IDE。我是否需要创建配置文件或安装像 Expresso 这样的 IDE 来解决这个问题,还是更有可能是线缆和目标连接问题? Ns: LinkServer RedlinkMulti 驱动程序 v26.9(2026 年 9 月 18 日 19:34:33 - crt_emu_cm_redlink.exe 版本 1382) PC:(0)读取远程配置 Wc(03)。不支持缓存。 Nc:在 C:\Users\T\AppData\Local\Temp\tmps4ueywdg\crt_directory.xml 中找到通用目录 XML 文件 PC:(5)远程配置完成 Nc:已重新连接到现有 LinkServer 进程。 Nc:连接到探测器 1 核心 0(使用外部启动的服务器)报告: 'Ee(42)。无法连接到核心服务器。 Nc:正在重试…… Nc:已重新连接到现有 LinkServer 进程。 Nc:服务器正常,但无法连接到探测 1 核心 0(尝试 3 次后)- Ee(42)。无法连接到核心服务器。 Ed:02: 连接失败: Ee(42)。无法连接到核心服务器。 Et:31:未连接到芯片的调试端口 PC:(100)目标操作失败 Re: Unable to save flash image from target board with MCULink probe 我还尝试过使用命令行界面(CL)而不是图形用户界面(GUI),但结果并没有什么不同。和你的输出结果对比后,我似乎卡在了这里: Nc:连接到探测器 1 核心 0(使用外部启动的服务器)报告: 'Ee(42)。无法连接到核心服务器。 这似乎是在抱怨探测器,而不是目标。 Re: Unable to save flash image from target board with MCULink probe 我认为你可能遇到了连接问题(物理电缆问题?)。 我在Ubuntu系统上使用过,但同样适用于Win10: /usr/local/LinkServer_26.9.130/LinkServer flash --probe 4FIQSNVD2MICA LPC804: dump 0x00000000 0x00001000 /tmp/memory.bin INFO: Exact match for LPC804: found INFO: Selected device LPC804:LPCXpresso804 INFO: Selected probe #1 4FIQSNVD2MICA (MCU-LINK Pro (r1CF) CMSIS-DAP V3.174) INFO: MCU-Link firmware update `check`: Probe ([4FIQSNVD2MICA] [MCU-LINK Pro (r1CF) CMSIS-DAP V3.174]) is already running the same firmware version as the included firmware version [3.174] Firmware update `check`: not required - forced update can be performed using: `./LinkServer probe #1 update forced` Ns: LinkServer RedlinkMulti Driver v26.9 (Sep 18 2026 19:46:03 - crt_emu_cm_redlink build 1382) Pc: ( 0) Reading remote configuration Wc(03). No cache support. Nc: Found generic directory XML file in /tmp/tmpuhtfp3bl/crt_directory.xml Pc: ( 5) Remote configuration complete Nc: Reconnected to existing LinkServer process. Nc: Probe Firmware: MCU-LINK Pro (r1CF) CMSIS-DAP V3.174 (NXP Semiconductors) Nc: Serial Number: 4FIQSNVD2MICA Nc: VID:PID: 1FC9:0143 Nc: USB Path: 0005:0013:00 Nc: Using memory from core 0 after searching for a good core Pc: ( 30) Emulator Connected Pc: ( 40) Debug Halt Pc: ( 50) CPU ID Nc: debug interface type = CoreSight DP (DAP DP ID 0BC11477) over SWD TAP 0 Nc: processor type = Cortex-M0+ (CPU ID 00000C60) on DAP AP 0 Nc: number of h/w breakpoints = 4 Nc: number of flash patches = 0 Nc: number of h/w watchpoints = 2 Nc: Probe(0): Connected&Reset. DpID: 0BC11477. CpuID: 00000C60. Info: Nc: Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled. Ns: Content of CoreSight Debug ROM(s): Nc: RBASE E00FF000: CID B105100D PID 04000BB4C0 ROM (type 0x1) Nc: ROM 1 E000E000: CID B105E00D PID 04000BB008 Gen SCS (type 0x0) Nc: ROM 1 E0001000: CID B105E00D PID 04000BB00A Gen DWT (type 0x0) Nc: ROM 1 E0002000: CID B105E00D PID 04000BB00B Gen FPB (type 0x0) Nc: NXP: LPC804 Nc: DAP stride is 1024 bytes (256 words) Nc: Inspected v.2 On-chip Flash Memory LPC80x_32.cfx Nc: Image 'LPC80x (32K) Sep 18 2026 18:35:07' Pc: ( 65) Chip Setup Complete Pc: ( 70) License Check Complete Nt: Dumping 'memory.bin' Binary section 0 at 0x00000000 len 0x1000 Nc: Opening flash driver LPC80x_32.cfx Nc: VECTRESET requested, but not supported on ARMv6-M CPUs. Using SOFTRESET instead. Nc: Using SOFT reset to run the flash driver Nc: Flash device supported (32KB = 32*1K at 0x0) Ps: ( 0) at 00000000: 0 bytes - 0/4096 Ps: (100) at 00000000: 4096 bytes - 4096/4096 Nc: Closing flash driver LPC80x_32.cfx Nt: Dumped 0x1000 bytes in 17ms (about 240kB/s) 使用图形用户界面: 希望这能帮到你。 埃里希 Re: Unable to save flash image from target board with MCULink probe 我自制的 TC2030 电缆没有连接 GNDdetect。我已经修复了这个问题,现在可以通过命令行或图形界面读写闪存。 Re: Unable to save flash image from target board with MCULink probe 是的,我看到MCULink套件只有一根10厘米长的Cortex连接线,如果再加一根TC2030连接线,长度就会增加一倍以上。 顺便一提,LPC804 UM 提到引脚 0.12 具有从故障状态恢复的能力。是否有关于如何以及何时使用此功能的更详细说明? Re: Unable to save flash image from target board with MCULink probe 更新:刚开始一个小时运行正常,但现在非常不稳定。有时我可以导出闪存内容,但无法擦除。有时我可以导出和擦除数据,但无法进行编程。尝试进行转储、擦除、编程和验证操作,结果只成功了一次,之后就再也没有成功过。我尝试了两种不同的 tc2030 电缆、各种线速,以及 CLI 和 GUI。即使 FlashLink 显示成功,我通常在转储闪存时发现有些字节没有被擦除或写入。我认为可能需要一根很短的电缆。 Re: Unable to save flash image from target board with MCULink probe 你的电缆有多长?不应超过约10厘米。 另外,你使用的是什么板?您自己/定制的?那样的话,你的板上可能存在连接器/线路问题。 希望这能帮到您, 埃里希 Re: Unable to save flash image from target board with MCULink probe 换用更短的 8 厘米电缆并没有什么区别。当我擦除所有 0x7F80 字节并报告成功时,我转储所有 0x7F80 字节,期望得到全部 0xFF。然而,转储结果几乎全部是0x00,因此要么是Flashlink报告的状态有误,要么是存在硬件问题,例如SWD信号部分短路,导致无法正确转储闪存数据。
View full article
How many Quadrature encoder inputs can an S32K44 and an S32K388 support? I found https://community.nxp.com/t5/S32K/Quadrature-decoder-on-S32K344/m-p/1507580 as well as the application notes on https://www.nxp.com/design/design-center/development-boards-and-designs/MCSPTE1AK344 but I'm struggling to pin down how many quadrature encoders I could instantiate. I have an application where, ideally, I would be able to have 4 independent quadrature decoders. Would either the S32K344 or the S32K388 support that? Re: How many Quadrature encoder inputs can an S32K44 and an S32K388 support? Hello, The S32K3 family does not include a dedicated quadrature decoder peripheral. Instead, the quadrature decoder functionality is implemented using a combination of the LCU, TRGMUX, and eMIOS modules. This is the approach described in the S32K3 Reference Manual and the motor-control example referenced in the community thread. According to the Reference Manual, the incremental encoder example requires two Logic Cells (LC0 and LC1) for a single quadrature decoder implementation. The S32K344 and S32K388 devices provide two LCU instances. However, I have also asked motor control team to provide the feedback. I will update you ASAP. Best regards, Peter Re: How many Quadrature encoder inputs can an S32K44 and an S32K388 support? Hello, Update: Based on the implementation described in the NXP example, the practical limit is three independent quadrature decoders on both S32K344 and S32K388. This solution consumes: 6 TRGMUX input pins (3 × A/B encoder inputs), 6 eMIOS channels capable of MCB operation (for example eMIOS0 CH1-CH6), 3 Logic Cells (one LCU instance). Therefore, three encoder instances can be implemented directly using the demonstrated architecture. A fourth encoder is not directly supported by the same resource mapping. The main limitation is the availability of suitable eMIOS channels operating in MCB mode together with the required signal routing through TRGMUX and LCU. A possible workaround may exist by using the remaining G-type channel (e.g. CH7) together with an X-channel and routing the LCU output externally through a device pin back into the eMIOS X input. For example, on S32K344, PTB2 can be configured as both LCU1_OUT3 and eMIOS0_CH8_X, effectively creating an external loopback path. However, this approach consumes an additional package pin and is not part of the standard demonstrated solution. As a result, 3 quadrature decoders are straightforwardly achievable, while a 4th decoder would require an alternative routing scheme or custom workaround and should be evaluated against the overall pin and peripheral resource usage. Best regards, Peter Re: How many Quadrature encoder inputs can an S32K44 and an S32K388 support? For my application, I don't really need the eMIOS-based interpretation which counts using the timer - I really only need to have the encoder counts available. Is there any configuration which would support having 8 TRGMUX inputs and 4 LCU cells leading to something which just counts up and down?
View full article
どのMatterブランチ/リリースを使うべきか こんにちは、 どのMatterブランチを選ぶべきか少し混乱しています。iMX93でLinux環境で動く際に推奨されている v1.6-branch-imx_matter_2026_q2 と、この2つのブランチ間で注目すべき大きな違いはありますか? __現在 __現在 Re: Which Matter Branch/Release should i use こんにちは@pengyong_zhangさん このブランチの用途と、ELEとgroupcast以外のconnectedhomeipとの違い、そしていくつかの例を知りたいのですが、両者の違いが全く分かりません。v1.6-branch-imx_matter_2026_q2はconnectedhomeipのリリースと比べて古くなっているように見えます。 __現在 __現在 Re: Which Matter Branch/Release should i use こんにちは、 @eldhokkさん v1.6-branch-imx_matter_2026_q2 を使用してください。v1.6.0.0.1のリリースはMCUプラットフォーム(FreeRTOS/Zephyr)向けに設計されています。 B.R
View full article
S32K44 和 S32K388 分别支持多少个正交编码器输入? 我找到了https://community.nxp.com/t5/S32K/Quadrature-decoder-on-S32K344/mp/1507580以及https://www.nxp.com/design/design-center/development-boards-and-designs/MCSPTE1AK344上的应用笔记。但我很难确定我可以实例化多少个正交编码器。 我的应用场景中,理想情况下,我希望能够使用 4 个独立的正交解码器。S32K344 或 S32K388 是否支持此功能? Re: How many Quadrature encoder inputs can an S32K44 and an S32K388 support? 你好, S32K3 系列不包含专用的正交解码器外设。相反,正交解码器功能是通过 LCU、TRGMUX 和 eMIOS 模块的组合来实现的。这是 S32K3 参考手册中描述的方法,也是社区帖子中提到的电机控制示例。 根据参考手册,增量编码器示例需要两个逻辑单元(LC0 和 LC1)来实现单个正交解码器。S32K344 和 S32K388 设备提供两个 LCU 实例。 不过,我也已要求电机控制团队提供反馈意见。 我会尽快通知您最新情况。 顺祝商祺! Peter Re: How many Quadrature encoder inputs can an S32K44 and an S32K388 support? 你好, 更新: 根据 NXP 示例中描述的实现方式,实际限制是在 S32K344 和 S32K388 上各使用三个独立的正交译码器。该方案消耗: 6 个 TRGMUX 输入引脚(3 × A/B 编码器输入), 6 个可进行 MCB 操作的 eMIOS 通道(例如 eMIOS0 CH1-CH6), 3 个逻辑单元(一个 LCU 实例)。 因此,可以使用所展示的架构直接实现三个编码器实例。 第四个编码器无法通过相同的资源映射直接支持。主要限制在于能否提供合适的以 MCB 模式运行的 eMIOS 通道,以及通过 TRGMUX 和 LCU 进行所需的信号路由。 可能存在一种变通方法,即使用剩余的 G 型通道(例如,CH7) 与 X 通道一起,并将 LCU 输出通过设备引脚外部路由回 eMIOS X 输入。例如,在 S32K344 上,PTB2 可以配置为 LCU1_OUT3 和 eMIOS0_CH8_X,从而有效地创建外部环回路径。然而,这种方法会占用一个额外的封装引脚,并且不属于标准演示解决方案的一部分。 因此,实现 3 个正交译码器是完全可行的,而第 4 个译码器则需要采用替代的布线方案或自定义变通方法,并且应该根据整体引脚和外设资源使用情况进行评估。 顺祝商祺! Peter Re: How many Quadrature encoder inputs can an S32K44 and an S32K388 support? 对于我的应用来说,我并不需要基于 eMIOS 的、使用计时器进行计数的解释——我只需要编码器计数即可。是否存在某种配置,能够支持 8 个 TRGMUX 输入和 4 个 LCU 单元,从而实现简单的加减计数?
View full article