Multi Source Translation Content

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multi Source Translation Content

ディスカッション

ソート順:
imx95-evk: NETC on cortex M7 Hi list, According to AN15047 'i.MX 95 Dual-Ethernet on M7 and A55 - Rev. 1.0 — 19 May 2026', i'm trying to use NETC0 on cortex-m7. The chapter '5 Implementation' section 1.b describes how you can affect NETC2 to A55 non-secure cores and NETC0 to cortex-m7. I downloaded the repository https://github.com/nxp-imx/imx-sm.git (hash:eec2328, tag: lf-6.18.37-2.1.0) and take a to *configs/mx95evk.cfg* to update it according to the former chapter. But there are inconsistencies especially concerning the items 'NETC_ECAM0' and 'NETC_ECAM2' which are available in the documentation but *not* in the repository. The file's *configs/mx95evk.cfg* history doesn't provide any reference to NETC_ECAM0 or NETC_ECAM2 i.e 'git log -S NETC_ECAM2' or 'git log -S NETC_ECAM0' return nothin... Do you know where i can find consistent information to define NETC0 to A55 and NETC2 to cortex-m7 please? Can you provide a file *configs/mx95evk.cfg* which is correct for this configuration please? I'm supposed to include the generated build/mx95evk/m33_image.bin to a yocto build with the manifest imx-6.12.49-2.2.0.xml. Is the tag lf-6.18.37-2.1.0 the right one for imx-sm? Thanks. Re: imx95-evk: NETC on cortex M7 Hi, Thank you for your interest in NXP Semiconductor products, You should refer to the following code that defines ECAM https://github.com/nxp-imx/imx-sm/blob/eec232878ab7dd460f5a8f3767d39dc7e9412efa/devices/MIMX95/configtool/netcmix.cfg#L45 In the appnote is stated that the following changes should be made: # modified split definition NETC_ECAM1: PD_NETC, MBC_E0=1.0-3 NETC_ECAM2: PD_NETC, MBC_E0=1.4-7 So, including netcmix.cfg should make it possible. For Yocto and branch of SM, you should select the SM branch of the BSP you are trying it on, if it's the latest BSP or the one where the appnote was tested with. You could modify the code in Yocto source code, create a patch or build it standalone and use imx-mkimage to generate it. make config=mx95evk cfg make config=mx95evk all Regards Re: imx95-evk: NETC on cortex M7 Hello Joseph, Thanks for your answer. After reading carefully the documentation, i reach your conclusion concerning the file netcmix.cfg and i build successfully the binary. So thanks for your confirmation. Now i'm trying to follow "6.2 Setting up Yocto and building the Linux image", especially the step 5. When i try to update the layer i get: build-imx95-19x19-lpddr5-evk$ bitbake-layers add-layer ../sources/meta-imx-dual-eth-m7-a55 NOTE: Starting bitbake server... WARNING: Layer meta-imx-dual-eth-m7-a55 should set LAYERSERIES_COMPAT_meta-imx-dual-eth-m7-a55 in its conf/layer.conf file to list the core layer names it is compatible with. ERROR: BBFILE_PATTERN_meta-imx-dual-eth-m7-a55 not defined ERROR: Parse failure with the specified layer added, exiting. where imx95-yocto-bsp$ ls sources/meta-imx-dual-eth-m7-a55/ conf LICENSE.txt patch-mcuxsdk README.md recipes-bsp recipes-kernel SBOM.spdx.json sources/meta-imx-dual-eth-m7-a55$ git show commit bd42e153e1f39c06ca148dff90362978567a8449 (HEAD -> lf-6.12.49-2.2.0_25.12, origin/lf-6.12.49-2.2.0_25.12, origin/HEAD) [..] Any hint concerning this issue please? Regards Re: imx95-evk: NETC on cortex M7 Hi Joseph, Following chapter "6.3 Setting up the EVK and testing the application" in "AN15047 i.MX 95 Dual-Ethernet on M7 and A55 - Rev. 1.0 — 19 May 2026" i flashed the generated image with uuu -b emmc_all imx-image-core-imx95-19x19-lpddr5-evk.rootfs.wic.zst i don't understand how this command update SM firmware configuration, u-boot on the target permanently For example if i delete the u-boot binary in yocto build and start "bitbake -f imx-image-core" the command terminates properly without any dependency to u-boot. Can you point me out, how to update SM firmware configuration, u-boot to properly open the access of ENETC to cortex-m7 please? It seems that writing imx-image-core-imx95-19x19-lpddr5-evk.rootfs.wic.zst doesn't do the trick. Regards.
記事全体を表示
imx95-evk:皮层 M7 上的 NETC 大家好, 根据AN15047 “i.MX 95 双以太网在 M7 和 A55 上 - 修订版 1.0 — 2026 年 5 月 19 日”,我正在尝试在 cortex-m7 上使用 NETC0 。 “5 实现”章节 1.b 节描述了如何将 NETC2 应用于 A55 非安全内核,以及如何将 NETC0 应用于 cortex-m7。 我下载了仓库https://github.com/nxp-imx/imx-sm.git (hash:eec2328, tag: lf-6.18.37-2.1.0)然后打开*configs/mx95evk.cfg*文件,根据前一章的内容进行更新。 但存在一些不一致之处,特别是关于“NETC_ECAM0”和“NETC_ECAM2”这两个项目,它们在文档中可用,但在存储库中*不可用* 。 文件*configs/mx95evk.cfg*历史记录中没有提供任何关于 NETC_ECAM0 或 NETC_ECAM2 的引用,即“git log -S NETC_ECAM2”或“git log -S NETC_ECAM0”没有任何返回结果…… 请问您知道哪里可以找到关于NETC0对应A55以及NETC2对应cortex-m7的统一信息吗? 请提供文件 *configs/mx95evk.cfg*请问哪种配置才是正确的? 我应该将生成的 build/mx95evk/m33_image.bin 添加到带有清单 imx-6.12.49-2.2.0.xml的yocto 版本中。 标签lf-6.18.37-2.1.0哪个型号适合 imx-sm? 谢谢。 Re: imx95-evk: NETC on cortex M7 您好, 感谢您对恩智浦半导体产品的关注, 您应该参考以下定义 ECAM 的代码:https://github.com/nxp-imx/imx-sm/blob/eec232878ab7dd460f5a8f3767d39dc7e9412efa/devices/MIMX95/configtool/netcmix.cfg#L45 应用说明中指出,应进行以下更改: # modified split definition NETC_ECAM1: PD_NETC, MBC_E0=1.0-3 NETC_ECAM2: PD_NETC, MBC_E0=1.4-7 因此,包含 netcmix.cfg 文件应该可以实现这一点。 对于 Yocto 和 SM 分支,您应该选择您正在尝试的电路板支持包的 SM 分支,如果它是最新的电路板支持包或应用笔记中测试的电路板支持包。您可以修改 Yocto 源代码中的代码,创建补丁,或者将其独立构建并使用 imx-mkimage 生成独立组网 \(SA\)。 make config=mx95evk cfg make config=mx95evk all 此致 Re: imx95-evk: NETC on cortex M7 你好,约瑟夫, 谢谢你的回答。 仔细阅读文档后,我认同您关于netcmix.cfg文件的结论,并成功构建了二进制文件。 谢谢你的确认。 现在我正在尝试遵循“6.2设置 Yocto 并构建 Linux 镜像”,特别是第 5 步。 当我尝试更新层时,出现以下错误: build-imx95-19x19-lpddr5-evk$ bitbake-layers add-layer ../sources/meta-imx-dual-eth-m7-a55 注意:Bitbake 服务器正在启动…… 警告:层 meta-imx-dual-eth-m7-a55 应在其 conf/layer.conf 文件中设置 LAYERSERIES_COMPAT_meta-imx-dual-eth-m7-a55,以列出与其兼容的核心层名称。 错误:未定义 BBFILE_PATTERN_meta-imx-dual-eth-m7-a55 错误:添加指定层时解析失败,程序退出。 其中: imx95-yocto-bsp$ ls sources/meta-imx-dual-eth-m7-a55/ conf LICENSE.txt patch-mcuxsdk README.md 配方-电路板支持包。 配方-kernel SBOM.spdx.json sources/meta-imx-dual-eth-m7-a55$ git show 提交 bd42e153e1f39c06ca148dff90362978567a8449 (HEAD -> lf-6.12.49-2.2.0_25.12,origin/lf-6.12.49-2.2.0_25.12,起源/HEAD) [...] 请问关于这个问题有什么线索吗? 此致 Re: imx95-evk: NETC on cortex M7 嗨,约瑟夫, 紧接第6.3章在“AN15047 i.MX 95 Dual-Ethernet on M7 and A55 - Rev.中设置 EVK 并测试应用程序”1.0 — 2026年5月19日“我刷入了生成的镜像” uuu -b emmc_all imx-image-core-imx95-19x19-lpddr5-evk.rootfs.wic.zst 我不明白这条命令是如何永久更新目标设备上的SM固件配置和u-boot的。 例如,如果我在 yocto 版本中删除u-boot 二进制文件并启动“bitbake -f imx-image-core”,该命令会正常终止,而不会依赖于 u-boot。 请问如何更新SM固件配置和u-boot,才能正确打开ENETC对cortex-m7的访问权限? 看来写入imx-image-core-imx95-19x19-lpddr5-evk.rootfs.wic.zst并不能解决问题。 此致问候
記事全体を表示
IMX95-EVK:Cortex M7上のNETC こんにちは、 AN15047『i.MX 95 Dual-イーサネット on M7 and A55 - Rev. 1.0 — 2026年5月19日』によると、Cortex-m7でNETC0を使おうとしています。 第5章「実装」セクション1.bでは、NETC2からA55非セキュアコア、NETC0からcortex-m7への影響方法が説明されています。 リポジトリhttps://github.com/nxp-imx/imx-sm.git (ハッシュ: eec2328、タグ: lf-6.18.37-2.1.0) をダウンロードしました。そして、 *configs/mx95evk.cfg*に移動して、前の章に従って更新します。 しかし、特にドキュメントにはあるもののリポジトリ には存在しない「NETC_ECAM0」と「NETC_ECAM2」という項目に関して矛盾があります。 ファイルの内容は*configs/mx95evk.cfg* です。履歴には NETC_ECAM0 または NETC_ECAM2 への参照が一切ありません。つまり、「git log -S NETC_ECAM2」または「git log -S NETC_ECAM0」を実行しても何も返されません。 NETC0からA55、NETC2からcortex-m7までを定義するための一貫した情報をどこで見つけられますか? ファイルを提供できますか *configs/mx95evk.cfg*この構成の場合、どちらが正しいでしょうか? 生成されたビルド/mx95evk/m33_image.binを 、マニフェストimx-6.12.49-2.2.0.xml付きのYoctoビルドに含めるべきです。 タグはlf-6.18.37-2.1.0ですか?imx-smに最適なのはどれですか? ありがとうございます。 Re: imx95-evk: NETC on cortex M7 こんにちは、 NXP Semiconductors製品にご関心いただきありがとうございます。 ECAMを定義する以下のコードを参照してください。https://github.com/nxp-imx/imx-sm/blob/eec232878ab7dd460f5a8f3767d39dc7e9412efa/devices/MIMX95/configtool/netcmix.cfg#L45 アプリケーションノートには、以下の変更を行う必要があると記載されています。 # modified split definition NETC_ECAM1: PD_NETC, MBC_E0=1.0-3 NETC_ECAM2: PD_NETC, MBC_E0=1.4-7 ですので、netcmix.cfgを含めることで可能になるはずです。 YoctoとSMのブランチの場合は、試しているBSPのSMブランチを選ぶべきです。最新のBSPか、Appnoteがテストされたものであれば。Yoctoのソースコードでコードを修正したり、パッチを作成したり、単体で構築してimx-mkimageで生成することもできます。 make config=mx95evk cfg make config=mx95evk all よろしくお願いします。 Re: imx95-evk: NETC on cortex M7 こんにちは、ジョセフさん。 ご回答ありがとうございます。 ドキュメントを注意深く読んだ結果、 netcmix.cfg ファイルに関する結論に達し、バイナリを成功裏に構築しました。 SO、ご確認ありがとうございます。 今は「6.2」に従おうとしていますYoctoの設定とLinuxイメージのビルディング」、特にステップ5について。 レイヤーを更新しようとすると、次のような結果が出ます: build-imx95-19x19-lpddr5-evk$ bitbake-layers add-layer ../sources/meta-imx-dual-eth-m7-a55 注:bitbakeサーバーを起動しています... 警告: レイヤー meta-imx-dual-eth-m7-a55 は、互換性のあるコア レイヤー名をリストするために、conf/layer.conf ファイルで LAYERSERIES_COMPAT_meta-imx-dual-eth-m7-a55 を設定する必要があります。 エラー: BBFILE_PATTERN_meta-imx-dual-eth-m7-a55 が定義されていません エラー: 指定されたレイヤーを追加した状態で解析に失敗しました。終了します。 ここで、 IMX95-yocto-bsp$ LS ソース/meta-imx-dual-eth-m7-a55/ conf LICENSE.txt patch-mcuxsdk README.md recipes-bsp recipes-kernel SBOM.spdx.json sources/meta-imx-dual-eth-m7-a55$ git show コミット bd42e153e1f39c06ca148dff90362978567a8449 (HEAD -> lf-6.12.49-2.2.0_25.12、origin/lf-6.12.49-2.2.0_25.12、起源/HEAD) [..] この件に関して何かヒントがあれば教えてください。 よろしくお願いします。 Re: imx95-evk: NETC on cortex M7 こんにちは、ジョセフさん。 「6.3」章の後「EVK のセットアップとアプリケーションのテスト」(「AN15047 i.MX 95 デュアルイーサネット on M7 および A55 - Rev.1.0 — 2026年5月19日" 生成されたイメージをフラッシュしました uuu -b emmc_all imx-image-core-imx95-19x19-lpddr5-evk.rootfs.wic.zst このコマンドがSMファームウェア構成、ターゲット上のu-bootを永続的に更新する方法が理解できません 例えば、yocto ビルドで u-boot バイナリ を削除 して 「bitbake -f imx-image-core 」を起動すると、コマンドは you-boot に依存しないまま正しく終了します。 SMのファームウェア設定をアップデートする方法を教えてもらえますか?U-bootでENETCからcortex-m7へのアクセスを正しく開く方法を教えてもらえますか? imx-image-core-imx95-19x19-lpddr5-evk.rootfs.wic.zstを書き込んでも解決しないようです。 よろしくお願いします。
記事全体を表示
i.MX 93 – 预构建的 Ubuntu/Debian Linux 镜像和定制载板支持 您好,NXP支持团队, 我正在评估 i.MX 93 平台在 EVSE 应用方面的性能,并发现了EVSE-IMX93 开发套件。 我想澄清一下可用的 Linux 镜像及其与潜在的定制载板设计的兼容性。 我们的目标是使用 MCIMX93-SOM,并基于 NXP 原有的载板设计开发一款简化的定制载板。我们将保留相同的SOM连接器和引脚分配,同时移除未使用的外围设备和电路。 由于我对 i.MX 处理器平台和基于 Yocto 的开发还比较陌生,我正在寻找一个简单易用的 Linux 解决方案来入门,然后再进行自定义。 请问您能否澄清以下问题? 是否有适用于 i.MX 93 的现成 Ubuntu 或 Debian 13 (Trixie) 镜像?最好是通用服务器/最小 Linux 镜像。 这个镜像可以直接下载并刷入microSD卡来启动板,而无需Yocto构建吗? 提供的镜像是否支持标准的 Linux 功能,例如apt 、Python 3、SSH、systemd 和网络功能? 它是否支持CAN/CAN-FD (SocketCAN)、Wi-Fi、以太网和 MQTT ?是否可以使用apt安装 Mosquitto 等软件包? 在我们保留原有SOM连接器和相关硬件连接的前提下,能否将相同的预构建镜像用于我们提出的定制载板?是否只需要更改设备树或配置? 如果有这样的镜像文件,能否分享一下直接下载链接、支持的板信息和安装说明? 我们的目标是将 i.MX 93 用作运行 EVerest 框架和其他 EVSE 应用软件的通用 Linux 平台,同时避免最初维护 Yocto 构建的需要。 谢谢你的帮助。 此致敬礼 加内什·巴格瓦特 Re: i.MX 93 – Prebuilt Ubuntu/Debian Linux Image and Custom Carrier Board Support 你好, 是的,有一个与 i.mx93 平台兼容的 Debian Linux SDK,您可以通过“Flexbuild”的实现来构建镜像,而不是使用 Yocto,然后使用 flexinstaller 工具刷写镜像。有关该发行版支持的软件包的更多信息,请参阅此处: DEBIAN-SDK Debian 软件版本说明 LDLSDK_26.06
記事全体を表示
S32K376NHT1MJBST:适用的功率估算器和单电源电流数据 你好, 请问您能否提供适用于 S32K376NHT1MJBST 的功率估算工具和供电电流数据? S32K-PET 是否支持这种特定衍生物?应该使用哪些工具和设备数据集版本?如果不支持,NXP 目前推荐的方法是什么? 对于采用外部 NMOS V11 稳压器配置的外部供电 V15,应如何将报告的需求分配给 V15、V11、VDD_HV_A/B 和其他模拟/偏置电源?请明确哪些项目包含在内,哪些项目不包含在内,特别是调节器损耗、共享核心/锁定步进需求、I/O 负载和外围电流,以免重复计算。 哪些适用的公共文件、数据或表征方法涵盖了最坏情况下的供电电流与电压/温度的关系,以及RESET、启动、唤醒和时钟/模式变化期间的峰值?请区分典型/平均估价和保证限额,并说明其适用条件。 已审核公开的PET页面和设置指南。他们的家族级支持清单和初始平均功率范围并未明确指出具体的衍生品或所有实物供应贡献。我们寻求的是适用的资源和方法,而不是没有明确操作规范的特定应用的当前结果。 如果这些信息不公开,请指出相应的公开资料或支持途径。 谢谢! Re: S32K376NHT1MJBST: applicable power estimator and per-supply current data 你好@JonasGranlund , 1.目前,S32K PET 工具不支持 S32K39/37/36 设备。推荐的方法是参考 S32K396 的数据手册(修订版)。5)关于供应电流数据,具体而言: 6.7 电源电流(待机和运行模式表) 6.9 循环唤醒平均电流计算 2. 数据手册中的电流表分别报告以下各轨的电流: VDD_HV_A被列为主 I/O 和模拟电源,它覆盖 VDD_HV_A 组中的两个 I/O 焊盘和所有模拟模块。 VDD_HV_B是辅助 I/O 电源,仅覆盖 VDD_HV_B 组中的 I/O 焊盘。您可以参考参考手册中的“S32K39_and_S32K37_IOMUX.xlsx”附件,以确定哪个引脚属于哪个电源域。 V11由 V15 利用外部 NMOS 产生。进入LPM模式前,应关闭外部V1.5电源。 测量中不包括 I/O 负载电流。实际的 I/O 电流需求将取决于应用程序中的 I/O 配置。请参阅 S32K39 数据表中的直流特性表。 数据表中核心供电量中包含了锁步/双核需求;由于没有根据核心负载单独制定的规格,因此功耗规定为相同。 3. 数据表中的数值包括环境温度、典型值和最大值。 据我所知,没有专门针对 S32K39 的文件详细说明最坏情况下的电流、RESET 期间的峰值等。然而, S32K3 低功耗电源管理单元 AN 和演示文档提供了电源模式转换、低功耗电源模式下的时钟操作、硬件注意事项和静态电流。它更侧重于家族层面,一般参考 S32K3xx,而不是 S32K39-37-36 的具体细节。 我还通过社区分享 S32K3 低功耗实验室演示文稿向您发送了一条私信,其中解释了 S32K3 的低功耗特性和注意事项。 此致, 朱利安
記事全体を表示
Battery pack active balancing solution Hello, I couldn't find a solution for active battery pack balancing on the website, only a demonstration video of a battery energy storage solution. I also couldn't find any related articles on the forum. Do you have any recommendations? Thank you. Re: 电池包主动均衡方案 That's too outdated. Active balancing should be the future trend for new energy sources. Re: 电池包主动均衡方案 Hi Bob We don't manufacture active balancing ICs, and there's not much information available on this topic. The attached file is an older app note and hopefully will be helpful.
記事全体を表示
ライセンスに関する質問:LA_OPTオンラインコードホスティングv1.4(SR250 UWBIoT)—結果の共有、AIツール、独自の こんにちは、 NXPのサポートチャットのアドバイスで、ライセンスチームのためにここにライセンスに関する質問を投稿します。  github.com/nxp-uwb/sr250-uwbiot-zephyr と github.com/nxp-appcodehub/an-sr250-uwb-plug-and-play-demo のソフトウェアを使って、SR250UWBSHIELD + FRDM-RW612を使った研究プロトタイプを計画しています(SR250 FW 01.41.04)どちらも「LA_OPT_Online Code Hosting NXP_Software_License – v1.4 May 2025」に基づいています。私はまだライセンスに同意しておらず、まず以下の点について明確にしておきたいと思います。 1.セクション3.8:「ライセンスソフトウェアの使用に関連するレポート」の配布制限は、私自身の測定結果、ログ、テストレポートにも適用されるのでしょうか?試験機関や外部査読者、お客様、あるいは科学論文に共有するのが良いでしょう。  2.AI ツール (セクション 3.2 / 3.8): AI アシスタント (例:ChatGPT、クロード)。(a)自分の結果やレポートをそのようなサービスと共有してもよろしいですか?(b)AIアシスタントにライセンスソフトウェアやNXPのドキュメント(例:Rancyd Software)を読み、扱ってもらえますか?UM12508)を自分のコンピューターでダウンロードするか、クラウドサービス経由でダウンロードするか? 3.自社ソフトウェア(セクション1.3 / 5):CIRデータのみを受け取りNXPコードを含まないPC側の信号プロセッシングソフトウェアは「派生作品」と言えますか?セクション5.1~5.2を実行してくださいそれに適用しますか? 4.製品(セクション2.1):v1.4はSR250(NXPボード、サードパーティ製SR250モジュール、または自分の基板上の裸SR250UK)とこのファームウェア、そしてお客様向けのファームウェアアップデートファイルを含みたデバイスを販売することを許可していますか?それとも、別途契約が必要ですか? 5.ライセンシー:今個人としてライセンスを受け入れた場合、後で設立する可能性のある会社に引き継がれますか?  書面での回答や、NXPのライセンス・法務チームへのお問い合わせをいただけると大変ありがたいです。ありがとう!
記事全体を表示
许可问题:LA_OPT 在线代码托管 v1.4 (SR250 UWBIoT) — 共享结果、AI 工具、自有 你好, 根据 NXP 支持聊天软件的建议,我在这里发布我的许可问题,以便向许可团队寻求帮助。 我计划使用 SR250UWBSHIELD + FRDM-RW612 构建一个研究原型,并使用来自 github.com/nxp-uwb/sr250-uwbiot-zephyr 和 github.com/nxp-appcodehub/an-sr250-uwb-plug-and-play-demo 的软件。(SR250 FW 01.41.04)。两者均受“LA_OPT_Online Code Hosting NXP_Software_License – v1.4 May 2025”保护。我尚未接受许可协议,因此想先澄清以下几点: 1.第 3.8 节:关于分发“与使用许可软件相关的报告”的限制是否涵盖我自己的测量结果、日志和测试报告?我会将它们分享给测试实验室、外部审稿人、客户或在科学出版物上发表。 2.AI 工具(第 3.2 节 / 3.8 节):我使用 AI 助手进行开发(例如,ChatGPT,克劳德)。我可以 (a) 与此类服务共享我的结果和报告,以及 (b) 让 AI 助手读取和使用许可软件和 NXP 文档(例如,(UM12508)是在我自己的电脑上还是通过云服务安装的? 3.自己的软件(第 1.3 / 5 节):我自己的 PC 端信号处理软件,只接收 CIR 数据,不包含 NXP 代码,是否属于“衍生作品”?完成第 5.1 至 5.2 节适用于它吗? 4.产品(第 2.1 节):v1.4 是否允许销售带有 SR250(NXP 板、第三方 SR250 模块或裸 SR250UK 芯片,安装在我自己的 PCB 上)和此固件的设备,包括为客户提供的固件更新文件?或者需要另行签订协议? 5.被许可方:如果我现在以个人身份接受许可,该许可是否适用于我以后可能成立的公司? 非常感谢您能提供书面答复,或者提供恩智浦(NXP)授权/法律团队的联系方式。谢谢你!
記事全体を表示
MC33PF8100A0TS 参考資料 こんにちは。MC33PF8100A0tsの設計参考資料はありますか? 1. プログラミングポートをどのように設計すればよいか? 2. 参考設計図はありますか? ご確認いただけますでしょうか?ありがとうございます。 Re: MC33PF8100A0TS参考资料 PF8100のGUIを使用してソフトウェアをフラッシュした後、インターフェースの接続図が記載されているユーザーマニュアルをダウンロードしてください。 PF8200/PF8100プログラミングボード | NXPセミコンダクターズ FRDM-KL25Zはこの制御基板を使用しており、そのプロセスは簡単ではありません。ソケットに直接コードを書き込む方が良いでしょう。 Re: MC33PF8100A0TS参考资料 はい、初期プロトタイプのデバッグ段階では、チップは基板に半田付けされています。 Re: MC33PF8100A0TS参考资料 こんにちは、ボブ 製品の回路基板をプログラムする予定ですか?
記事全体を表示
FS2643D H世代:S32K376NHT1MJBSTの本格的なOTP/オーダー可能なサポート こんにちは、 S32K376NHT1MJBST対応するFS2643D H世代の生産構成について教えていただけますか? 1. この組み合わせに対応する、既存のプログラム済み生産発注書およびOTP構成はありますか?もしそうであれば、正確な注文コード、OTP ID/リビジョン、該当する設定レポートおよびプログラミング/設定ファイルのリンクを特定してください。 2. カスタムOTPが必要な場合、互換性のある構成と本番プログラム部品を得るために、どのNXPまたは認可チャネルプロセスを使用すべきか?これは、ブランクデバイスを用いたエンジニアリングのエミュレーション/プログラミングとは区別してください。 3. MFS2643HMDA0ADとMFS2643HMDA0UDは該当するブランク開発バリアントであり、ADとUDの違いはパッケージ、組み立て、ご注文の適用性にどのような影響を与えるか? 公開されているFS26標準構成例とS32K376POCページを確認しました。後者はFS2633ベースのボードについて説明しており、その構成はFS2643Dにそのまま適用できるとは想定されていません。これらの詳細が公開されていない場合は、正確な該当書類または適切なサポートルートをご指摘ください。 よろしくお願いします。 Re: FS2643D H-generation: production OTP/orderable support for S32K376NHT1MJBST こんにちは、ジョナス 以下のコメントをご覧ください。 1. この組み合わせに対応する、既存のプログラム済み生産発注書およびOTP構成はありますか?もしそうであれば、正確な注文コード、OTP ID/リビジョン、該当する設定レポートおよびプログラミング/設定ファイルのリンクを特定してください。 [gw]以下は推奨事項です。まず、このパワーツリーがS32K376に適しているかどうかを評価してください。 https://www.nxp.com/products/FS26 2. カスタムOTPが必要な場合、互換性のある構成と本番プログラム部品を得るために、どのNXPまたは認可チャネルプロセスを使用すべきか?これは、ブランクデバイスを用いたエンジニアリングのエミュレーション/プログラミングとは区別してください。 [gw]上記の回答をご覧ください。 3. MFS2643HMDA0ADとMFS2643HMDA0UDは該当するブランク開発バリアントであり、ADとUDの違いはパッケージ、組み立て、ご注文の適用性にどのような影響を与えるか? [gw] A0 は空白部分を意味します。以下は FS26 の命名規則です。UD サフィックスは見つかりませんでした。 回路図デザインが終わったら、再度確認のために当社にご連絡ください。 よろしくお願いします!
記事全体を表示
S32K376NHT1MJBST: applicable power estimator and per-supply current data Hello, Could you please identify the applicable power-estimation tool and supply-current data for S32K376NHT1MJBST? Does S32K-PET support this exact derivative? Which tool and device-dataset revisions should be used? If it is not supported, what is the recommended current NXP method? For externally supplied V15 with the external NMOS V11 regulator arrangement, how should reported demand be attributed to V15, V11, VDD_HV_A/B and other analog/bias supplies? Please identify what is included or excluded, especially regulator losses, shared core/lockstep demand, I/O loading and peripheral currents, so these are not counted twice. Which applicable public documents, data or characterization method cover worst-case supply current versus voltage/temperature, and peaks during reset, startup, wake and clock/mode changes? Please distinguish typical/average estimates from guaranteed limits and identify their conditions. The public PET page and setup guide have been reviewed. Their family-level support listing and initial average-power scope do not identify the exact derivative or all physical-supply contributions. We are seeking the applicable sources and method, not an application-specific current result without a defined operating profile. Please point to the appropriate public material or support route if these details are not public. Thank you. Re: S32K376NHT1MJBST: applicable power estimator and per-supply current data Hello @JonasGranlund, 1. As of now, the S32K PET tool does not support S32K39/37/36 devices. The recommended method is to refer to S32K396's Data Sheet (Rev. 5) for supply current data, specifically: 6.7 Supply currents (Standby and RUN mode tables) 6.9 Cyclic wake-up average current calculation 2. The datasheet supply current tables report current at the following rails independently: VDD_HV_A is catalogued as the main I/O and analog supply, and it covers both I/O pads in the VDD_HV_A bank and all analog blocks.  VDD_HV_B is the secondary I/O supply and covers I/O pads in the VDD_HV_B bank only. You can refer to "S32K39_and_S32K37_IOMUX.xlsx" attachment inside the Reference Manual in order to identify which pin belongs to which power domain. V11 is generated by V15 using external NMOS. The external V1.5 power supply should be turned off before entering LPM mode. IO load current is not included in measurements. The actual current requirements for IOs will depend on the I/O configuration in the application. Refer to the DC characteristics tables in the S32K39 Data sheet. Lockstep/dual-core demand is included in the core supply figures in the data sheet; the power consumption is specified to be the same because there are no separate specifications depending on the load of the cores. 3. Data Sheet values include ambient temperature, typical and maximum values.  As far as I know, there are no specific S32K39 documents detailing worst-case scenario currents, peaks during reset, etc. However, S32K3 Low Power Management AN and demos document provide power mode transitions, clock operation in low-power modes, hardware considerations and quiescent current. It is focused on a more family-level, referencing S32K3xx in general, rather than S32K39-37-36 specifics. I've also sent you a private message in community sharing S32K3 Low Power Lab presentation, which explains S32K3 low power behavior and considerations. Best regards, Julián
記事全体を表示
トリメンションSR250 — 試作前のライセンスとレーダーデータの質問 FRDM-RW612と「SR250 UWBIoT for Zephyr」(github.com/nxp-uwb/sr250-uwbiot-zephyr)を用いたSR250UWBSHIELDを基に研究プロトタイプを計画しています。これはタグフリーのUWBレーダーで、ビルディング資材の背後にいる人を探知し、検索救助に使用されます。ソフトウェアライセンス(LA_OPT_Online Code Hosting v1.4)を受け入れる前に、以下の5つの質問に簡潔にお答えいただけると幸いです。 1. レーダーデータ:レーダーモードでSR250は複雑なI/Q(位相保持)としてCIRをホストに届けますか?複数の受信アンテナからCIRを同時にキャプチャし、ホストが到着角度を推定できるのでしょうか? 2. 結果共有:セクション3.8は「ライセンスソフトウェアの使用に関連する報告」をNXP以外の者に配布することを禁止しています。これは、私自身の測定結果やテストラボ、外部査読者、お客様、科学論文と共有したログも含まれますか?もしそうなら、NXPは書面での許可を出せますか? 3. 自社ソフトウェア:私自身のホスト側信号プロセッシング(PC上で動作し、CIRデータを受信し、NXPコードを含まない)は、セクション1.3および5の下で「派生作品」として扱われますか? 4. 製品経由:プロトタイプが成功した場合、v1.4は自社のPCBにSR250を搭載した機器の商業販売を許可し、お客様向けのファームウェアアップデートも含めて提供できますか?それとも別途合意が必要でしょうか? 5. コンプライアンス:SR250UWBSHIELDのEU適合宣言全文はどこで入手できますか?レーダーモードはカバーされていますか? ご返信よろしくお願いします。 Re: Trimension SR250 — licensing and radar data questions before prototyping こんにちは、 プライベートメッセージを送りました! よろしくお願いいたします。 リカルド
記事全体を表示
FS2643D H 代:生产 OTP/可订购支持 S32K376NHT1MJBST 你好, 请问能否说明一下 S32K376NHT1MJBST 支持的 FS2643D H 代生产配置? 1. 是否存在针对此组合的已编程生产可订购和OTP配置?如果是,请提供确切的订单代码、OTP ID/版本以及适用的配置报告和编程/配置文件链接。 2. 如果需要定制 OTP,应该使用 NXP 的哪个流程或授权渠道来获得兼容的配置和生产编程部件?请将此与空白设备工程仿真/编程区分开来。 3. MFS2643HMDA0AD 和 MFS2643HMDA0UD 是否是适用的空白开发变体?它们的 AD/UD 差异对封装、组装和订购适用性有何意义? 已审查公开的 FS26 标准配置示例和 S32K376POC 页面。后者描述的是基于 FS2633 的板;其配置不被认为可以转移到 FS2643D。如果这些信息不公开,请指出适用的具体文件或正确的求助途径。 谢谢! Re: FS2643D H-generation: production OTP/orderable support for S32K376NHT1MJBST 嗨,乔纳斯 请看下方评论: 1. 是否存在针对此组合的已编程生产可订购和OTP配置?如果是,请提供确切的订单代码、OTP ID/版本以及适用的配置报告和编程/配置文件链接。 [gw]以下是推荐配置,请先评估此电源树是否适用于 S32K376。 https://www.nxp.com/products/FS26 2. 如果需要定制 OTP,应该使用 NXP 的哪个流程或授权渠道来获得兼容的配置和生产编程部件?请将此与空白设备工程仿真/编程区分开来。 [gw]请看上面的答案。 3. MFS2643HMDA0AD 和 MFS2643HMDA0UD 是否是适用的空白开发变体?它们的 AD/UD 差异对封装、组装和订购适用性有何意义? [gw] A0 表示空白部分,以下是 FS26 的名称规则,我没有找到 UD 后缀。 请注意,原理图设计完成后请发送给我们进行复核。 谢谢您!
記事全体を表示
Trimension SR250 — licensing and radar data questions before prototyping I am planning a research prototype based on the SR250UWBSHIELD with FRDM-RW612 and "SR250 UWBIoT for Zephyr" (github.com/nxp-uwb/sr250-uwbiot-zephyr). It is a tag-free UWB radar for detecting people behind building materials, for search-and-rescue use. Before accepting the software license (LA_OPT_Online Code Hosting v1.4), I would appreciate short answers to five questions: 1. Radar data: In radar mode, does the SR250 deliver CIR to the host as complex I/Q (phase preserved)? Can it capture CIR from more than one RX antenna simultaneously, so that the host can estimate angle of arrival? 2. Sharing results: Section 3.8 prohibits distributing "reports associated with the use of the Licensed Software" to anyone other than NXP. Does this cover my own measurement results and logs shared with test labs, external reviewers, customers or scientific publications? If so, can NXP give written permission? 3. Own software: Is my own host-side signal processing (running on a PC, receiving CIR data, containing no NXP code) treated as a "Derivative Work" under Sections 1.3 and 5? 4. Product path: If the prototype succeeds, does v1.4 allow commercial sale of a device with SR250 on my own PCB, including firmware updates for customers? Or would a separate agreement be needed? 5. Compliance: Where can I find the full EU Declaration of Conformity for SR250UWBSHIELD? Does it cover radar mode? Thank you very much. Re: Trimension SR250 — licensing and radar data questions before prototyping Hello, I sent you a private message! Regards, Ricardo
記事全体を表示
Trimension SR250——原型制作前的许可和雷达数据问题 我正在计划基于 SR250UWBSHIELD、FRDM-RW612 和“SR250 UWBIoT for Zephyr”(github.com/nxp-uwb/sr250-uwbiot-zephyr)的研究原型。它是一种无需标签的超宽带雷达,用于探测建筑物材料后面的人员,可用于搜救。在接受软件许可协议(LA_OPT_Online Code Hosting v1.4)之前,我希望您能简要回答以下五个问题: 1. 雷达数据:在雷达模式下,SR250 是否以复数 I/Q(相位保持)的形式向主机提供 CIR?它能否同时从多个接收天线捕获 CIR,以便主机可以估计到达角? 2. 分享结果:第 3.8 节禁止向 NXP 以外的任何人分发“与使用许可软件相关的报告”。这是否涵盖我自己的测量结果和与测试实验室、外部审阅者、客户或科学出版物共享的日志?如果可以,恩智浦能否提供书面许可? 3. 自己的软件:我自己的主机端信号处理(在 PC 上运行,接收 CIR 数据,不包含 NXP 代码)是否被视为第 1.3 节和第 5 节中的“衍生作品”? 4. 产品路径:如果原型成功,v1.4 是否允许我在自己的 PCB 上进行带有 SR250 的设备的商业销售,包括为客户提供固件更新?或者是否需要另行签订协议? 5. 合规性:我可以在哪里找到 SR250UWBSHIELD 的完整欧盟符合性声明?它是否支持雷达模式? 非常感谢。 Re: Trimension SR250 — licensing and radar data questions before prototyping 你好, 我给你发了私信! 此致, 里卡多
記事全体を表示
Licensing question: LA_OPT Online Code Hosting v1.4 (SR250 UWBIoT) — sharing results, AI tools, own Hello,  On the advice of NXP support chat, I'm posting my licensing questions here for the licensing team.  I plan a research prototype with SR250UWBSHIELD + FRDM-RW612, using software from github.com/nxp-uwb/sr250-uwbiot-zephyr and github.com/nxp-appcodehub/an-sr250-uwb-plug-and-play-demo (SR250 FW 01.41.04). Both are under "LA_OPT_Online Code Hosting NXP_Software_License – v1.4 May 2025". I have not accepted the license yet and would like to clarify the following first:  1. Section 3.8: Does the restriction on distributing "reports associated with the use of the Licensed Software" cover my own measurement results, logs and test reports? I would share them with a test laboratory, external reviewers, customers or in a scientific publication.  2. AI tools (Sections 3.2 / 3.8): I develop with AI assistants (e.g. ChatGPT, Claude). May I (a) share my results and reports with such services, and (b) let an AI assistant read and work with the Licensed Software and NXP documentation (e.g. UM12508), on my own computer or via a cloud service?  3. Own software (Sections 1.3 / 5): Is my own PC-side signal-processing software, which only receives CIR data and contains no NXP code, a "Derivative Work"? Do Sections 5.1–5.2 apply to it?  4. Product (Section 2.1): Does v1.4 allow selling a device with the SR250 (NXP board, third-party SR250 module or bare SR250UK on my own PCB) and this firmware, including firmware update files for customers? Or is a separate agreement required?  5. Licensee: If I accept the license as an individual now, does it carry over to a company I may set up later?  A written answer, or a contact at the NXP licensing/legal team, would be much appreciated. Thank you!
記事全体を表示
MC33PF8100A0TS参考资料 你好,又MC33PF8100A0ts的设计参考资料吗?  1. 如何设计烧写口? 2.参考设计原理图有吗? 帮忙看看,谢谢。 Re: MC33PF8100A0TS参考资料 用我们的PF8100的GUI 烧录,然后下载usermanual上面有接口的连接示意图: PF8200/PF8100 Programming Board | NXP Semiconductors FRDM-KL25Z用的是这个控制板,这一套操作下来也不简单,还不如直接在socket上烧写。 Re: MC33PF8100A0TS参考资料 是的,初期样板调试是芯片焊在板子上。 Re: MC33PF8100A0TS参考资料 HI Bob 您是要在产品的板子上做烧写吗?
記事全体を表示
FS2643D H-generation: production OTP/orderable support for S32K376NHT1MJBST Hello, Could you please clarify the supported FS2643D H-generation production configuration for S32K376NHT1MJBST? 1. Is there an existing programmed production orderable and OTP configuration for this combination? If so, please identify the exact order code, OTP ID/revision, and the applicable configuration report and programming/configuration file links. 2. If a custom OTP is required, which NXP or authorized-channel process should be used to obtain a compatible configuration and production-programmed parts? Please distinguish this from blank-device engineering emulation/programming. 3. Are MFS2643HMDA0AD and MFS2643HMDA0UD the applicable blank development variants, and what does their AD/UD difference mean for package, assembly and ordering applicability? The public FS26 standard-configuration examples and the S32K376POC page have been reviewed. The latter describes an FS2633-based board; its configuration is not being assumed transferable to FS2643D. Please point to the exact applicable documents or the correct support route if these details are not public. Thank you. Re: FS2643D H-generation: production OTP/orderable support for S32K376NHT1MJBST Hi Jonas Please see comment below: 1. Is there an existing programmed production orderable and OTP configuration for this combination? If so, please identify the exact order code, OTP ID/revision, and the applicable configuration report and programming/configuration file links. [gw]Below is the recommend please firstly evaluate this power tree is suitable or not for S32K376 https://www.nxp.com/products/FS26 2. If a custom OTP is required, which NXP or authorized-channel process should be used to obtain a compatible configuration and production-programmed parts? Please distinguish this from blank-device engineering emulation/programming. [gw]Please see answer above. 3. Are MFS2643HMDA0AD and MFS2643HMDA0UD the applicable blank development variants, and what does their AD/UD difference mean for package, assembly and ordering applicability? [gw] A0 means blank part, Below is the name rule of FS26,I didn't find the UD suffix. Please note that after you finish schematic design please send to us for double check. Thanks!
記事全体を表示
S32K376NHT1MJBST:適用可能な電力推定器および電源ごとの電流データ こんにちは、 S32K376NHT1MJBSTに適用される電力推定ツールと供給電流データを教えていただけますか? S32K-PETはこの派生モデルをサポートしていますか?どのツールとデバイスデータセットの改訂版を使用すべきですか?もしサポートされていない場合、現在の推奨されているNXP方法は何ですか? 外部供給のV15に外部NMOSのV11レギュレータ配置がある場合、報告された需要はV15、V11、VDD_HV_A/Bおよびその他のアナログ/バイアス供給にどのように帰属すべきでしょうか?特にレギュレーター損失、共有コア/ロックステップ需要、I/O負荷、ペリフェラル電流などを含め、何が含まれているか、何が除外されているかを特定してください。これらが二重にカウントされないようにするためです。 どの適用可能な公文書、データ、特性評価方法が、最悪のケースの電源電流と電圧/温度、リセット、起動、ウェイク、クロック/モード変更時のピークをカバーしていますか?標準値/平均値と保証限度額を区別し、それぞれの条件を明記してください。 公開されているPETページとセットアップガイドを確認しました。ファミリレベルの支援リストと初期の平均出力範囲では、正確な微分やすべての物理的供給貢献は特定されていません。私たちは、定義された運用プロファイルのない応用特有の現行結果ではなく、適用される情報源と方法を求めています。 これらの詳細が公開されていない場合は、適切な公開資料やサポートルートをご紹介ください。 よろしくお願いします。 Re: S32K376NHT1MJBST: applicable power estimator and per-supply current data こんにちは、@JonasGranlund さん。 1.現時点で、S32K PETツールはS32K39/37/36デバイスをサポートしていません。推奨される方法は、S32K396のデータシート(Rev.5) 供給電流データについては、具体的には: 6.7 供給電流(スタンバイモードおよび動作モードの表) 6.9 周期的なウェイクアップ平均電流の計算 2. データシートの供給電流表には、以下のレールにおける電流が個別に記載されています。 VDD_HV_A メインのI/Oおよびアナログ電源としてカタログ化されており、VDD_HV_AバンクのI/Oパッドとすべてのアナログブロックをカバーしています。 VDD_HV_Bは二次I/O電源であり、VDD_HV_Bバンク内のI/Oパッドのみを対象としています。どのピンがどのパワードメインに属しているかを特定するために、リファレンスマニュアル内の「S32K39_and_S32K37_IOMUX.xlsx」アタッチメントを参照できます。 V11は、外部NMOSを用いてV15によって生成される。LPMモードに入る前に、外部V1.5電源をオフにしてください。 IO負荷電流は測定値に含まれていません。IOの現在の要件は、アプリケーションのI/O構成によって異なります。S32K39データシートのDC特性表を参照してください。 データシートのコア供給量には、ロックステップ/デュアルコア動作時の需要が含まれています。コアの負荷に応じて個別の仕様が定められていないため、消費電力は同じ値として規定されています。 3.データシートの値には、周囲温度、標準値、最大値が含まれます。 私の知る限り、最悪のシナリオの電流やリセット時のピークなどを詳述したS32K39の文書は存在しません。しかし、S32K3の低電力パワーマネージメントANおよびデモでは、電源モードの遷移、低消費電力モードのクロック動作、ハードウェアの考慮事項、静止電流が記載されています。よりファミリレベルに焦点を当てており、S32K39-37-36の詳細ではなく、S32K3xx全体を指しています。 S32K3の低消費電力動作と留意事項について説明したS32K3低消費電力ラボのプレゼンテーションを、コミュニティ共有のプライベートメッセージでお送りしました。 よろしくお願いします、 ジュリアン
記事全体を表示
i.MX 93 – Prebuilt Ubuntu/Debian Linux Image and Custom Carrier Board Support Hello NXP Support Team, I am evaluating the i.MX 93 platform for an EVSE application and came across the EVSE-IMX93 development kit. I would like to clarify the available Linux images and their compatibility with a potential custom carrier-board design. Our intention is to use the MCIMX93-SOM and develop a simplified custom carrier board based on the original NXP carrier-board design. We would retain the same SOM connector and pin assignments while removing unused peripherals and circuitry. As I am relatively new to the i.MX processor platform and Yocto-based development, I am looking for a straightforward, ready-to-use Linux solution to get started before moving towards customisation. Could you please clarify the following? Is a ready-to-use Ubuntu or Debian 13 (Trixie) image available for the i.MX 93, preferably a general-purpose server/minimal Linux image? Can this image be downloaded and flashed directly onto a microSD card to boot the board, without requiring a Yocto build? Does the available image support standard Linux functionality such as apt, Python 3, SSH, systemd and networking? Does it include support for CAN/CAN-FD (SocketCAN), Wi-Fi, Ethernet and MQTT? Can packages such as Mosquitto be installed using apt? Can the same prebuilt image be used with our proposed custom carrier board, provided we retain the original SOM connector and relevant hardware connections? Would only device-tree or configuration changes be required? If such an image is available, could you please share the direct download link, supported board details and installation instructions? Our objective is to use the i.MX 93 as a general-purpose Linux platform for running the EVerest framework and other EVSE application software, while avoiding the need to maintain a Yocto build initially. Thank you for your assistance. Kind regards Ganesh Bhagwat Re: i.MX 93 – Prebuilt Ubuntu/Debian Linux Image and Custom Carrier Board Support Hello,  Yes, there is a Debian Linux SDK compatible with the i.mx93 platform, you can build the image through the implementation of "Flexbuild" instead of Yocto and flash the image with the  flexinstaller tool , more information about supported packages of the distro is available here: DEBIAN-SDK  Debian Software Release Notes LDLSDK_26.06
記事全体を表示