Multi Source Translation Content

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multi Source Translation Content

ディスカッション

ソート順:
AAOS 15 User Switch Crash on i.MX8QM Multi-Display Setup Hello Team, We are running Android Automotive OS 15 (AAOS 15) on the i.MX8QuadMax board with a multi-display setup (Main Display + Passenger Display). We are observing an issue with the default Car Launcher during user switching: System boots normally and the launcher is displayed on both main and passenger displays. When switching from the current user to a new user or guest user, both the main display and passenger display crash and become unusable. The issue is consistently reproducible after user switching. We would like to know: Is there any known issue related to user switching in AAOS 15 on i.MX8QM multi-display systems? Are there any additional configurations required for passenger display handling during user switch? What logs or debug information should we collect to further analyze this issue? Any suggestions or guidance would be appreciated. Thanks. Re: AAOS 15 User Switch Crash on i.MX8QM Multi-Display Setup Hi @AldoG, Thanks for the clarification.   We are using the NXP i.MX8QM MEK board with NXP BSP. Since this issue is related to Android Automotive, could you please let us know the correct support channel or forum where we should raise our AAOS-related questions? Thank you. Re: AAOS 15 User Switch Crash on i.MX8QM Multi-Display Setup Hello, Are you using NXP MEK board? If yes, you are using NXP BSP? Please note that we do not support Android Automotive we can provide asistance if issues are found on our BSP release. Best regards/Saludos, Aldo. Re: AAOS 15 User Switch Crash on i.MX8QM Multi-Display Setup Hi @AldoG, Thank you for the response. I have attached the full logcat,the reproduction steps.and changes we made to bring multi displays. Reproduction Steps: Boot AAOS 15 on i.MX8QM with center and passenger displays enabled. Open User Settings on the passenger display. Create or switch to a new user/guest user on the passenger display. During the user switch, com.android.car.carlauncher crashes with:   android.view.WindowManager$InvalidDisplayException: Unable to add window -- the specified display can not be found From the log, it appears that CarLauncher is trying to resume on a display that is no longer available or has an invalid display mapping after the user switch. Could you please advise: Whether this is a known issue in AAOS 15 multi-user/multi-display scenarios on i.MX8QM? Which component is responsible for assigning the display during user switching (OccupantZone, CarUserService, TaskDisplayArea, or WindowManager)? Are there any known requirements or patches related to MUMD (Multi-User Multi-Display) support for launcher launching on secondary displays? Is there any recommended debug information we should collect to identify why the display becomes invalid after the user switch?
記事全体を表示
AAOS 15 用户切换在 i.MX8QM 多显示器设置中崩溃 各位团队成员,大家好! 我们在 i.MX8QuadMax 板 上 运行 Android Automotive OS 15(AAOS 15), 采用多显示器设置( 主 显示器 + 乘客 显示器) 。 我们发现 用户 切换过程 中 默认 的 汽车 启动 器 存在 问题 : 系统 正常 启动 , 主 显示屏 和 乘客 显示屏 上 均 显示 启动 器 。 当 从 当前 用户 切换 到 新 用户 或 访客 用户 时 , 主 显示屏 和 乘客 显示屏 都会 崩溃 并 变得 无法 使用 。 用户 切换 后, 该 问题 始终 可以 重现 。 我们 想 知道 : 在 i.MX8QM 多 显示器 系统 中 , AAOS 15 是否 存在 与 用户切换 相关 的 已知 问题 ? 用户 切换 期间, 乘客 显示屏 的 处理 是否 需要 任何 额外 的 配置 ? 我们 应该 收集 哪些 日志 或 调试 信息 来 进一步 分析 此 问题? 任何建议或指导都将不胜感激。 谢谢。 Re: AAOS 15 User Switch Crash on i.MX8QM Multi-Display Setup 嗨@AldoG , 谢谢你的解释。   我们 正在 使用 NXP i.MX8QM MEK 板 和 NXP 电路板支持包 。由于 此 问题 与 Android Automotive 相关 , 请问 我们 应该 通过 哪个 支持 渠道 或 论坛 提出 与 AAOS 相关 的 问题 ? 谢谢。 Re: AAOS 15 User Switch Crash on i.MX8QM Multi-Display Setup 你好, 你使用的是NXP MEK开发板吗? 如果是,您使用的是NXP 电路板支持包。吗? 请注意,我们不提供 Android Automotive 的支持,但如果我们的 电路板支持包。 版本出现问题,我们可以提供帮助。 此致敬礼/Saludos, 阿尔多。 Re: AAOS 15 User Switch Crash on i.MX8QM Multi-Display Setup 嗨@AldoG , 谢谢你的回复。我 已 附上 完整的 logcat 日志 、 重现 步骤 以及 我们为实现多显示器功能所做的更改。 重现步骤: 在 i.MX8QM 上 启动 AAOS 15 ,并 启用 中央 和 乘客 显示屏 。 打开 乘客 显示屏 上的 用户 设置 。 在 乘客 显示屏 上 创建 或 切换 到 新 用户 /访客 用户 。 用户 切换 期间 , com.android.car.carlauncher 崩溃 并显示以下错误信息:   android.view.WindowManager$InvalidDisplayException: 无法添加窗口——找不到指定的显示器。 从日志 来看 ,用户 切换 后, CarLauncher 似乎正在尝试在 不再 可用 的 显示器 或 显示 映射 无效 的 显示器上恢复运行 。 请问 您 能否 提供以下建议: 在 i.MX8QM 上, AAOS 15 多 用户/多 显示器 场景 中 是否 存在 已知 问题 ? 在用户切换期间,哪个 元器件 负责 分配 显示 内容 (OccupantZone、 CarUserService、 TaskDisplayArea 或 WindowManager)? 对于 在 辅助 显示器 上 启动 启动器 , 是否 存在 与 MUMD (多用户 多显示器) 支持 相关的 已知 要求 或 补丁 ? 是否 有 任何 建议 的 调试 信息 需要 收集 , 以 确定 用户 切换 后 显示 失效 的 原因 ?
記事全体を表示
S32K312 EVB - 使用 LPSPI 硬件 PCS0 进行 SD 卡 SPI 初始化 您好, 我正在使用 RTD 6.0.0(非 AUTOSAR Lpspi_ Ip 驱动程序)在 S32K312 EVB 上通过 SPI 实现 SD 卡驱动程序。 根据SD物理层简化规范,SPI初始化序列为: 启动后保持 CS 值高。 生成至少 74 个时钟脉冲(我通过发送 10 字节的 0xFF 来发送 80 个时钟)。 拉低 CS。 发送 CMD0 (0x40 00 00 00 00 95)。 在轮询 0xFF 时保持 CS 低,直到卡响应 **R1 = 0x01`。 我的问题出在硬件控制的PCS0上。 当使用 Lpspi_Ip 驱动程序和硬件 PCS0 时,在 SPI 传输期间,LPSPI 外设会自动钳位/置低 PCS 信号。因此,我无法按照 SD 规范的要求,在保持 CS 高电平的同时生成初始 80 个时钟脉冲,然后在保持 CS 低电平的同时生成 CMD0。 我有以下几个问题: S32K312 LPSPI 外设是否支持在生成 SPI 时钟时保持 PCS 非活动(高电平)? 在 SD 卡初始化序列期间,是否有任何 Lpspi_Ip API、寄存器配置或推荐的方法来手动控制 PCS 或暂时禁用硬件 PCS? 如果不是,推荐的方法是否是将 SD 卡 CS 引脚配置为 GPIO 并手动控制它,而仅使用 LPSPI 控制 SCK、MOSI 和 MISO? 此外,如果 NXP 有任何参考实现、应用笔记、示例项目或 SDK/RTD 示例演示 S32K3 系列通过 SPI 进行 SD 卡通信,能否请您分享一下参考资料? 谢谢! Re: S32K312 EVB - SD Card SPI Initialization using LPSPI Hardware PCS0 嗨@parvathitp PCS(外设片选)信号设计为由 LPSPI 模块控制。当选择硬件 PCS 时,LPSPI 外设会在 SPI 帧传输期间自动对其进行钳位和取消置位。 当硬件 PCS 信号分配给 LPSPI 模块时,没有专用的 API 可用于手动控制该信号。因此,正如您所提到的,这种情况的最佳方法是将 CS 引脚配置为 GPIO。 在此配置中,CS 信号通过 SIUL2/GPIO API 进行控制,您负责控制它。 目前还没有专门针对 S32K3 的应用说明、示例项目或参考文档来演示这种确切的实现方式。 BR,VaneB
記事全体を表示
S32K 比较器公差/偏移 我们正在对S32K116比较器进行一些测试: 我们向 INN(或 INP)施加输入电压(238mV),以带隙为参考,然后我们将 VOSEL 从 0 增加到 255,并监测比较器输出何时发生变化。 不知何故,当输入电压和带隙的连接互换时,我们在 MCU2 上观察到了不同的容差/偏移。(详情请参见测试1和测试2) 1)这是像VAIO那样已知的某种功能,还是其他什么功能? 2)对于这种公差/偏差,它是否稳定,我们可以通过校准消除它吗? (例如,记录目标电压下的触发信号) 测试1:输入电压接V-,带隙接V+ ,低速模式 Sid_Zhou_5-1784193940847.png 测试2:输入电压接V+,带隙接V- ,低速模式 Sid_Zhou_6-1784193974436.png Re: S32K comparator tolerance/offset 1)输入引脚 CMP0_IN 始终设置为通道 0。(PIN26,PTA0) 是的,输入电压仍然通过相同的 CMP0_IN 引脚 26、PTA0 输入。 2)带隙 我想弄清楚的特性并不是两个MCU之间的区别。当 INN 和 INP 互换时,同一个 MCU 的容差/偏移量就会不同。我认为在这种交换过程中带隙不应该发生变化。(此处MCU1的数据仅供参考) 3) VDD/VDDA: 这两个MCU使用相同的+3.3V网络(LDO容差在1.25%以内)。 我完全理解MCU的带隙会有所不同,但是,我再次强调,我检查的是交换后的带隙差异。 4)测试方法 上述测试数据并非增加输入电压,而是使用固定输入电压,并增加 VOSEL 值。(关于降低 VOSEL 值,我尚未测试,稍后会进行检查。) 对于固定 VOSEL 的增加/减少输入电压的情况,有类似的 -9mV。 IncreaseInput_FixedVOSEL.PNG 5)滞后现象 我确实有低速模式下磁滞现象的测试数据: 此处的测试数据是固定输入电压并增加 VOSEL: Hysteresis_LowSpeedMode.PNG 6)MCU照片 您可以参考附件照片“MCU1.PNG”和“MCU2.PNG”。 阻焊层是 FS32K11-6LFMMF-ON96V-S12YM16 Re: S32K comparator tolerance/offset 你好 Sid_Zhou, 您将输入电压连接到了哪个 CMP0_IN 引脚? 当交换 INN 和 INP 时,输入电压是否仍然通过同一个 CMP0_IN 引脚输入? 此外,带隙电压范围在 0.97-1.03V 之间。您是否考虑过暂时排除两个 MCU 的带隙电压不同所导致的问题?例如,能否使用不同的 CMP0_IN 引脚来输入更精确的外部电压基准? 你检查过两个 S32K1 的 VDD/VDDA 电压是否相同吗? 调试过程中是否确认 OFFSET=1 和 HYSTCTR=0? 我注意到您提高了输入电压并记录了 VOSEL。你试过降低输入电压并记录VOSEL值吗?另外,检查一下模拟比较器的迟滞是否受到影响,虽然我看到你已将 HYSTCTR 配置为 0。 拍摄两张 S32K116 照片,并告诉我 MCU 掩模。 此致敬礼, Robin Re: S32K comparator tolerance/offset 感谢您的详细解释。我现在明白您关心的是 S32K1 数据手册中的VAIO (模拟输入偏移电压)参数。 我在内部看到了AE团队的解释: AIO偏移量是比较器本身的偏移量,即INP和INN之间的偏移量。 由于 INL 误差是对 DNL 的积分,因此 INL 误差包含了 DNL 误差。 错误为 |V_AIO| + |INL| 根据我的理解,直接使用来自外部信号源的两个模拟电压分别输入INP和INN来测试VAIO应该比使用带隙分压器更直观。 关于您的问题:对于同一个 MCU,VAIO 不是一个随机值,不会随意地随时间变化,而是会随着工作条件(尤其是温度)而漂移。数据表中的 VAIO 值应理解为整个温度范围内的保证/最坏情况极限。 在设计阈值时,不要将 VAIO 视为可忽略不计或固定的校准值。保持裕量基于全温最坏情况 |VAIO|,加上 DAC/INL 误差。 我还查看了您之前关于此问题的讨论: S32K116 比较器容差。 看来CMP的精度无法满足您的需求。您是否考虑过 S32K1XXRM Rev14.2 的“ 44.5.5 自动比较功能”部分中描述的功能? S32K1 数据手册 Rev15 中的“ 表 41. 12 位 ADC 特性 (2.7 V 至 3 V) ”显示最大 TUE 为 ±8 LSB。这似乎比CMP更准确。 Re: S32K comparator tolerance/offset 感谢您的详细解释。 我注意到,在我们的应用中,ADC 可能具有更高的精度。 但是,从高层架构来看,我们有使用 CMP 作为功能安全监视器的要求,我不确定是否可以将其更改为 ADC。
記事全体を表示
S32K comparator tolerance/offset we are having some test on the comparator of S32K116: we apply an input voltage(238mV) to INN (or INP), use bandgap as reference, then we increase VOSEL from 0 to 255 and monitor when the comparator output changed. Somehow, we see different tolerance/offset on MCU2 when the connection of input voltage and bandgap is swapped.  (Details shown in Test1 and Test2) 1) Is this some kind of known feature like VAIO or something else? 2) For this tolerance/offset, is it stable and can we eliminate this by calibration? (like record the trigger VOSEL at the target voltage) Test1: Input Voltage on V-, Bandgap on V+, Low Speed Mode Sid_Zhou_5-1784193940847.png Test2: Input Voltage on V+, Bandgap on V-, Low Speed Mode Sid_Zhou_6-1784193974436.png Re: S32K comparator tolerance/offset 1) Input Pin CMP0_IN is always set to channel 0. (PIN26, PTA0) Yes, input voltage still being input through the same CMP0_IN Pin26, PTA0. 2) Bandgap The feature I want to figure out is not the difference between two MCU.  It is this different tolerance/offset from the same MCU when INN and INP is swapped. I think the bandgap should not change during this swapped.  (The data of MCU1 here is just use as reference) 3) VDD/VDDA: The two MCU are using same +3.3V network (LDO within 1.25% tolerance).  I am fully understanding there will be difference between MCUs bandgap, but, again, it is the difference during swapped I am checking. 4) test method The test data above is not increasing input voltage, it is using fixed input voltage, and increasing VOSEL. (For decreasing VOSEL, i have not test yet, will check this later.) As for increasing/decreasing input voltage with fixed VOSEL, there is similar -9mV.  IncreaseInput_FixedVOSEL.PNG  5) Hysteresis I do have test data for hysteresis in low-speed mode: Test data here is fixing input voltage and increase VOSEL:  Hysteresis_LowSpeedMode.PNG  6) MCU photos you can refer to attached photo "MCU1.PNG" and "MCU2.PNG" Solder mask is  FS32K11-6LFMFM-ON96V-S12YM16 Re: S32K comparator tolerance/offset Hi Sid_Zhou, Which CMP0_IN pin are you connecting the input voltage to? When swapping INN and INP, is the input voltage still being input through the same CMP0_IN pin? Also, the BandGap voltage range is between 0.97-1.03V. Have you considered temporarily ruling out issues caused by different BandGap voltages on the two MCUs? For example, could you use a different CMP0_IN pin to input a more accurate external voltage reference? Have you checked whether the VDD/VDDA voltages of the two S32K1s are the same? Were OFFSET=1 and HYSTCTR=0 confirmed during debugging? I noticed you increased the input voltage and recorded VOSEL. Have you tested decreasing the input voltage and recording VOSEL? Also, check if the Analog comparator hysteresis is affected, although I see you configured HYSTCTR=0. Take two S32K116 photos and tell me the MCU mask. Best Regards, Robin Re: S32K comparator tolerance/offset Thank you for your detailed explanation. I now understand that you are concerned about the VAIO (Analog Input Offset Voltage) parameter in the S32K1 Datasheet. Internally, I saw the AE team's explanation: The AIO offset is the offset of the comparator itself. the offset between INP and INN. The INL error includes the DNL error since it is an integral over the DNL. The error is then |V_AIO| + |INL| Based on my understanding, directly using two analog voltages from an external signal source to input INP and INN respectively to test VAIO should be more intuitive than using bandgap voltage divider.  Regarding your question:  for the same MCU, VAIO is not a random value that changes arbitrarily from moment to moment , but it can drift with operating conditions, especially temperature. The VAIO value in the datasheet should be understood as a guaranteed/worst-case limit over the full temperature range. When designing the threshold, do not treat VAIO as negligible or as a fixed calibrated-out value . Keep margin based on the full-temperature worst-case |VAIO| , plus the DAC/INL error. I also checked your previous discussion on this: S32K116 comparator tolerance. It seems that CMP's accuracy doesn't meet your needs. Have you considered the feature described in section "44.5.5 Automatic compare function" of S32K1XXRM Rev14.2? "Table 41. 12-bit ADC characteristics (2.7 V to 3 V)" in S32K1 DataSheet Rev15 shows a maximum TUE of ±8 LSB. This appears to be more accurate than CMP. Re: S32K comparator tolerance/offset Thanks for your detailed explanation. I noted that the ADC may have better accuracy in our application. But somehow, we have requirements for using CMP as safety monitor from high level architecture and i am not sure if this can be changed to ADC.
記事全体を表示
S32K312 EVB - LPSPIハードウェアPCS0を使用したSDカードSPI初期化 こんにちは、 私はRTD 6.0.0(Non-AUTOSAR Lpspi_ Ipドライバー)を使って、S32K312 EVB上でSPI経由でSDカードドライバーを実装しています。 SD物理層簡略仕様書によると、SPI初期化シーケンスは次のとおりです。 電源投入後はCSレベルをHIGHに維持してください。 少なくとも74個のクロックパルスを生成します(私は0xFFを10バイト送信することで80個のクロックを送信しています)。 CS LOW を引いてください。 CMD0 (0x40 00 00 00 00 95) を送信します。 カードが「R1 = 0x01」と応答するまで、0xFFでポーリングしながらCSをLOWに保ってください。 私の問題は、ハードウェア制御のPCS0に関するものです。 ハードウェアPCS0でLpspi_Ipドライバを使用する場合、SPI転送中にLPSPIペリフェラルによってPCS信号が自動的にアサッサーされます。そのため、SD仕様で求められるCSをHIGHに保ち、その後CMD0とCS LOWを保持しながら最初の80クロックパルスを生成できません。 私には以下の質問があります。 S32K312 LPSPIペリフェラルは、SPIクロックを生成しながらPCSを非アクティブ(HIGH)に保つことに対応していますか? SDカードの初期化シーケンス中にPCSを手動で制御したり、一時的にハードウェアPCSを無効化したりするための、Lpspi_Ip APIやレジスタ設定、または推奨される方法はありますか? そうでない場合、推奨されるアプローチは、SDカードのCSピンをGPIOとして構成し、SCK、MOSI、およびMISOのみにLPSPIを使用しながら手動で制御することでしょうか? また、NXPがS32K3シリーズでSPIを介したSDカード通信を示すリファレンス実装、アプリケーションノート、サンプルプロジェクト、SDK/RTDの例があれば、ぜひ教えていただけますか? よろしくお願いします。 Re: S32K312 EVB - SD Card SPI Initialization using LPSPI Hardware PCS0 こんにちは、 @parvathitp PCS(周辺チップセレクト)信号はLPSPIモジュールによって制御されるよう設計されています。ハードウェアPCSを選択すると、SPIフレーム転送中にLPSPIペリフェラルによって自動的にアサッティングおよびデアッサートされます。 LPSPIモジュールに割り当てられているハードウェアPCS信号を手動で制御するための専用APIは提供されていません。したがって、あなたが言及したように、この場合の最良の方法はCSピンをGPIOとして設定することです。 この構成では、CS信号はSIUL2/GPIO APIを介して制御され、その制御はユーザーの責任となります。 現在、この正確な実装を示すS32K3専用のアプリケーションノート、例プロジェクト、参考文書は存在しません。 BR、VaneB
記事全体を表示
HSE INSTALL S32K311 下面的所有内容都是从附件中复制 S32DS版本:S32DS.3.5_b220726_win32.x86_64 (1).exe RTD版本:SW32K3_RTD_R21-11_3.0.0_P07_D2306_DS_updatesite.zip S32K311支持包版本:SW32K3_S32DS_3.5.6_D2309.zip SBAF版本:SBAF_S32K311_0_0_15_0, Bin文件:s32k311_Secure_Baf_0.12.0_0.15.0.6_pb230804.bin.pink HSE版本:HSE_FW_S32K311_0_2_40_0, bin文件为s32k311_hse_fw_0.12.0_2.40.0_pb230730.bin.pink 使用FULL_MEM 没有安全启动 当前遇到的一个问题 程序运行会一直卡在这里while ( FALSE == HSE_CheckStatus(HSE_STATUS_INIT_OK) ); 图片3.png   图片4.png 图片1.png 图片5.png   图片6.png   图片2.png      Re: HSE INSTALL S32K311 这个是补充的printf信息 DCMROF21: 0x00040000 HSE GPR3: 0x000000C0 Current_SBAF_Version-0x4039c020: 0x00000C00 LC 配置字-0x4039C02C: 0x00000000 生命周期相关信息-0x402AC200: 0x00000000 HSE Status: 0x00000000 我从网上查阅资料,是不是芯片出场自带的SBAF不识别我现在使用的HSE固件? Re: HSE INSTALL S32K311 我怀疑是SBAF没有将flash中的hse固件复制到hse_nvm中,如果是这个问题,我应该怎么解决 Re: HSE INSTALL S32K311 这个是我打印的数据 DCMROF21: 0x00040000 HSE GPR3: 0x000000C0 HSE Status: 0x00000000 HSE 固件未启动(NVM 空或固件损坏) 111.png Re: HSE INSTALL S32K311 嗨@iiiddd 请问能否提供 HSE_CONFIG_GPR3 (0x4039C028) 的值?位 0 表示 HSE 固件是否存在。 BR,VaneB Re: HSE INSTALL S32K311 我在编写 UTEST 时调用了 RTD 库。 gHsePort_FlsIf.writeApi(UTEST_BASE_ADDR,(uint8_t*)hseFwFeatureFlag,FW_FEATURE_FLAG_LEN); 将使用 FLS_MAX_VIRTUAL_SECTOR 定义。我的 RTD 库默认值为 135,但访问地址 0x1B000000UL 需要 136。我使用的RTD库与HSE不兼容吗? Re: HSE INSTALL S32K311 嗨@iiiddd HSE_CONFIG_GPR3[0] 位未设置,这表明设备上不存在 HSE 硬件。 作为参考,下图显示了为在 S32K311 设备上安装 HSE FW FULL_MEM 而配置的链接器文件示例: VaneB_0-1784568701705.png Re: HSE INSTALL S32K311 我在调试时发现 pflash 中有与 hse 固件对应的数据。你的意思是说,sbaf 未能将 pflash 中的固件复制到 hsenvm 中吗?如果这是问题所在,那么可能是什么原因造成的呢?
記事全体を表示
MRF13750H原理图 如何将 MRF13750H-915MHz 板转换为原理图?MRF13750H 数据手册包含 915 MHz 的参考板布局,但不包含原理图。 Luis_V_1-1784224999094.png
記事全体を表示
LLCE example and U-boot Hello. I'm trying to make the LLCE examples work on the Goldbox. I modified the CAN2CAN example a little bit, and it works if I debug it from S32DS. If I try to run it from U-boot, however, it executes, but hangs U-boot itself. These are the commands I'm running: dcache off; mw.q 0x34000000 0x0 0x100000; dcache on fatload mmc 0:2 ${loadaddr} /llce.elf bootm7 ${loadaddr} VTABLE I can see the CAN traffic on the bus, so the example is running, but U-boot hangs and is not able to accept commands anymore. After some debugging, I was able to trace the problem to the PlatformInit() call, and in particular the code to set the clock. If I remove that code, however, the example does not work anymore. Do you have any suggestions? Re: LLCE example and U-boot Hello, @GioMusto  Thanks for your reply. Yes, it is for S32G2, not G3, but the method introduced is similar. Since it is based on early version software packages, it could not be considered as a step by step guide when using recent version software combinations. BR Chenyin Re: LLCE example and U-boot Hi @chenyin_h, thanks for your reply. I see the guide you posted is for the S32G2. Is it the same for S32G3, or are there some differences? Do you have any suggestion on things to keep an eye on? Common problems, and so on. Re: LLCE example and U-boot Hello, @GioMusto  Thanks for your post. The issue you mentioned may be caused clock or other resource confliction between M and A side. 1. On S32G product, under default settings, the BSP running on A53 side is designed under the assumption that it has exclusive access to the system, and therefore does not consider potential conflicts introduced by other software components, while in your M core application, it may also touch critical resources like clock/memory, etc. You have to careful about every part of the code, to avoid any possible confliction/re-configuration for critical resources. 2. For running both M7 application and Linux BSP simultaneously, the recommended way is to firstly running a M7 bootloader to manage the resources, as introduced via AN13750  BR Chenyin Re: LLCE example and U-boot I'm trying to build the M7 bootloader by following AN13750 and the "System-Level Bootloader Integration Example for S32G3XX". I managed to compile the bootloader (with some difficulties, since I'm missing the SAF package), but now I'm stuck with the IVT tool in S32DS. When I create a new project, select S32G399A, Cortex-M7_0, and create a configuration, I get the error "IVT tool does not support the current processor. The same is true for DCD, QuadSPI, DDR and eFuse (see screenshot). What am I doing wrong? IVT_error.png Re: LLCE example and U-boot Hello, @GioMusto  Thanks for your reply. 1. Commonly, I suggest using S32DS3.5.x(for example, 3.5.14) for working with S32G(mentioned in release notes of S32G RTD release), and make sure that the following packages are installed at least:(RTD and development package) chenyin_h_0-1786010049364.png 2. To simplify the process, you may import an example project into the S32DS, and then open the IVT tool, for example: chenyin_h_1-1786010241259.png Then have a try if the IVT tool could be used for generating blob based on your own images. BR Chenyin
記事全体を表示
MPC5746C FXOSC 出力周波数 パーツ:MPC5746C(Power Architecture Z4、SDK:NXP MPC57xxプラットフォームSDK)。 MPC5746Cのマニュアルには、FXOSCは8~40MHzの出力周波数を提供すると記載されています。以下の構成におけるFXOSCの出力周波数を特定するのを手伝ってください。 1. FXOSC_CTL: OSCBYP = 0 かつ OSCM = LCP 2. FXOSC_CTL: OSCBYP = 0 かつ OSCM = FSP 3. FXOSC_CTL: OSCBYP = 1 かつ OSCM = LCP 4. FXOSC_CTL: OSCBYP = 1 かつ OSCM = FSP 他のレジスタ項目についてもデフォルト値を検討してください。ありがとう。 Re: MPC5746C FXOSC output frequency @petervlna さん、ご回答ありがとうございます。 クリスタル/共振器(OSCBYP = 0)と外部クロック(OSCBYP = 1)が提供する周波数はどのように見つければよいのでしょうか? Re: MPC5746C FXOSC output frequency こんにちは、 FXOSCモジュールは、OSCBYPおよびOSCMの設定に基づいて特定の周波数を生成しません。FXOSCの出力周波数は常にFXOSCに接続された外部ソースの周波数(OSCBYP=0のクリスタル/共振器、OSCBYP=1の時は外部クロック)と等しく、8〜40 MHzのサポート範囲内で行われます。 したがって、記載されている4つの構成すべてにおいて、FXOSCの出力周波数は外部入力周波数と全く同じになります。OSCMの設定(LCP/FSP)は発振器の動作モードに影響を与えますが、クロック周波数は変更しません。 よろしくお願いいたします。 ピーター Re: MPC5746C FXOSC output frequency @petervlna上記のFXOSCの問い合わせについてサポートいただければ幸いです。 Re: MPC5746C FXOSC output frequency クリスタル/共振器(OSCBYP = 0)と外部クロック(OSCBYP = 1)が提供する周波数はどのように見つければよいのでしょうか? 上記の質問について、 @petervlna さんにお知らせください。FXOSCをタイマーのクロックソースとして使用したい。提供される周波数に基づいて、カウント値をタイマーレジスタに読み込めます Re: MPC5746C FXOSC output frequency こんにちは、 MPC5746Cには、FXOSCレジスタからFXOSC周波数を測定または判定する方法がありません。周波数はハードウェア設計から知られている必要があります: OSCBYP = 0: FXOSC周波数は、基板に取り付けられた外部水晶発振器/共振器の周波数と等しい。 OSCBYP = 1: FXOSC周波数は、FXOSC入力ピンに印加される外部クロック信号の周波数と等しくなります。 FXOSCをタイマークロックソースとして使用するには、タイマーカウント値を計算する際に基板の回路図やクロックデザインで指定された周波数(例:8 MHz、16 MHz、40 MHzなど)を使用する必要があります。OSCBYPとOSCMの設定は、周波数自体には影響しません。 よろしくお願いいたします。 ピーター
記事全体を表示
LLCE 示例和 U-boot 您好。 我正在尝试让 LLCE 示例在 Goldbox 上运行。 我对 CAN2CAN 示例做了一些修改,如果我从 S32DS 进行调试,它可以正常工作。 但是,如果我尝试从 U-boot 运行它,它会执行,但会导致 U-boot 本身卡死。 以下是我运行的命令: dcache 关闭;mw.q 0x34000000 0x0 0x100000;dcache 开启 fatload mmc 0:2 ${loadaddr} /llce.elf bootm7 ${loadaddr}虚函数表 我可以看到总线上的 CAN 通信,所以示例程序正在运行,但是 U-boot 卡住了,无法再接受命令。 经过一番调试,我最终将问题追溯到PlatformInit()调用,特别是设置时钟的代码。 但是,如果我删除那段代码,示例就无法正常运行了。 您有什么建议吗? Re: LLCE example and U-boot 你好, @GioMusto 感谢您的回复。 是的,它是针对 S32G2 的,而不是 G3,但介绍的方法类似。 由于它是基于早期版本的软件包,因此在使用最新版本的软件组合时,不能将其视为分步指南。 BR 陈银 Re: LLCE example and U-boot 你好@chenyin_h ,谢谢你的回复。 我看到你发的指南是针对S32G2的。S32G3 也一样吗?还是有一些区别? 您有什么建议,需要重点关注哪些方面?常见问题等等。 Re: LLCE example and U-boot 你好, @GioMusto 感谢你的帖子。 您提到的问题可能是由于 M 端和 A 端之间的时钟或其他资源冲突引起的。 1. 在 S32G 产品上,默认设置下,运行在 A53 端的 BSP 被设计为假定其拥有对系统的独占访问权限,因此不考虑其他软件组件引入的潜在冲突,而您的 M 内核应用程序也可能访问时钟/内存等关键资源。你必须仔细检查代码的每个部分,以避免关键资源出现任何可能的冲突/重新配置。 2. 要同时运行 M7 应用程序和 Linux 电路板支持包,建议先运行 M7 引导加载程序来管理资源,如AN13750中所述。 BR 陈银 Re: LLCE example and U-boot 你好, @GioMusto 感谢您的回复。 1. 通常情况下,我建议使用 S32DS3.5.x 版本(例如 3.5.14)。要使用 S32G(在 S32G RTD 版本发布说明中提到),请确保至少安装了以下软件包:(RTD 和开发软件包) chenyin_h_0-1786010049364.png 2. 为简化流程,您可以将示例项目导入 S32DS,然后打开 IVT 工具,例如: chenyin_h_1-1786010241259.png 然后尝试使用 IVT 工具根据您自己的图像生成 blob。 BR 陈银 Re: LLCE example and U-boot 我正在尝试按照 AN13750 和“S32G3XX 的系统级引导加载程序集成示例”来构建 M7 引导加载程序。 我成功编译了引导加载程序(虽然遇到了一些困难,因为我缺少 SAF 软件包),但现在我在 S32DS 中使用 IVT 工具时遇到了问题。 当我创建一个新项目,选择 S32G399A、Cortex-M7_0 并创建一个配置时,出现错误“IVT 工具不支持当前处理器”。DCD、QuadSPI、DDR 和 eFuse 也存在同样的问题(见截图)。 我做错了什么? IVT_error.png
記事全体を表示
what the hell is wrong with MCUXpresso IDE support on ubuntu linux not a single bloody simplest of the simplest thing like creating a hello world program in the MCUXpresso IDE on Linux. I have a rt700 evkb board and that ide just keep crashing and hanging up i am struggling with it for the past 2-3 days just what in the world is this BS. it is obviously expected to have a decent enough support one day it works and then the other day it does not. there is also no guide to have some fix. even after creating some basic project when opening the peripheral configuration tab it magically just does not work it weirdly just say the processor core whatever does not support this or something like that. these days all we have is slop or what from Microsoft windows to even this IDE and then to some degree ubuntu as well.  to run this ide what is do you expect us to do to run it on windows? please for love of everything please fix this issues and i can't even take a screenshot it hangs up that bad.   prathamvora_0-1784244137157.png Re: what the hell is wrong with MCUXpresso IDE support on ubuntu linux The BOM file for the EVKB itself uses the same package as being used in ide project creation.  prathamvora_1-1784245217062.png Re: what the hell is wrong with MCUXpresso IDE support on ubuntu linux please have  a look at this video and please make some training videos on how to even use this tool. let alone use the vscode extension i can only imagine what kind of broken support it is going to be. Re: what the hell is wrong with MCUXpresso IDE support on ubuntu linux prathamvora_0-1784244495436.png this is what i get after rebooting my system and opening the IDE Re: what the hell is wrong with MCUXpresso IDE support on ubuntu linux Hi @prathamvora, According to the MCUXpresso Integrated Development Environment (IDE) webpage, the supported Ubuntu versions are Ubuntu 22.04 LTS and Ubuntu 24.04 LTS. In the case of MCUXpresso for Visual Studio Code, the supported Ubuntu versions are Ubuntu 20.04.2 LTS, Ubuntu 22.04 LTS, and Ubuntu 24.04 LTS. I would recommend using one of the supported Ubuntu versions for MCUXpresso IDE or MCUXpresso for Visual Studio Code. Best Regards, Pablo
記事全体を表示
MCUXpresso IDE 在 Ubuntu Linux 上的支持到底出了什么问题? 连在 Linux 系统上使用 MCUXpresso IDE 编写一个“Hello World”程序这样最简单的事情都做不到。我有一块RT700 EVKB板,那个IDE总是崩溃死机,我已经为此苦恼了两三天了,这到底是怎么回事?它明明应该有像样的支持才对,今天能用,明天就出问题了。也没有任何指南可以解决这个问题。即使创建了一些基本项目,打开外围设备配置选项卡时,它也会神奇地无法工作,奇怪地显示处理器核心不支持此功能或类似信息。如今我们看到的都是些垃圾,从微软的Windows到这个IDE,甚至在某种程度上还有Ubuntu。要在 Windows 系统上运行这个 IDE,您希望我们做什么?看在上帝的份上,请修复这些问题吧,我甚至都无法截图,系统卡得太厉害了。 prathamvora_0-1784244137157.png Re: what the hell is wrong with MCUXpresso IDE support on ubuntu linux EVKB 本身的 BOM 文件使用的包与 ide 项目创建中使用的包相同。 prathamvora_1-1784245217062.png Re: what the hell is wrong with MCUXpresso IDE support on ubuntu linux 请观看这段视频,并请制作一些关于如何使用此工具的培训视频。更别提使用 VS Code 扩展了,我简直不敢想象它的技术支持会有多糟糕。 Re: what the hell is wrong with MCUXpresso IDE support on ubuntu linux prathamvora_0-1784244495436.png 这是我重启系统并打开IDE后得到的结果。 Re: what the hell is wrong with MCUXpresso IDE support on ubuntu linux 你好@prathamvora , 根据MCUXpresso 集成开发环境 (IDE)网页显示,支持的 Ubuntu 版本为 Ubuntu 22.04 LTS 和 Ubuntu 24.04 LTS。对于Visual Studio Code 的 MCUXpresso ,支持的 Ubuntu 版本为 Ubuntu 20.04.2 LTS、Ubuntu 22.04 LTS 和 Ubuntu 24.04 LTS。 我建议使用 MCUXpresso IDE 或 MCUXpresso for Visual Studio Code 支持的 Ubuntu 版本之一。 此致, 巴勃罗
記事全体を表示
IW612 Bluetooth RF Test Hello everyone, I'm trying to execute the RF Test for the module based on IW612. For this, I followed a couple of documents, such as: AN14310 - NXP Bluetooth UART Driver Integration AN14114 - RF Test Mode on Linux OS AN14163 - Bluetooth Direct Test Mode And others. I'm facing some problems: - In Wi-fi 5 GHz, I'm not able to see waveforms generated for low channels, near to 5 GHz, only for higher channels  - For Bluetooth, I'm not able to generate waveforms for the classic Bluetooth, only for BLE (commands for scan and get the pair information using hcitool work fine, hence I don't think this is a Hardware issue) In my setup, I'm using the SoM Variscite Dart IMX8M (version 2.0), with a 2EL radio, based on IW612. To get the waveforms, I'm using HackRF. I'm using the system with Kernel 6.6.23, Yocto custom version, and with Firmware sduart_nw61x_v1.bin.se, default from the version The feedback for the HCI commands is compatible with the documents, but I can't see the waveforms. May you help me if I'm missing something in our system or procedures to generate it? This is part of the Certification process, and now I'm stuck on it. THanks very much Re: IW612 Bluetooth RF Test Hello Could you share test cmd and result screen shot to us? Best Regards Shaun Re: IW612 Bluetooth RF Test Hello Shaun, Sure. I ran these commands for hcitool and for wifi, I attached the final file for the config For Bluetooth Classic ------------------------------------ THESE COMMANDS WERE COLLECTED DIRECTLY FROM UM11490 (pg 149) # RESET root@oaslv:/home/hexagon# hcitool -i hci0 cmd 0x03 0x0003 < HCI Command: ogf 0x03, ocf 0x0003, plen 0 > HCI Event: 0x0e plen 4 01 03 0C 00 # ENABLE SCAN root@oaslv:/home/hexagon# hcitool -i hci0 cmd 0x03 0x001a 0x3 < HCI Command: ogf 0x03, ocf 0x001a, plen 1 03 > HCI Event: 0x0e plen 4 01 1A 0C 00 # ENABLE EVENT FILTER root@oaslv:/home/hexagon# hcitool -i hci0 cmd 0x03 0x0005 0x02 0x00 0x02 < HCI Command: ogf 0x03, ocf 0x0005, plen 3 02 00 02 > HCI Event: 0x0e plen 4 01 05 0C 00 # ENTER IN TEST MODE root@oaslv:/home/hexagon# hcitool -i hci0 cmd 0x06 0x0003 < HCI Command: ogf 0x06, ocf 0x0003, plen 0 > HCI Event: 0x0e plen 4 01 03 18 00 # START THE TX TRANSMISSION root@oaslv:/home/hexagon# hcitool -i hci0 cmd 0x3F 0x0019 0x80 0x80 0x80 0x80 0x01 0x00 0x01 0x01 0x0D 0x03 0x0F 0x00 0x00 0x00 0x00 0x00 0x00 0x04 < HCI Command: ogf 0x3f, ocf 0x0019, plen 18 80 80 80 80 01 00 01 01 0D 03 0F 00 00 00 00 00 00 04 > HCI Event: 0x0e plen 4 01 19 FC 00 # STOP THE TX TRANSMISSION root@oaslv:/home/hexagon# hcitool -i hci0 cmd 0x3F 0x0019 0x80 0x80 0x80 0x80 0xF F 0x00 0x01 0x01 0x0D 0x03 0x0F 0x00 0x00 0x00 0x00 0x00 0x00 0x04 < HCI Command: ogf 0x3f, ocf 0x0019, plen 18 80 80 80 80 FF 00 01 01 0D 03 0F 00 00 00 00 00 00 04 > HCI Event: 0xff plen 6 19 01 39 00 00 00 -------------------- STOPPING THE SCAN FOR BLE AND CLASSIC BEFORE THE TX TRANSMISSION ---------------- # RESET root@oaslv:/home/hexagon# hcitool -i hci0 cmd 0x03 0x0003 < HCI Command: ogf 0x03, ocf 0x0003, plen 0 > HCI Event: 0x0e plen 4 01 03 0C 00 # ENABLE SCAN root@oaslv:/home/hexagon# hcitool -i hci0 cmd 0x03 0x001a 0x3 < HCI Command: ogf 0x03, ocf 0x001a, plen 1 03 > HCI Event: 0x0e plen 4 01 1A 0C 00 # ENABLE EVENT FILTER root@oaslv:/home/hexagon# hcitool -i hci0 cmd 0x03 0x0005 0x02 0x00 0x02 < HCI Command: ogf 0x03, ocf 0x0005, plen 3 02 00 02 > HCI Event: 0x0e plen 4 01 05 0C 00 # ENTER IN TEST MODE root@oaslv:/home/hexagon# hcitool -i hci0 cmd 0x06 0x0003 < HCI Command: ogf 0x06, ocf 0x0003, plen 0 > HCI Event: 0x0e plen 4 01 03 18 00 # DISABLE THE BLE SCAN root@oaslv:/home/hexagon# hcitool -i hci0 cmd 0x03 0x001a 0x0 < HCI Command: ogf 0x03, ocf 0x001a, plen 1 00 > HCI Event: 0x0e plen 4 01 1A 0C 00 # DISABLE THE CLASSIC SCAN root@oaslv:/home/hexagon# hcitool -i hci0 cmd 0x08 0x000C 0x00 0x00 < HCI Command: ogf 0x08, ocf 0x000c, plen 2 00 00 > HCI Event: 0x0e plen 4 01 0C 20 00 # START THE TX TRANSMISSION root@oaslv:/home/hexagon# hcitool -i hci0 cmd 0x3F 0x0019 0x80 0x80 0x80 0x80 0x01 0x00 0x01 0x01 0x0D 0x03 0x0F 0x00 0x00 0x00 0x00 0x00 0x00 0x04 < HCI Command: ogf 0x3f, ocf 0x0019, plen 18 80 80 80 80 01 00 01 01 0D 03 0F 00 00 00 00 00 00 04 > HCI Event: 0x0e plen 4 01 19 FC 00 # STOP THE TX TRANSMISSION root@oaslv:/home/hexagon# hcitool -i hci0 cmd 0x3F 0x0019 0x80 0x80 0x80 0x80 0xFF 0x00 0x01 0x01 0x0D 0x03 0x0F 0x00 0x00 0x00 0x00 0x00 0x00 0x04 < HCI Command: ogf 0x3f, ocf 0x0019, plen 18 80 80 80 80 FF 00 01 01 0D 03 0F 00 00 00 00 00 00 04 > HCI Event: 0xff plen 6 19 01 63 07 00 00 ** When disabling the scan before entering in the test mode, the stop for TX transmission give us: root@oaslv:/home/hexagon# hcitool -i hci0 cmd 0x3F 0x0019 0x80 0x80 0x80 0x80 0xFF 0x00 0x01 0x01 0x0D 0x03 0x0F 0x00 0x00 0x00 0x00 0x00 0x00 0x04 < HCI Command: ogf 0x3f, ocf 0x0019, plen 18 80 80 80 80 FF 00 01 01 0D 03 0F 00 00 00 00 00 00 04 > HCI Event: 0xff plen 6 19 01 ED 04 00 00 For Wifi 5 GHz -------------------------------------------------------------------------------- Paramters: Continuous transmit, BW = 40 MHz, 802.11ac, No DFS, CH = 40, MCS0 (13.5), Power = 14 dBm root@oaslv:/home/hexagon# cat /proc/mwlan/adapter0/config hardware_status=0 netlink_num=31 drv_mode=7 hssetpara=7,0xff,200,400 sdcmd52rw=0 0x0 0x00 rf_test_mode=1 tx_antenna=1 rx_antenna=1 band=1 bw=1 channel=44 radio_mode[0]=3 radio_mode[1]= total rx pkt count=0 rx multicast/broadcast pkt count=0 rx fcs error pkt count=0 tx_power=14 2 0 tx_continuous=0 tx_frame=1 4352 0xaaa 1024 1 20 4294967295 0 0 4294967295 0 0 0 -1 -1 -1 -1 -1 -1 -1 05:43:3f:c4:51:ff he_tb_tx=0 trigger_frame=0 otp_mac_add_rd_wr= 00:00:00:00:00:00
記事全体を表示
Ubuntu LinuxでのMCUXpresso IDEサポートに一体何が問題なのでしょうか? LinuxのMCUXpresso IDEでHello Worldプログラムを作るような、本当に単純なことなんて一つもありません。私はrt700のevkbボードを使っていますが、そのIDEは何度もクラッシュして切れてしまいます。ここ2〜3日ずっと苦戦しています。一体これは一体何なんだ?ある日は十分なサポートがあるはずですが、ある日は動かないのに。解決策を見つけるためのガイドもありません。基本的なプロジェクトを作成しても、ペリフェラルの設定タブを開くと、なぜか動作せず、奇妙なことにプロセッサコアがこれをサポートしていないとか、そんな感じです。最近はMicrosoft WindowsからこのIDE、そしてある程度はUbuntuまで、スロップか何かしらしかありません。このIDEを動かすには、Windows上でどうすればいいのですか?どうかこの問題を直してください。スクリーンショットも撮れません。あまりにもひどくフリーズします。 prathamvora_0-1784244137157.png Re: what the hell is wrong with MCUXpresso IDE support on ubuntu linux EVKBのBOMファイル自体は、IDEプロジェクト作成で使われるのと同じパッケージを使用しています。 prathamvora_1-1784245217062.png Re: what the hell is wrong with MCUXpresso IDE support on ubuntu linux ぜひこの動画を見て、このツールの使い方についてトレーニング動画も作ってください。VScode拡張機能を使うなんて、どれほどサポートが壊れるのか想像するしかありません。 Re: what the hell is wrong with MCUXpresso IDE support on ubuntu linux prathamvora_0-1784244495436.png システムを再起動してIDEを開くとこれが起きています Re: what the hell is wrong with MCUXpresso IDE support on ubuntu linux こんにちは、 @prathamvora さん。 MCUXpresso統合開発環境(IDE)のウェブページによると、サポートされているUbuntuバージョンはUbuntu 22.04 LTSとUbuntu 24.04 LTSです。Visual Studio Code版MCUXpressoの場合、サポートされているUbuntuバージョンはUbuntu 20.04.2 LTS、Ubuntu 22.04 LTS、Ubuntu 24.04 LTSです。 MCUXpresso IDEにはサポートされているUbuntuバージョン、Visual Studio CodeにはMCUXpressoを使うことをおすすめします。 よろしくお願いします、 パブロ
記事全体を表示
MRF13750H Schematic How to convert the MRF13750H-915MHz board to a schematic? The MRF13750H datasheet includes the reference board layout for 915 MHz, but not the schematic. Luis_V_1-1784224999094.png
記事全体を表示
NFCリーダー・ライブラリ こんにちは、みんな。 DESFire EV3カードに対応したサンプルおよびライブラリのPN7642 NDA版の見つけ方とダウンロード方法。 私はすでに有効なNDAを持っています。 再開まで今しばらくお待ちください。 NFCリーダー・ライブラリ Re: NFC reader library こんにちは、 @dbogovicさん。 あなたの調子が良いといいのですが。 すでに有効なNDAをお持ちの場合、MIFARE DESFireをサポートするPN7642 SDKは、このページの指示に従ってSecure Access Rightsを通じて申請する必要があります: Secure Access Rights | NXP Semiconductors。また、 Secure Access Rights FAQs(セキュリティアクセス権FAQs)も確認することをお勧めします。NXP Semiconductors。 利用可能なセキュアリソースは PN7642製品ページのソフトウェアセクション(セキュア)で確認できます。 よろしくお願いいたします。 エドゥアルド。
記事全体を表示
MPC5746C FXOSC 输出频率 部件: MPC5746C(电源架构 Z4,SDK:NXP MPC57xx 平台 SDK)。 MPC5746C 的手册中指出,FXOSC 提供 8 -40 MHz 的输出频率。请帮我查找FXOSC在以下配置下的输出频率? 1. FXOSC_CTL:OSCBYP = 0 且 OSCM = LCP 2. FXOSC_CTL:OSCBYP = 0 且 OSCM = FSP 3. FXOSC_CTL:OSCBYP = 1 且 OSCM = LCP 4. FXOSC_CTL:OSCBYP = 1 且 OSCM = FSP 请考虑为其他注册字段设置默认值。谢谢。 Re: MPC5746C FXOSC output frequency 感谢你的回复@petervlna 。 如何找到晶体/谐振器(OSCBYP = 0)和外部时钟(OSCBYP = 1)提供的频率? Re: MPC5746C FXOSC output frequency 你好, FXOSC 模块不会根据 OSCBYP 和 OSCM 设置生成特定频率。FXOSC 的输出频率始终等于连接到 FXOSC 的外部源的频率(当 OSCBYP=0 时为晶体/谐振器,当 OSCBYP=1 时为外部时钟),在支持的 8–40 MHz 范围内。 因此,对于列出的所有四种配置,FXOSC 输出频率就是外部输入频率。OSCM 设置(LCP/FSP)会影响振荡器的工作模式,但不会改变时钟频率。 顺祝商祺! Peter Re: MPC5746C FXOSC output frequency @petervlna请您协助解答我上面提到的关于 FXOSC 的问题。 Re: MPC5746C FXOSC output frequency 如何找到晶体/谐振器(OSCBYP = 0)和外部时钟(OSCBYP = 1)提供的频率? @petervlna ,请告诉我以上问题的答案。我想使用 FXOSC 作为定时器的时钟源。根据它提供的频率,我可以将计数值加载到定时器寄存器中。 Re: MPC5746C FXOSC output frequency 你好, MPC5746C 不提供从 FXOSC 寄存器测量或确定 FXOSC 频率的方法。频率必须从硬件设计中得知: OSCBYP = 0:FXOSC 频率等于安装在板上的外部晶体/谐振器的频率。 OSCBYP = 1:FXOSC 频率等于施加到 FXOSC 输入引脚的外部时钟信号的频率。 要将 FXOSC 用作定时器时钟源,应用程序在计算定时器计数值时必须使用电路板原理图或时钟设计中指定的频率(例如,8 MHz、16 MHz、40 MHz 等)。OSCBYP 和 OSCM 设置不会影响频率本身。 顺祝商祺! Peter
記事全体を表示
IW612 Bluetooth RFテスト 皆さん、こんにちは。 IW612を基にモジュールのRFテストを実行しようとしています。そのために、いくつかの文書を参考にしました。例えば: AN14310 - NXP Bluetooth UARTドライバ統合 AN14114 - Linux OS上のRFテストモード AN14163 - Bluetooth ダイレクトテストモード 他にも。 いくつか問題に直面しています: - Wi-Fi 5 GHzでは、5 GHz付近の低チャネルで波形が生成されず、高チャネルでしか波形が見えません - Bluetoothについては、クラシックなBluetoothで波形を生成できず、BLEでしか波形を生成できません(hcitoolでスキャンやペア情報取得のコマンドは問題なく動作するため、ハードウェアの問題ではないと思います) 私のセットアップでは、SoM Variscite Dart IMX8M(バージョン2.0)と2ELラジオを使い、IW612をベースにしています。波形を取得するために、HackRFを使用しています。 私はカーネル6.6.23を搭載したシステムを使用しています。Yoctoのカスタムバージョンと、Firmware sduart_nw61x_v1.bin.seを搭載しています。バージョンからのデフォルト HCIコマンドのフィードバックはドキュメントと互換性がありますが、波形は見えません。システムや手順に何か不足している点があれば、ご指摘いただけますでしょうか?これは認証プロセスの一部なのですが、今ここで行き詰まっています。 どうもありがとうございました Re: IW612 Bluetooth RF Test Hello テストのコマンドと結果のスクリーンショットを教えてもらえますか? よろしくお願いいたします。 ショーン Re: IW612 Bluetooth RF Test こんにちは、ショーンさん。 もちろん。hcitoolとwifi用にこれらのコマンドを実行しました。設定の最終ファイルを添付しました。 Bluetooth Classic用 ------------------------------------ これらのコマンドはUM11490(149ページ)から直接収集したものです。 # リセット root@oaslv:/home/hexagon# hcitool -i hci0 cmd 0x03 0x0003 < HCIコマンド:ogf 0x03、ocf 0x0003、プレン0 > HCIイベント:0x0eプレン4 01 03 0C 00 # スキャンを有効にする root@oaslv:/home/hexagon# hcitool -i hci0 cmd 0x03 0x001a 0x3 < HCIコマンド:ogf 0x03、ocf 0x001a、プレン1 03 > HCIイベント:0x0eプレン4 01 1A 0C 00 # イベントフィルターを有効にする root@oaslv:/home/hexagon# hcitool -i hci0 cmd 0x03 0x0005 0x02 0x00 0x02 < HCIコマンド:ogf 0x03、ocf 0x0005、プレン3 02 00 02 > HCIイベント:0x0eプレン4 01 05 0C 00 # テストモードでエントリー root@oaslv:/home/hexagon# hcitool -I HCi0 cmd 0x06 0x0003 < HCIコマンド:ogf 0x06、ocf 0x0003、プレン0 > HCIイベント:0x0eプレン4 01 03 18 00 # TXトランスミッションを開始 root@oaslv:/home/hexagon# hcitool -i hci0 cmd 0x3F 0x0019 0x80 0x80 0x80 0x80 0x01 0x00 0x01 0x01 0x0D 0x03 0x0F 0x00 0x00 0x00 0x00 0x00 0x00 0x04 < HCI司令部:ogf 0x3f、ocf 0x0019、プレン18 80 80 80 80 01 01 01 0D 03 0F 00 00 00 00 00 00 04 > HCIイベント:0x0eプレン4 01 19 FC 00 # TXの送信を止めろ root@oaslv:/home/hexagon# hcitool -i hci0 cmd 0x3F 0x0019 0x80 0x80 0x80 0x80 0xF F 0x00 0x01 0x01 0x0D 0x03 0x0F 0x00 0x00 0x00 0x00 0x00 0x00 0x04 < HCI司令部:ogf 0x3f、ocf 0x0019、プレン18 80 80 80 80 FF 00 01 01 0D 03 0F 00 00 00 00 00 04 > HCIイベント:0xffプレン6 19 01 39 00 00 00 --------------------、TXトランスミッションの前にBLEとCLASSICのスキャンを止めること---------------- # リセット root@oaslv:/home/hexagon# hcitool -i hci0 cmd 0x03 0x0003 < HCIコマンド:ogf 0x03、ocf 0x0003、プレン0 > HCIイベント:0x0eプレン4 01 03 0C 00 # スキャンを有効にする root@oaslv:/home/hexagon# hcitool -i hci0 cmd 0x03 0x001a 0x3 < HCIコマンド:ogf 0x03、ocf 0x001a、プレン1 03 > HCIイベント:0x0eプレン4 01 1A 0C 00 # イベントフィルターを有効にする root@oaslv:/home/hexagon# hcitool -i hci0 cmd 0x03 0x0005 0x02 0x00 0x02 < HCIコマンド:ogf 0x03、ocf 0x0005、プレン3 02 00 02 > HCIイベント:0x0eプレン4 01 05 0C 00 # テストモードでエントリー root@oaslv:/home/hexagon# hcitool -I HCi0 cmd 0x06 0x0003 < HCIコマンド:ogf 0x06、ocf 0x0003、プレン0 > HCIイベント:0x0eプレン4 01 03 18 00 # BLEスキャンを無効に root@oaslv:/home/hexagon# hcitool -i hci0 cmd 0x03 0x001a 0x0 < HCIコマンド:ogf 0x03、ocf 0x001a、プレン1 00 > HCIイベント:0x0eプレン4 01 1A 0C 00 # クラシックスキャンを無効にする root@oaslv:/home/hexagon# hcitool -i hci0 cmd 0x08 0x000C 0x00 0x00 < HCIコマンド:ogf 0x08、ocf 0x000c、プレン2 00 00 > HCIイベント:0x0eプレン4 01 0C 20 00 # TXトランスミッションを開始 root@oaslv:/home/hexagon# hcitool -i hci0 cmd 0x3F 0x0019 0x80 0x80 0x80 0x80 0x01 0x00 0x01 0x01 0x0D 0x03 0x0F 0x00 0x00 0x00 0x00 0x00 0x00 0x04 < HCI司令部:ogf 0x3f、ocf 0x0019、プレン18 80 80 80 80 01 01 01 0D 03 0F 00 00 00 00 00 00 04 > HCIイベント:0x0eプレン4 01 19 FC 00 # TXの送信を止めろ root@oaslv:/home/hexagon# hcitool -i hci0 cmd 0x3F 0x0019 0x80 0x80 0x80 0x80 0xFF 0x00 0x01 0x01 0x0D 0x03 0x0F 0x00 0x00 0x00 0x00 0x00 0x00 0x04 < HCI司令部:ogf 0x3f、ocf 0x0019、プレン18 80 80 80 80 FF 00 01 01 0D 03 0F 00 00 00 00 00 04 > HCIイベント:0xffプレン6 19 01 63 07 00 00 **テストモードに入る前にスキャンを無効にすると、TX送信の停止により次のようになります。 root@oaslv:/home/hexagon# hcitool -i hci0 cmd 0x3F 0x0019 0x80 0x80 0x80 0x80 0xFF 0x00 0x01 0x01 0x0D 0x03 0x0F 0x00 0x00 0x00 0x00 0x00 0x00 0x04 < HCI司令部:ogf 0x3f、ocf 0x0019、プレン18 80 80 80 80 FF 00 01 01 0D 03 0F 00 00 00 00 00 04 > HCIイベント:0xffプレン6 19 01 ED 04 00 00 Wi-Fi 5GHz用 -------------------------------------------------------------------------------- パラメータ: 連続送信、帯域幅 = 40 MHz、802.11ac、DFSなし、CH = 40、MCS0 (13.5)、電力 = 14 dBm root@oaslv:/home/hexagon# cat /proc/mwlan/adapter0/config hardware_status=0 netlink_num=31 drv_mode=7 hssetpara=7,0xff,200,400 SDCMD52RW=0 0x0 0x00 rf_test_mode=1 tx_antenna=1 rx_antenna=1 バンド=1 BW=1 チャネル=44 radio_mode[0]=3 radio_mode[1]= 総処方PKT数=0 RXマルチキャスト/ブロードキャストのPKTカウント=0 rx FCSエラー PKTカウント=0 tx_power=14 2 0 tx_continuous=0 tx_frame=1 4352 0xaaa 1024 1 20 4294967295 0 0 0 4294967295 0 0 0 0 -1 -1 -1 -1 -1 -1 -1 -1 05:43:3f:c4:51:ff he_tb_tx=0 trigger_frame=0 otp_mac_add_rd_wr= 00:00:00:00:00:00
記事全体を表示
NFC reader library Hello everyone. How to find and download the PN7642 NDA version of the examples and libraries with support for DESFire EV3 cards. I already have an active NDA. Thank you for your support. NFC Reader Library Re: NFC reader library Hello @dbogovic Hope you are doing well. If you already have an active NDA, PN7642 SDK supporting MIFARE DESFire must be requested through the Secure Access Rights by following the instructions from this page: Secure Access Rights | NXP Semiconductors. Also, I would recommend checking the Secure Access Rights FAQs | NXP Semiconductors. Available Secure Resources can be found in PN7642 product page, Software section (Secure). Regards, Eduardo.
記事全体を表示