2396129_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2396129_en-US

2396129_en-US

what the hell is wrong with MCUXpresso IDE support on ubuntu linux

not a single bloody simplest of the simplest thing like creating a hello world program in the MCUXpresso IDE on Linux. I have a rt700 evkb board and that ide just keep crashing and hanging up i am struggling with it for the past 2-3 days just what in the world is this BS. it is obviously expected to have a decent enough support one day it works and then the other day it does not. there is also no guide to have some fix. even after creating some basic project when opening the peripheral configuration tab it magically just does not work it weirdly just say the processor core whatever does not support this or something like that. these days all we have is slop or what from Microsoft windows to even this IDE and then to some degree ubuntu as well.  to run this ide what is do you expect us to do to run it on windows? please for love of everything please fix this issues and i can't even take a screenshot it hangs up that bad.  

prathamvora_0-1784244137157.pngprathamvora_0-1784244137157.png


Re: what the hell is wrong with MCUXpresso IDE support on ubuntu linux

The BOM file for the EVKB itself uses the same package as being used in ide project creation. 

prathamvora_1-1784245217062.pngprathamvora_1-1784245217062.png


Re: what the hell is wrong with MCUXpresso IDE support on ubuntu linux

please have  a look at this video and please make some training videos on how to even use this tool. let alone use the vscode extension i can only imagine what kind of broken support it is going to be.

Re: what the hell is wrong with MCUXpresso IDE support on ubuntu linux

prathamvora_0-1784244495436.pngprathamvora_0-1784244495436.png

this is what i get after rebooting my system and opening the IDE

Re: what the hell is wrong with MCUXpresso IDE support on ubuntu linux

Hi @prathamvora,

According to the MCUXpresso Integrated Development Environment (IDE) webpage, the supported Ubuntu versions are Ubuntu 22.04 LTS and Ubuntu 24.04 LTS. In the case of MCUXpresso for Visual Studio Code, the supported Ubuntu versions are Ubuntu 20.04.2 LTS, Ubuntu 22.04 LTS, and Ubuntu 24.04 LTS.

I would recommend using one of the supported Ubuntu versions for MCUXpresso IDE or MCUXpresso for Visual Studio Code.

Best Regards,
Pablo

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎07-18-2026 03:30 AM
更新者: