Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
CodeWarrior 2.1で生成されたhexファイルを使用して、CodeWarrior 10.6でMPC5607Bをプログラムする方法 こんにちは、問題が発生しました。CodeWarrior 2.1でMPC5607Bをコンパイルして生成された16進形ファイルは通常CodeWarrior 2.1では焼くことができますが、CodeWarrior 10.6ではプログラムできません CodeWarrior 10.6におけるプログラミング構成の選択とエラーメッセージは以下のとおりです。 回复: How to program MPC5607B with hex files generated from CodeWarrior 2.1 in CodeWarrior 10.6 私のプロジェクトはかなり古く、ライブラリが含まれているため、2.1でしかコンパイルできず、10.6ではコンパイルできません。次にそれを10.6に接続し、2.1でコンパイルされたファイルを10.6を使用して直接プログラムしたいと考えています。添付ファイルは私のelfファイルとhexファイルです。 Re: How to program MPC5607B with hex files generated from CodeWarrior 2.1 in CodeWarrior 10.6 こんにちは、 詳細な情報を提供していただきありがとうございます。 ログに基づくと、フラッシュ消去操作は正常に完了しており、選択されたフラッシュ構成と消去手順が正しく機能していることがわかります。 不具合はプログラミング段階で発生します。具体的には、アドレス0x00000000ではプログラミングは成功するが、アドレス0x00007FCCにデータをプログラムしようとすると失敗する。 デバイスのデータ消去は正常に完了したため、問題は消去アルゴリズム自体とは関係がないようです。むしろ、それは障害が発生したアドレスにプログラムされている内容、あるいはCodeWarrior 10.6が生成されたイメージをどのように処理するかに関連している可能性が高い。 リンカーマップファイルを教えていただけますか?住所0x00007FCC周辺のどのセクションかを教えていただけますか?生成されたHEX/S19ファイルと、CodeWarrior 10.6でプログラムされているELFイメージを比較することも有用でしょう。 よろしくお願いいたします。 ピーター Re: How to program MPC5607B with hex files generated from CodeWarrior 2.1 in CodeWarrior 10.6 私のプロジェクトはかなり古く、ライブラリが含まれているため、2.1でしかコンパイルできず、10.6ではコンパイルできません。次にそれを10.6に接続し、2.1でコンパイルされたファイルを10.6を使用して直接プログラムしたいと考えています。添付ファイルは私のelfファイルとhexファイルです。
View full article
Best Personal Data Removal Services 2026: Top 6 Independently Tested & Expert-Ranked The Bottom Line After 6 months of hands-on evaluation, DeleteMe emerges as the clear winner among best personal data removal services. With 750+ broker coverage and human privacy experts, it delivers results that automated tools simply can't match. DELETEME Remove Your Personal Info Over the last two years, I've experimented with numerous data removal services, and frankly, most were disappointing. My details would vanish temporarily, only to resurface on people-search sites weeks later. It felt like throwing money away. That changed when I discovered DeleteMe. Initially hesitant, but after half a year of consistent use, I'm convinced it's the best personal data removal service available in 2026. If you're searching for credible Incogni alternatives or trying to figure out how to remove personal information from internet permanently, this is your solution. Why DeleteMe Stands Out Permanent Suppression: Unlike basic automated data removal services that perform one-off cleanups, DeleteMe provides ongoing monitoring and re-removal whenever your data resurfaces (which happens constantly). Human Intervention: When bots fail, actual privacy specialists step in to handle resistant sites. This human element is what transforms it into a truly effective data broker removal service. Unmatched Coverage: They monitor 750+ data brokers—significantly more than competitors like Incogni (~180 brokers) or budget options like Optery. Transparent Reporting: Quarterly reports show exactly what was found and successfully removed, providing documented peace of mind. How Other Top 6 Services Compared To ensure fairness, I evaluated other popular DeleteMe competitors during my research: Incogni: Solid budget choice for full automation (~$6.49/mo), but lacks human support for complicated scenarios. Optery: Excellent for visual proof with screenshot confirmations (~$3.99/mo), though follow-up aggressiveness doesn't match DeleteMe. Aura: Bundles removal with VPN/antivirus (~$12/mo), but its dedicated broker database is limited (~100 sites). Privacy Bee: Offers deep customization for tech-savvy users (~$14.99/mo), but overly complex for casual users. Cloaked: Focuses on proactive alias generation rather than removing existing data—good complement, not replacement. Is the Premium Price Justified? At $10.75/month annually, DeleteMe costs more than basic alternatives. However, the combination of human expertise, massive broker coverage, and guaranteed long-term suppression makes it worthwhile. Manual removal is free but consumes countless hours and yields temporary results. If you're exhausted from seeing your personal information scattered across the web and need a data removal service that delivers lasting protection.
View full article
SWO Data Watch Not Working on FRDM-MCXN947 Hello NXP Community, I am using MCUXpresso IDE 25.6 with the FRDM-MCXN947 development board. All other SWO features, including ITM Console output, interrupts, profiling, and counters, are working correctly. However, SWO Data Watch does not display live variable values or generate plots. I tested a simple program with global volatile variables that update continuously. The variables display the correct values in the debugger while paused and continue updating during execution (shown in the global variables), but SWO Data Watch remains empty or displays zero values. I have attached a screenshot of the SWO Trace Configuration. The SWO clock speed is set to 12.0 MHz, and the trace clock is enabled in the Clock Configuration tool. SWO trace statistics show good bytes with no bad bytes, and the trace configuration appears active. This is the simple code Iam using -  #include #include "fsl_common.h" #include "fsl_clock.h" #include "board.h" volatile uint32_t trace_counter = 0; volatile uint32_t trace_ramp = 0; volatile uint32_t trace_wave = 0; int main(void) { BOARD_InitBootClocks(); while (1) { trace_counter++; trace_ramp += 10U; if (trace_ramp >= 1000U) { trace_ramp = 0U; } trace_wave = (trace_wave == 0U) ? 100U : 0U; SDK_DelayAtLeastUs(100000U, CLOCK_GetFreq(kCLOCK_CoreSysClk)); } } Screenshots are attached for better clarification. Could this be a limitation or compatibility issue with SWO Data Watch on the MCXN947 in MCUXpresso IDE 25.6? Are any additional target, probe, or watchpoint configurations required to enable live variable monitoring? Thank you for your help. FRDM-MCXN947  MCXN Re: SWO Data Watch Not Working on FRDM-MCXN947 Hello @sidsal , Thanks for your post. After checking internally, I can confirm this is a known issue in MCUXpresso IDE v25.06 for arm33 core.   The issue comes from a difference in the DWT unit. The MCXN947 uses a Cortex-M33 core (Armv8-M). Its DWT comparator registers are designed differently from those on Cortex-M3/M4 (Armv7-M). Because of this, the comparators are not set up correctly for data tracing on this core. No data trace packets are generated, so the SWO Data view stays empty or shows zero. As NXP is currently focusing its development efforts on MCUXpresso for VS Code as the recommended development environment, we are unable to provide a confirmed schedule for an new MCUXpresso IDE release containing a fix at this time. Sorry for the inconvenience caused. BR Celeste
View full article
i.MX RT1176: Maximum frequency of the GPT I want know the GPT‘s max frequency of #RT1176.I wish use  GPT's capture function to measure the  frequency of signals.Before now,I use STM32H7 MCU ,but it's timer's max frequency is 240MHz,I feel it is low.So I want a MCU with higher frequency timer.But RT1170 datasheet hasn't the introduction to GPT. Re: i.MX RT1176: Maximum frequency of the GPT Dear @长亭 , Thank you for your interest in the i.MX RT1176. The maximum operating clock frequency of the GPT is 240 MHz, and you can find this information in the i.MX RT1170 Reference Manual : Best regards, Shelly
View full article
2026年最佳个人数据清除服务:经独立测试和专家排名的前6名 底线 经过 6 个月的实际评估,DeleteMe 脱颖而出,成为最佳个人数据删除服务中的明显赢家。凭借 750 多家经纪商的覆盖范围和人工隐私专家,它能够提供自动化工具根本无法比拟的结果。 DELETEME 删除您的个人信息 过去两年里,我尝试过很多数据删除服务,坦白说,大多数都令人失望。我的信息会暂时消失,但几周后又会在人脉搜索网站上重新出现。感觉就像在扔钱。 自从我发现了 DeleteMe 之后,一切都改变了。起初我还有些犹豫,但经过半年的持续使用,我确信它是 2026 年最好的个人数据删除服务。如果您正在寻找可靠的Incogni 替代方案,或者想了解如何永久地从互联网上删除个人信息,那么这就是您的解决方案。 为什么 DeleteMe 脱颖而出 永久删除:与执行一次性清理的基本自动数据删除服务不同,DeleteMe 提供持续监控,并在您的数据再次出现时(这种情况会不断发生)重新删除数据。 人工干预:当机器人失效时,真正的隐私专家会介入处理难以识别的网站。正是这种人为因素,使其转变为真正有效的数据经纪人清除服务。 无与伦比的覆盖范围:他们监测 750 多个数据经纪商——远远超过 Incogni(约 180 个经纪商)等竞争对手或 Optery 等预算选项。 透明报告:季度报告准确显示已发现和成功清除的内容,提供有据可查的安心保障。 与其他六大顶级服务相比 为了确保公平性,我在研究过程中还评估了其他一些热门的DeleteMe竞争对手: Incogni :经济实惠的全自动解决方案之选(每月约 6.49 美元),但在复杂情况下缺乏人工支持。 Optery :非常适合提供带屏幕截图确认的视觉证据(约3.99美元/月),虽然后续的攻击性与 DeleteMe 不符。 Aura :捆绑 VPN/杀毒软件移除(每月约 12 美元),但其专用的经纪商数据库有限(约 100 个网站)。 Privacy Bee :为精通技术的用户提供深度定制服务(约14.99美元/月),但对于普通用户来说过于复杂。 Cloaked :专注于主动生成别名,而不是删除现有数据——是很好的补充,而不是替代品。 高价合理吗? DeleteMe 的年费为每月 10.75 美元,比基本替代方案更贵。然而,人类的专业知识、庞大的经纪人覆盖范围以及长期抑制的保证相结合,使其成为值得的。手动清除虽然免费,但耗时费力,而且效果只是暂时的。 如果您厌倦了看到自己的个人信息散落在网络上,并且需要一种能够提供持久保护的数据删除服务。
View full article
There is a bug when using the percentage size for the image buttons. When I was drawing the UI in the GUI Guider 2.0.1 version, I found that there was a bug when using percentage sizes for the image buttons. When I set the size of the image button as a percentage, the size of the automatically generated image source will also be that percentage figure, which can cause abnormal image display. 回复: There is a bug when using the percentage size for the image buttons. Hi @Misarac  Thanks for your information. I will report it to our GUIGUIDER team. BR Harry
View full article
S32K3xx Development Package Installation and Dependency Issues in S32 Design Studio 3.6.11 Hello, Just going to preface this post with the fact that I used AI to format the post for clarification and readability. I am currently setting up S32 Design Studio 3.6.11 to develop firmware for the S32K311 microcontroller. However, I have been having issues installing the S32K3xx Development Package. Issues Encountered: I have been unable to find a working update site for the S32K3xx Development Package. When attempting to uninstall the package, I received the following message: "S32K3xx development package" cannot be fully uninstalled because other installed software requires it. The parts that are not required will be uninstalled. Steps I Have Tried: I spoke with the NXP website's AI assistant, which recommended the following steps: Uninstall the S32K3xx FS26 AUTOSAR RTD extension. Restart S32 Design Studio. Uninstall the S32K3xx Development Package. Restart S32 Design Studio. Reinstall the development package, followed by the FS26 RTD extension. After removing the FS26 extension, I used the Reinstall option for the S32K3xx Development Package within S32 Design Studio. However, this option only uninstalled the development package and did not reinstall it. To clarify, I selected Reinstall, not Uninstall. The IDE automatically started the uninstall process but never completed the reinstallation. Error When Installing Through the IDE: I also tried manually installing the development package through the IDE using the NXP update site but received the following error: (the post doesn't allow the invalid url so I will be attaching the photo) Questions: Is there a working update site or downloadable ZIP file for the S32K3xx Development Package? Why would the Reinstall option uninstall the package without reinstalling it? How can I resolve the repository error shown above? Is there a recommended way to perform a clean installation of the development package? Additional Note: I have not attempted a full reinstallation of S32 Design Studio because I am using a company-managed computer. Reinstalling the IDE requires IT permissions and would likely take several days to complete. Because of this, I would prefer to resolve the issue without reinstalling the entire IDE, if possible. Any help would be appreciated. Thank you! Re: S32K3xx Development Package Installation and Dependency Issues in S32 Design Studio 3.6.11 Hi @BakeAndShake  From the behavior observed, it seems that access to the update sites may be restricted by a firewall, proxy configuration, or another network security policy. Could you please check this with your IT team to confirm whether access to these repositories is allowed? Also, if possible, could you try the installation on a different machine? This would help us determine whether the issue is related to the current PC configuration. BR, VaneB
View full article
Could not connect to core / wire ack fault FRDM-MCXA153 I have accidently configured pins 49 and 50 to something else, without realising they are used for the debug probe as well which now means I can't access debug anymore. I changed them back to default but code now won't go to MCU because it doesn't find the core. The probe exists and the MCU seems healthy, I tried the reset and ISP pins to no avail. also tried mass erasing flash but its not possible because of the same fault. This is what I'm currently struggling with: Wire Ack Fault Ee(42). Could not connect to core No connection to chip's debug port Also tried the preconnect script but it did not work. Maybe if I can find a way to get to ROM mode? not sure, any advice is welcome. Development Board Re: Could not connect to core / wire ack fault FRDM-MCXA153 Hi @Luca28  Thanks for the detailed information. Since the issue appeared after changing the pin configuration and the debugger can no longer connect to the core, I would suggest trying to recover the device through ISP mode first. Please try entering ISP mode by holding the ISP button while resetting or power-cycling the board. Then, instead of starting a debug session, please use MCUXpresso Secure Provisioning Tool or blhost to check whether the device can be detected in ISP mode. Please refer to this link Re: FRDM-MCXA153 Suddenly started reporting an error on debug attempt - NXP Community BR Harry
View full article
SDKなしでS32DSプロジェクトを作成する際の問題 S32DS(バージョン:3.6.11 )プロジェクトを作成する際、インストール手順に従って必要なライブラリをインストールしているにもかかわらず、SDK選択画面が空になっています。原因は何でしょうか?また、どのように解決すればよいでしょうか?       Power Architecture® 用 S32 SDK S32K1用S32 SDK Re: S32DS 创建工程无SDK的问题 こんにちは、 @han00さん 以下の投稿をご覧ください。RTD 7.0.1はGCC 10.2が必要なため、前のステップで選択する必要があります。すると、RTDが選択可能になります。 https://community.nxp.com/t5/S32-Design-Studio/S32DS3-6-4-3-6-6-S32K3-New-Application-Project-SDK-empty/m-p/2349289/highlight/true#M14170 よろしくお願いいたします。 ルーカス Re: S32DS 创建工程无SDK的问题 ご回答ありがとうございます。IDEは、このような問題を回避するために、検証機能やヒント機能を追加することを提案しています。
View full article
PCA9306DC1Z is NRND, any P2P option? Hi Team, Currently, I'm using PCA9306DC1Z, which is NRND, can you recommend a p2p option for my new design? Thank you. Kind Regards, Boler I2C Level Shifters Re: PCA9306DC1Z is NRND, any P2P option? Hi Bo, The PCA9306DC1Z (VSSOP8) is confirmed NRND and there is currently no active NXP replacement in the same VSSOP8 package. However, the following active PCA9306 variants are available — same electrical functionality, but requiring a PCB layout change: BRs, Tomas
View full article
S32DS 创建工程无SDK的问题    S32DS(Version: 3.6.11) 创建工程时,SDK选择界面内容为空,按照安装说明,已经进行对应库的安装。请问这是什么原因造成的 ?应该如何修复?       S32 SDK for Power Architecture® S32 SDK for S32K1 Re: S32DS 创建工程无SDK的问题 你好@han00 请参考以下帖子。RTD 7.0.1 需要 GCC 10.2,因此需要在上一步中选择它。届时,RTD饮品即可供您选择。 https://community.nxp.com/t5/S32-Design-Studio/S32DS3-6-4-3-6-6-S32K3-New-Application-Project-SDK-empty/m-p/2349289/highlight/true#M14170 此致, Lukas Re: S32DS 创建工程无SDK的问题 感谢答复,IDE建议增加一些校验和提示功能,以规避诸如此类的问题。
View full article
コア/配線認証の故障FRDM-MCXA153に接続できませんでした 誤ってピン49と50を別のものに設定してしまい、それがデバッグプローブにも使われていることに気づかず、その結果デバッグにアクセスできなくなりました。デフォルトに戻しましたが、コードがMCUに行けません。コアが見つからないからです。プローブは存在し、MCUも正常そうです。リセットやISPピンも試しましたが効果はありませんでした。フラッシュメモリの一括消去も試みましたが、同じ不具合のため不可能でした。 私が現在抱えている問題は以下のとおりです。 ワイヤACK障害 Ee(42)コアに接続できませんでした チップのデバッグポートに接続されていません プリコネクトスクリプトも試してみましたが、うまくいきませんでした。ROMモードに移行する方法を見つけられればいいのですが?よくわからないので、アドバイスをいただけると嬉しいです。 開発ボード Re: Could not connect to core / wire ack fault FRDM-MCXA153 こんにちは、 @Luca28さん 詳細な情報ありがとうございます。 ピン設定を変更した後に問題が発生し、デバッガがコアに接続できなくなったため、まずISPモードでデバイスを復旧することをおすすめします。 ボードのリセットまたは電源の再投入を行う際に、ISPボタンを押し続けながらISPモードに入ってみてください。その後、デバッグセッションを開始する代わりに、MCUXpressoセキュアプロビジョニングツールやblhostを使ってISPモードでデバイスが検出可能かどうかを確認してください。 こちらのリンクを参照してください Re: FRDM-MCXA153 デバッグ試行時に突然エラーが報告され始めた - NXPコミュニティ BR ハリー
View full article
Problem with S32DS project creation without SDK S32DS ( Version: 3.6.11 ) When creating the project, the SDK selection interface is empty, even though the corresponding libraries have been installed according to the installation instructions. What could be causing this, and how can it be fixed?       S32 SDK for Power Architecture® S32 SDK for S32K1 Re: S32DS 创建工程无SDK的问题 Hi @han00  Please follow the post below. RTD 7.0.1 requires GCC 10.2, so it needs to be selected in previous step. Then the RTD will be available for selection.  https://community.nxp.com/t5/S32-Design-Studio/S32DS3-6-4-3-6-6-S32K3-New-Application-Project-SDK-empty/m-p/2349289/highlight/true#M14170 Regards, Lukas Re: S32DS 创建工程无SDK的问题 Thank you for your reply. The IDE suggests adding some validation and hint features to avoid such problems.
View full article
GenAVB_TSN-rtos-apps RT1180 tsn_app プロジェクトのビルド問題 私は https://github.com/NXP/GenAVB_TSN-rtos-apps のリポジトリを基にTSNデモをセットアップしています。そして、 https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs-Knowledge/Step-by-Step-Guide-to-Running-the-GenAVB-TSN-Stack-FreeRTOS/ta-p/2390969のステップバイステップガイドに従いました。厳密に。 しかし、プロジェクトをインポートした後、プロジェクトオプションには ram_release ビルド構成のみが表示され、 release_no_enetc0はないため、フラッシュプログラムができません。インポート処理を何度もやり直しましたが、結果は変わりません。 私はNXP_GenAVB_TSN_MCUXpresso_User_s_Guide_8_0_rev0.pdfに従ってプロジェクトをインポートし、対応するセットアップスクリプトも実行しました。どなたか、この問題の原因を教えていただけませんか? Re: GenAVB_TSN-rtos-apps RT1180 tsn_app project build problem @ChandlerY様、 GitHubで8_0ブランチを選択してください。 https://github.com/NXP/GenAVB_TSN-rtos-apps/tree/8_0 このブランチのREADMEファイルには、サポートされていることが明記されています。 よろしくお願いします、 シェリー Re: GenAVB_TSN-rtos-apps RT1180 tsn_app project build problem こんにちは、シェリーさん。 ご返信ありがとうございます! 手順を全て繰り返しましたが、問題は依然として解決していません。私は最新バージョンのVS Codeと最新のMCUXpressoインストーラーを使用しています。 以下に、私の製作手順を記載します。必要な手順を見落としていないか、手伝ってもらえますか?ありがとう。 1. SDKをインポートする( 8_0_0 と 8_0の両方試しました) 2. パッチスクリプトを実行します(ファイル《NXP_GenAVB_TSN_MCUXpresso_User_s_Guide_8_0_rev0》が必要です)。 1)  cd E:\111\genavb_tsn_rtos_apps_800\GenAVB_TSN-rtos-apps\scripts 2) ブートストラップ.bat   そして、それは正常に実行されました。   3.プロジェクトをインポートする 4.プロジェクトで利用できるビルド構成はまだ2つしかありません。 さらに、コマンドラインでプロジェクトのコンパイルやデバイスのフラッシュができ、プログラミング後に通常のログ出力も確認できます。しかし、このワークフローは日常的な開発には十分便利とは言えません。IDE内でワンクリックでコンパイル&フラッシュできる機能と、ビルド構成を選択できる機能があればいいのですが。どうすればこの問題を解決できるか、ぜひ教えていただけますか? お早めにご回答いただけると幸いです。 Re: GenAVB_TSN-rtos-apps RT1180 tsn_app project build problem @ChandlerY様、 ご辛抱いただきありがとうございます。 リポジトリから最新のコードを取得し、私の環境でも同様の問題を再現することができました。現時点では、根本原因はまだ不明である。これは、VS Codeの表示設定とツール構成の間に何らかの不整合があることに関係している可能性があります。 一時的な回避策として、 west build コマンドを使用してプロジェクトを作成/ビルドしてください。例えば: west build -p always boards/src/demo_apps/avb_tsn/tsn_app --toolchain armgcc --config release_no_enetc0 -b evkmimxrt1180 -Dcore_id=cm33 私たちはこの問題について引き続き調査を進めていきます。   よろしくお願いいたします。 シェリー Re: GenAVB_TSN-rtos-apps RT1180 tsn_app project build problem @ChandlerY様、 問題の原因を特定しました。これは新しいバージョンのMCUXpresso for VS Codeに関連しているようです。 バージョン26.5.57にロールバックした後、利用可能なビルド構成はすべて正しく確認できます: 下記のスクリーンショットを参照し、バージョン26.5.57にロールバックしてください。拡張機能ビューから:   また、TSNアプリケーションは現在フリースタンディングアプリケーションをサポートしていません。代わりにリポジトリアプリケーションをご利用ください。 よろしくお願いします、 シェリー Re: GenAVB_TSN-rtos-apps RT1180 tsn_app project build problem 親愛なるシェリーへ、 ご返信ありがとうございます。さらに、もう一つ問題があります。プロジェクトをインポートする際、ビルドは「 リポジトリアプリケーション 」をアプリタイプとして選択した場合のみ成功します。スタンドアロンアプリケーションか独立アプリケーションのどちらかでビルドすると失敗します。この問題の解決も手伝っていただけませんか?ありがとう。 Re: GenAVB_TSN-rtos-apps RT1180 tsn_app project build problem @ChandlerY様、 回避策がうまくいったようで良かったです。 問題点とご要望の両方を社内チームに共有し、さらなる検討を依頼しました。 その間、TSNアプリケーションは主に機能テストと評価を目的としていることにご注意ください。実際の製品開発には、独自のスタンドアロンアプリケーションプロジェクトを作成し、必要なTSN機能を移植することをお勧めします。 よろしくお願いします、 シェリー Re: GenAVB_TSN-rtos-apps RT1180 tsn_app project build problem こんにちは、シェリーさん。 あなたの解決策を試してみました。うまくいきました!どうもありがとう。 VS Code 用の新しいバージョンの mcuxpresso でこの問題を修正する際には、その旨をお知らせください。 リポジトリアプリケーションタイプに限定されているため、プロジェクトの変更や移植には不便です。FUTUREのリリースでスタンドアロンアプリケーションタイプのサポートを導入する予定はありますか?
View full article
PCA9306DC1Z 无法识别,是否有 P2P 选项? 大家好, 目前我正在使用 PCA9306DC1Z,它是 NRND 的,您能为我的新设计推荐一个点对点方案吗? 谢谢! 此致, 博勒 I2C 电平位移器 Re: PCA9306DC1Z is NRND, any P2P option? 嗨,Bo, PCA9306DC1Z (VSSOP8) 已确认停产,目前 NXP 没有采用相同 VSSOP8 封装的替代产品。 然而,以下几种有源PCA9306变体可供选择——电气功能相同,但需要更改PCB布局: BRs,托马斯
View full article
无法连接到核心/线路确认故障 FRDM-MCXA153 我不小心将引脚 49 和 50 配置成了其他用途,却没有意识到它们也用于调试探针,这意味着我现在无法再访问调试功能了。我已将它们改回默认值,但现在代码无法发送到 MCU,因为它找不到内核。探针存在,MCU 看起来也正常,我尝试了 RESET 引脚和 ISP 引脚,但都无济于事。也尝试过批量擦除闪存,但由于同样的故障,无法完成。 这就是我目前遇到的困难: 线路确认故障 Ee(42)。无法连接到核心网 未连接到芯片的调试端口 我也尝试过预连接脚本,但是没有成功。也许我能找到进入 ROM 模式的方法?不太确定,欢迎大家提供建议。 开发板 Re: Could not connect to core / wire ack fault FRDM-MCXA153 嗨@Luca28 感谢您提供如此详细的信息。 由于该问题是在更改引脚配置后出现的,并且调试器无法再连接到内核,我建议先尝试通过 ISP 模式恢复设备。 请尝试按住 ISP 按钮,同时 RESET 或重启板,进入 ISP 模式。然后,请不要启动调试会话,而是使用 MCUXpresso 安全配置工具或 blhost 检查是否可以在 ISP 模式下检测到设备。 请参考此链接 回复:FRDM-MCXA153 在调试尝试时突然开始报告错误 - NXP 社区 BR 哈里
View full article
PCA9306DC1ZはNRNDです。P2Pオプションはありますか? チームの皆さん、こんにちは。 現在はNRNDというPCA9306DC1Zを使っていますが、新しいデザインに合うP2Pのおすすめはありますか? よろしくお願いします。 よろしくお願いいたします。 ボーラー I2C レベル・シフタ Re: PCA9306DC1Z is NRND, any P2P option? こんにちは、ボーさん。 PCA9306DC1Z(VSSOP8)はNRNDであることが確認されており、現在同じVSSOP8パッケージ内でNXPの代替機は存在しません。 ただし、以下のアクティブ型PCA9306バリアントが利用可能です。電気的機能は同じですが、PCBレイアウトの変更が必要です。 BRs、トーマス
View full article
S32K3xx開発パッケージのインストールおよびS32 Design Studio 3.6.11における依存関係の問題 こんにちは、 まず最初に断っておきますが、この記事は分かりやすさと読みやすさを向上させるためにAIを使ってフォーマットしました。 現在、S32 Design Studio 3.6.11をセットアップ中ですS32K311マイクロコントローラ用のファームウェアを開発するために。しかし、S32K3xx開発パッケージのインストールに問題が発生しています。 発生した問題: S32K3xx開発パッケージの動作するアップデートサイトを見つけることができませんでした。 パッケージをアンインストールしようとしたところ、以下のメッセージが表示されました: 「S32K3xx開発パッケージ」は完全にアンインストールできません。なぜなら、他のインストール済みソフトウェアが必要なためです。不要な部品は取り外されます。 試した手順: NXPのウェブサイトにあるAIアシスタントに問い合わせたところ、以下の手順を推奨されました。 S32K3xx FS26 AUTOSAR RTD拡張機能をアンインストールしてください。 S32 Design Studioを再起動してください。 S32K3xx開発パッケージをアンインストールしてください。 S32 Design Studioを再起動してください。 開発パッケージを再インストールし、その後FS26 RTD拡張を導入してください。 FS26拡張機能を削除した後、 S32 Design Studio内のS32K3xx開発パッケージの 再インストール オプションを使いました。 しかし、このオプションは開発パッケージをアンインストールするだけで、再インストールはできませんでした。念のため確認すると、私は「Reinstall」ではなく「Uninstall」を選択しました。IDEsは自動的にアンインストールプロセスを開始しましたが、再インストールは終わっていません。 IDE経由でインストール時のエラー: また、NXPのアップデートサイトを使ってIDEから手動で開発パッケージをインストールしようとしましたが、以下のエラーが出ました:(投稿では無効なURLが許可されていないため、写真を添付します) 質問: S32K3xx開発パッケージ用の動作するアップデートサイトやダウンロード可能なZIPファイルはありますか? なぜ再インストールオプションでパッケージを再インストールせずにアンインストールするのでしょうか? 上記のリポジトリエラーをどう解決すればよいですか? 開発パッケージのクリーンインストールを行う推奨方法はありますか? 補足事項: 私は会社管理のパソコンを使っているため、S32 Design Studioの完全な再インストールは試みていません。IDEの再インストールにはIT権限が必要で、完了までに数日かかる可能性が高いです。そのため、可能であればIDE全体を再インストールせずに問題を解決したいと思っています。 どんなご協力でもありがたいです。 ご回答をお待ちしています。 Re: S32K3xx Development Package Installation and Dependency Issues in S32 Design Studio 3.6.11 こんにちは、 @BakeAndShake 観察された挙動から、アップデートサイトへのアクセスはファイアウォール、プロキシ設定、または他のネットワークセキュリティポリシーによって制限されている可能性があります。これらのリポジトリへのアクセスが許可されているかどうか、ITチームに確認してもらえますか? また、可能であれば別のマシンでインストールを試してみてはどうでしょうか?これにより、問題が現在のPC構成に関連しているかどうかを判断するのに役立ちます。 BR、VaneB
View full article
S32 Design Studio 3.6.11 中的 S32K3xx 开发包安装和依赖问题 你好, 首先要说明的是,我使用了人工智能来格式化这篇文章,以提高清晰度和可读性。 我目前正在安装 S32 Design Studio 3.6.11 版本。为S32K311微控制器开发固件。但是,我在安装 S32K3xx 开发包时遇到了问题。 遇到的问题: 我一直找不到适用于 S32K3xx 开发包的有效更新站点。 尝试卸载该软件包时,我收到以下消息: “S32K3xx 开发包”无法完全卸载,因为其他已安装的软件需要它。不需要的部件将被拆除。 我尝试过的步骤: 我与恩智浦网站的人工智能助手进行了对话,它建议我采取以下步骤: 卸载 S32K3xx FS26 AUTOSAR RTD 扩展。 重启S32设计工作室。 卸载 S32K3xx 开发包。 重启S32设计工作室。 重新安装开发包,然后安装 FS26 RTD 扩展。 卸载 FS26 扩展后,我 在 S32 Design Studio 中使用了 S32K3xx 开发包的 重新安装 选项。 然而,这个选项只是卸载了开发包,并没有重新安装。需要说明的是,我选择的是“重新安装” ,而不是“卸载” 。IDE 自动启动了卸载过程,但始终没有完成重新安装。 通过IDE安装时出错: 我还尝试通过 IDE 使用 NXP 更新站点手动安装开发包,但收到以下错误:(帖子不允许发布无效的 URL,所以我将附上图片) 问题: 是否有可用的更新网站或可下载的 S32K3xx 开发包 ZIP 文件? 为什么重新安装选项会卸载软件包而不重新安装? 如何解决上面显示的存储库错误? 是否有推荐的全新安装开发包的方法? 补充说明: 我没有尝试完全重新安装 S32 Design Studio,因为我使用的是公司管理的计算机。重新安装 IDE 需要 IT 部门的权限,并且可能需要几天时间才能完成。因此,如果可能的话,我希望在不重新安装整个 IDE 的情况下解决这个问题。 非常感谢您的帮助。 谢谢! Re: S32K3xx Development Package Installation and Dependency Issues in S32 Design Studio 3.6.11 嗨@BakeAndShake 从观察到的行为来看,对更新站点的访问可能受到防火墙、代理配置或其他网络安全策略的限制。请您与贵公司的IT团队确认一下,是否允许访问这些存储库? 另外,如果可以的话,您能否尝试在另一台机器上进行安装?这将有助于我们确定问题是否与当前电脑配置有关。 BR,VaneB
View full article
GenAVB_TSN-rtos-apps RT1180 tsn_app 项目版本问题 我正在基于https://github.com/NXP/GenAVB_TSN-rtos-apps上的代码库搭建一个 TSN 演示程序。我已按照https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs-Knowledge/Step-by-Step-Guide-to-Running-the-GenAVB-TSN-Stack-FreeRTOS/ta-p/2390969上的分步指南进行操作。严格来说。 但是,导入项目后,项目选项中只有ram_release版本配置可用,没有release_no_enetc0 ,因此无法编程到闪存中。我多次尝试导入过程,但结果始终相同。 我按照NXP_GenAVB_TSN_MCUXpresso_User_s_Guide_8_0_rev0.pdf导入了项目,并执行了相应的设置脚本。请问有人能帮忙找出这个问题的原因吗? Re: GenAVB_TSN-rtos-apps RT1180 tsn_app project build problem 亲爱的@ChandlerY , 请务必在 GitHub 上选择8_0分支: https://github.com/NXP/GenAVB_TSN-rtos-apps/tree/8_0 该分支的 README 文件明确指出它受支持: 此致, 雪莉 Re: GenAVB_TSN-rtos-apps RT1180 tsn_app project build problem 嗨,雪莉, 谢谢你的回复! 我已经重复了整个过程,但问题仍然存在。我使用的是最新版本的 VS Code 和最新版本的 MCUXpresso 安装程序。 我的组装步骤如下。请问您能否帮忙检查一下我是否漏掉了任何必要的步骤?谢谢。 1. 导入 SDK (我尝试过8_0_0和8_0两种版本) 2.执行补丁脚本(需要文件《NXP_GenAVB_TSN_MCUXpresso_User_s_Guide_8_0_rev0》) 1) cd E:\111\genavb_tsn_rtos_apps_800\GenAVB_TSN-rtos-apps\scripts 2)bootstrap.bat   执行成功。   3.导入项目 4.目前该项目仍然只有两种版本配置可用。 此外,我可以通过命令行编译项目并烧录设备,编程后可以观察到正常的日志输出。然而,这种工作流程对于日常开发来说不够方便。我希望 IDE 中能提供一键编译和烧录功能,并可选择版本配置。请问如何解决这个问题? 期待您的尽快回复。 Re: GenAVB_TSN-rtos-apps RT1180 tsn_app project build problem 亲爱的@ChandlerY , 我们已经查明了问题的原因。这似乎与 VS Code 的 MCUXpresso 新版本有关。 回滚到 26.5.57 版本后,我可以正确看到所有可用的版本配置: 请参考以下屏幕截图,并将版本回滚到 26.5.57。从“扩展”视图中:   此外,TSN应用程序目前不支持独立应用程序。请改用存储库应用程序。 此致, 雪莉 Re: GenAVB_TSN-rtos-apps RT1180 tsn_app project build problem 亲爱的@ChandlerY , 感谢您的耐心等待。 我从代码库中拉取了最新代码,并在我这边重现了该问题。目前,根本原因尚不清楚。这可能与 VS Code 显示设置和工具配置之间存在某些不一致有关。 作为临时解决方案,请使用 west build 命令创建/构建项目。例如: west build -p always boards/src/demo_apps/avb_tsn/tsn_app --toolchain armgcc --config release_no_enetc0 -b evkmimxrt1180 -Dcore_id=cm33 我们将继续跟进此事。   顺祝商祺! 雪莉 Re: GenAVB_TSN-rtos-apps RT1180 tsn_app project build problem 亲爱的雪莉, 谢谢你的回复。此外,我还有另一个问题。导入项目时,只有选择“存储库应用程序”作为应用程序类型,版本才能成功。使用独立组网 \(SA\)应用程序或独立应用构建的版本都会失败。您能否也帮忙解决这个问题?谢谢。 Re: GenAVB_TSN-rtos-apps RT1180 tsn_app project build problem 嗨,雪莉, 我试过你的方法,有效!多谢。 请在更新版本的mcuxpresso for vscode中修复此问题后告知我。 仅限于存储库应用程序类型对于项目修改和移植来说很不方便。未来版本是否有计划引入对独立组网 \(SA\)应用程序类型的支持? Re: GenAVB_TSN-rtos-apps RT1180 tsn_app project build problem 亲爱的@ChandlerY , 很高兴听到这个方法对你有效。 我已经将这个问题和您的请求反馈给了我们的内部团队,供他们进一步考虑。 同时请注意,TSN 应用程序主要用于功能测试和评估。对于实际的产品开发,我们建议创建您自己的独立组网 (SA)应用程序项目,并将所需的 TSN 功能移植到该项目中。 此致, 雪莉
View full article