Correct snvs_cfg values for TAMPER_OUT0/TAMPER_IN4 active tamper loop on i.MX8DXL EVK (J20) Hi, I'm validating the external active-tamper loop on the i.MX8DXL EVK (MCIMX8DXL-WEVK) via U-Boot. From the board schematic, I've confirmed J20 (TAMPER header, 1x3) is wired as: - Pin 1 = TAMPER_IN4 (net SNVS.TAMPER_IN4, ball AJ13) - Pin 2 = GND - Pin 3 = TAMPER_OUT0 (net SNVS.TAMPER_OUT0, ball AP22) These are dedicated SNVS pins, not shared with SAI2/SAI3 like TAMPER_OUT1-4/IN0-3. Available U-Boot commands: tamper_pin_cfg, snvs_cfg (with sub-registers hp.lock, hp.secvio_intcfg, hp.secvio_ctl, lp.lock, lp.secvio_ctl, lp.tamper_filt_cfg, lp.tamper_det_cfg, lp.tamper_det_cfg2, lp.tamper_filt1_cfg, lp.tamper_filt2_cfg, lp.act_tamper1_cfg through lp.act_tamper5_cfg, lp.act_tamper_ctl, lp.act_tamper_clk_ctl, lp.act_tamper_routing_ctl1, lp.act_tamper_routing_ctl2), snvs_sec_status, snvs_clear_status. Since TAMPER_OUT0/TAMPER_IN4 form an active tamper pair, my questions: 1. Which lp.act_tamperN_cfg channel (1-5) corresponds to TAMPER_OUT0? 2. What values for lp.act_tamper_routing_ctl1/routing_ctl2 route TAMPER_OUT0's pattern to be checked against TAMPER_IN4? 3. What value for lp.act_tamper_clk_ctl enables the pattern clock for this channel? 4. What value for lp.act_tamper_ctl globally enables active tamper detection for this channel? Goal: closing a jumper across J20 pins 1-3 should read as secure in snvs_sec_status, and opening it should trigger a violation. I've attempted several values on hardware (routing 4, 5, 10; various clock/detector settings) — all were either rejected by the SECO firmware (error res:9 / SC_ERR_PARM) or accepted with no observable change in snvs_sec_status's SNVS a4(1) (LPTDSR) register when physically toggling the loop. Is there a reference test procedure or app note for external active tamper validation on i.MX8DXL? Thanks! Re: Correct snvs_cfg values for TAMPER_OUT0/TAMPER_IN4 active tamper loop on i.MX8DXL EVK (J20) Hello,
1. lp.act_tamper1_cfg drives TAMPER_OUT0.
2. The i.MX8DXL SNVS has 5 Active Tamper (AT) output sources and up to 8 External Tamper (ET) input detectors.
Please use this configuration:
lp.act_tamper_routing_ctl1 = 0x00010000 # ET5 (TAMPER_IN4) to AT1 (TAMPER_OUT0) lp.act_tamper_routing_ctl2 = 0x00000000 # ET6-ET8 not used
3. That value changes the clock divider, use 0x00 for maximum frequency configuration.
lp.act_tamper_clk_ctl = 0x00000000
4. Use lp.act_tamper_ctl = 0x00010001:
Bit 0: AT1EN enable AT1 LFSR pattern generator
Bit 16: AT1_OUT_EN drive TAMPER_OUT0 pad with AT1 pattern
There is no application note available for this processor but you can use this from an i.MX7 that can be used as reference:
/* Config ET5 (pin in et4) <-> (pin out et5) AT 1 *
/* reset */
write32(0, &svregs->lp.act_tamper_clk_ctl);
write32(0, &svregs->lp.act_tamper_ctl);
write32(0, &svregs->lp.tamper_det_cfg);
write32(0, &svregs->lp.tamper_det_cfg2)
/* Deault value for LFSR */
write32(0x84000000 | 0x00001111, &svregs->lp.act_tamper1_cfg)
/* Set the clock at max freq */
write32(0x00000000, &svregs->lp.act_tamper_clk_ctl);
/* ET5 (pin et4) takes ref from AT1 (pin et5) */
write32(0x00010000, &svregs->lp.act_tamper_routing_ctl1);
write32(0x0, &svregs->lp.act_tamper_routing_ctl2)
/* activate out pad of AT1 and enable it, AT1 output on pin et5 */
write32(0x00010000 | 0x00000001, &svregs->lp.act_tamper_ctl)
/* Configuring IRQs and secviols */
write32(0x8000003f, &svregs->hp.secvio_intcfg);
write32(0x4000003f, &svregs->hp.secvio_ctl);
write32(0x0000003f, &svregs->lp.secvio_ctl)
/* Activating detector for ET5 */
write32(0x00000000, &svregs->lp.tamper_det_cfg);
write32(0x00000004, &svregs->lp.tamper_det_cfg2);
Best regards. Re: Correct snvs_cfg values for TAMPER_OUT0/TAMPER_IN4 active tamper loop on i.MX8DXL EVK (J20) Thank you for the configuration. I applied it exactly on a fresh power cycle: snvs_dgo_cfg 0 0 20000000 0 80000000 0 snvs_cfg 0 8000003f 4000003f 0 3f 0 0 4 0 0 84001111 0 0 0 0 10001 0 10000 0 Readback matches your values: SNVS e8(2) = 00010000 00000000, SNVS 48(2) = 00000000 00000004, SNVS e0 = 00010001, DGO 20 = 20000000, DGO 40 = 80000000. Result: LPTDSR (SNVS a4) = 00000004 (ET5D set). It reads 00000004 both with no jumper and with an insulated jumper connected between J20 pin 1 (TAMPER_IN4) and pin 3 (TAMPER_OUT0). It also stays 00000004 after snvs_clear_status 107ff ff. So detection asserts with the loop open, but I never get a clean 00000000 state with the loop closed. Questions: 1. Does the TAMPER_OUT0 / TAMPER_IN4 loop on this EVK need a pad or pull setting (for example DGO tamper_pull_ctl), or a different act_tamper_clk_ctl value, for a wired-jumper loop? 2. Is snvs_clear_status expected to clear LPTDSR while the tamper condition is still present? 3. Is any other setting needed for the loop to be seen as closed? Thanks again.
記事全体を表示